Skip to content

Software Setup

ESP32 Firmware

We have intentionally kept the ESP32 firmware as simple as possible - its only tasks are to: discipline the TCXO oscillator; control the OLED display. The intention is that you can easily develop your own firmware for the GNSSDO if the SparkFun firmware does not meet your needs.

The /Firmware/Binaries folder contains the firmware binaries.

You can update or reload the firmware using the SparkFun RTK Firmware Uploader.

You can of course modify the hardware too, should you want to. The design is completely open-source.

Note

The mosaic-T module has numerous capabilities and a multitude of ways to configure and interface with them. Without regurgitating all the information that is documented in Septentrio's user manuals and videos, we have tried to highlight a good majority of the module's aspects.

With that said, please feel free to file an issue if you feel we have missed something that may benefit other users. (Don't forget to provide us with a link to the documentation and what section the information is located.)

Septentrio logo mosaic-T

RxTools Software Suite

Tip

Even if you aren't necessarily interested in it, we highly recommend that users install the RXTools software suite before plugging in their board. For Windows PCs, it also includes the USB driver for the module that enables the Ethernet-over-USB support and virtual COM ports.

Users should install the RXTools software suite on their computer to interact with the mosaic-T module through the USB interface. The software package includes the USB-IP driver1 necessary to recognize the board as an ethernet device on Windows PCs (1).

  1. On Linux, the standard Linux CDC-ACM driver is suitable.
System Requirements2
  • Windows 7
  • Windows 8
  • Windows 10
  • Fedora 23 (or later) using Qt technology.
    • The standalone tools (except bin2asc) will run on older distributions.

The minimal hardware requirements (1Hz update3):

  • CPU: 1 GHz processor
  • RAM: 1 GB RAM
  • Screen Resolution: 1024×768 or higher resolution
Installation Instructions2

Users can install RxTools software suite by running the installation executable4(1), located in the RxTools\windows directory of the downloaded *.zip file5. During the installation process, users will be notified if a previous version of RxTools is already installed then the previous version will be uninstalled. Next, users will need to provide an installation directory for the RxTools software suite. Users will then select which of the following applications6 are installed:

  1. For RxTools v22.1.0, the installation filename is RxTools_22_1_0_Installer.exe for Windows PCs.
  • RxControl
  • SBF Converter
  • SBF Analyzer
  • RxLogger
  • RxUpgrade
  • RxDownload
  • RxPlanner
  • Data Link
  • RxAssistant
  • RxLauncher

Warning

It is recommended that users NOT install RxControl as root, for security reasons and to avoid installation overwrites of other system settings. To make RxTools available to more than one user, provide a shared installation directory.

Users can install RxTools software suite by running the installation binary4(1), located in the RxTools/linux-i386/ directory of the downloaded *.zip file5. During the installation, users will be prompted for an installation directory. If there are any previous installations of RxControl, please use a different directory to avoid conflicts.

  1. For RxTools v22.1.0, the installation filename is RxTools_22_1_0_Installer.bin for Linux.
Permission Settings

Once installed, users may need to reconfigure their permission settings:

  • RxTools will need rights to access the /dev/ttyS* serial ports.

    • To access the serial ports, users must be part of the uucp and lock groups (1). This can be configured by editing the /etc/group7 file and adding the username to the lines defining the uucp group and the lock group.

      For example, when adding the user jsmith to the uucp group, users would modify the /etc/group file as shown below:

      uucp:x:14:uucp # (2)!
      uucp:x:14:uucp,jsmith # (3)!
      
    • On Linux machine administered centrally on a local network, ask your system administrator to be included in the uucp and lock groups.

  • RxTools also needs read/write (rw) access(4) to the /dev/ttyS* serial ports.

    • Users can change the permissions with the chmod8 command:

      chmod 660 /dev/ttyS<add port> # (5)!>
      
  1. On most Linux operating systems, the /dev/ttyS* devices are owned by root and belong to the uucp group with read/write (rw) access. Additionally, the devices are normally locked by writing a file in the /var/lock/ directory, with the same permissions.
  2. Remove
  3. Replace with this line
  4. By default, users will normally have read/write (rw) access to the /dev/ttyS* serial ports.
  5. where users must specify the port number
    e.g. /dev/ttyS0 might be port COM1

Note

In order for these changes to take effect, users must update their environment by logging out and back in.

Be aware that the X-session has to be restarted as well. On most systems, this can be done by pressing the key combination Ctrl + Alt + Backspace

64-bit OS

In order to run the RxTools on a 64-bit Linux operating system, users might have to install the 32-bit version of the C standard library.

  • For Fedora installations, this is the glibc.i686 package.
  • The equivalent for Debian(/Ubuntu) installations is the ia32-libs package.

Septentrio USB Driver

If users haven't already installed the RxTools software suite on their Windows PC, they will need to install the USB driver1 necessary to recognize and interact with the mosaic-T module through the USB interface.

A Windows USB driver for the mosaic-T can be installed through two methods:

  • RxTools Software Suite (1)
  • mosaic-T GNSS Receiver Module (2)
  1. The driver is installed during the installation process.
  2. The installation file for the Windows USB driver will be available from the mass-storage device when the board is initially connected to the computer.

Once installed, the driver emulates two virtual serial ports, which can be accessed as standard COM ports to the receiver.

Terminal Emulators

Most terminal emulation programs will not make a distinction between virtual or native COM ports. However, for virtual serial ports, the port settings (i.e. baud rate, etc.) are not relevant and the default configuration is used in the terminal emulation program. However, the physical/native COM ports will have the following default setting:

  • Baudrate: 115200bps
  • Data Bits: 8
  • Parity: No
  • Stop Bits: 1
  • Flow Control: None
Having Trouble?

For users who are having trouble installing the USB driver, we have an archived version (v3.0.29) of the installation file. Users can download version 3.0.2 of the driver, by clicking on the button below.

On Linux, the standard Linux CDC-ACM driver is suitable for the mosaic-T module.

Web Interface

With the USB driver installed, the mosaic-T module supports Ethernet-over-USB. The default IP address allocated for the Ethernet-over-USB interface is 192.168.3.1. This IP can be entered in any browser to open a connection to the receiver's Web Interface as shown below.

navigation tabs in the web interface

All the drop-down navigation tabs in the web interface.

Info

The default IP address cannot be changed; this feature is only to be used when a single receiver is connected to your computer.

Invalid IP Address (WiFi Only)

One of the documentation pages on Septentrio's website, specifies a default IP address of 192.168.20.1 for the web interface. However, that address is for a WiFi enabled product and cannot be used with this product.

Espressif logo ESP32

CH340 USB Driver

Users will need to install a USB driver for the CH340 serial-to-USB chip, in order to communicate with the ESP32 module. The latest USB drivers for the CH340 are available from the manufacturer, on the WCH website:

Need Directions?

For users having trouble installing the CH340 USB driver, check out our video and hookup guide:

Terminal Emulator

In order to configure the firmware settings on the ESP32, users will need to install a serial terminal emulator on their computer.

For Windows computers, we highly recommend TeraTerm.

Some Linux operating systems will already have the screen terminal emulator preinstalled.

Need Directions?

Check out our hookup guide to install your favorite terminal emulator:

Software Settings

When connected to the ESP32 CH340 COM port at 115200 baud, pressing any key in the terminal emulator will open the firmware Main Menu:

ESP32 firmware main menu

The ESP32 firmware main menu.

Configure Operation

Select option c ("c" followed by "Enter") to configure the firmware:

ESP32 firmware configuration menu

The ESP32 firmware configuration menu.

  • 1) RX Clock Bias Lock Limit
    • This allows the clock bias limit to be set. The units are milliseconds.
    • The LOCK LED will illuminate when the bias is below this limit.
    • PPS output will begin when the bias has been below this limit for RX Clock Bias Limit Count seconds.
  • 2) RX Clock Bias Initial Limit
    • This allows the initial clock bias limit to be set. The units are milliseconds.
    • The firmware will soft-reset the GNSS if the clock bias is above this limit for RX Clock Bias Limit Count seconds.
    • This allows the firmware to restart the GNSS and re-sync the TCXO if the initial bias is excessive.
  • 3) RX Clock Bias Limit Count
    • This defines how many consecutive 1Hz samples are needed to trigger the two clock bias limits.
  • 4) Pk (PI P term)
    • This defines the Proportional term for the TCXO frequency PI control loop. Default is 0.63
    • This value was determined using approximate Ziegler-Nichols tuning of the SiT5358 loop.
  • 5) Ik (PI I term)
    • This defines the Integral term for the TCXO frequency PI control loop. Default is 0.151
    • This value was determined using approximate Ziegler-Nichols tuning of the SiT5358 loop.
  • 6) Prefer non-composite GPS bias
    • With a subscription to Fugro AtomiChron, this option allows the individual GPS clock bias to be preferred over the composite Fugro bias.
    • You can enable a preference for either GPS or Galileo. Enabling GPS will disable Galileo.
  • 7) Prefer non-composite Galileo bias
    • With a subscription to Fugro AtomiChron, this option allows the individual Galileo clock bias to be preferred over the composite Fugro bias.
    • You can enable a preference for either GPS or Galileo. Enabling Galileo will disable GPS.
  • 8) Pulse-Per-Second Interval
    • This defines the interval of the PPS signal. The intervals are defined by the mosiac-T firmware. Use "8" and "Enter" to scroll through the intervals:
      • "off"
      • "msec10"
      • "msec20"
      • "msec50"
      • "msec100"
      • "msec200"
      • "msec250"
      • "msec500"
      • "sec1"
      • "sec2"
      • "sec4"
      • "sec5"
      • "sec10"
      • "sec30"
      • "sec60"
  • 9) Pulse-Per-Second Polarity
    • This defines the PPS signal polarity: Low2High or High2Low
  • 10) Pulse-Per-Second Delay
    • This allows the timing of the PPS signal to be advanced or retarded. The units are nanoseconds.
  • 11) Pulse-Per-Second Time Scale
    • This defines which time scale is used to generate the PPS signal.
      • "GPS"
      • "Galileo"
      • "BeiDou"
      • "GLONASS"
      • "UTC"
      • "RxClock"
  • 12) Pulse-Per-Second Max Sync Age
    • This defines how long PPS pulses will be produced when the GNSS signal is lost or jammed: 0 to 3600 seconds.
  • 13) Pulse-Per-Second Pulse Width
    • This defines the width of the PPS signal. The units are milliseconds: 0.000001 to 1000.000000.
  • 14) TCP Server (IPS1)
  • 15) TCP Server Port
    • The port for the TCP connection. Default is 28785.

To reset all settings to their default values, select "r", "Enter", "y", "Enter"

The settings are saved to non-volatile memory (NVM, LittleFS) on exiting the menu. Ensure you fully exit the menu ("x", "Enter", "x", "Enter") to save any modified settings.

The TCXO frequency control word is saved to NVM once per hour, to allow a quicker startup at the next power-on.

TCP Server (IPS1)

When TCP Server (IPS1) is enabled, the ESP32 serial console is diverted from the CH340 USB (CONFIG ESP32) interface to the mosaic-T COM3 UART interface and daisy chained to the IPS1 TCP server. The configuration menu and debug messages can then be accessed over TCP / Telnet on the chosen port. The CH340 USB (CONFIG ESP32) interface is then no longer active.

TCP / Telnet is supported over both Ethernet and the Ethernet-over-USB connection. Only one TCP2Way connection is supported.

If you are using Tera Term:

  • Select TCP/IP and Telnet
  • Enter the mosaic-T's IP address in Host
    • If you are connected via the CONFIG MOSAIC Ethernet-over-USB interface, the IP address is 192.168.3.1
  • Enter the TCP Server Port number in TCP port#
    • The default port is 28785

Tera Term configuration for TCP

Tera Term configuration for TCP.

Debug Software

Select option d ("d" followed by "Enter") to configure the software debug options:

ESP32 firmware debug menu

The ESP32 firmware debug menu.

The debug options are what we use at SparkFun to check that the firmware is running correctly. You should not need change any of the options, except perhaps option 8 Print conditions. This option controls the periodic CSV messages seen in the console when the menu is closed. The format can be changed to human-readable text, or the messages can be disabled if desired.

The format of the Print conditions CSV data is:

YYYY/MM/DD,HH:MM:SS,Epoch,Lat,Lon,Alt,TimeSys,Error,Fine,PPS,Bias,Source,TCXO,Pk,Ik,Press,Temp,Hum

  • YYYY/MM/DD is the date from the ReceiverTime SBF message
  • HH:MM:SS is the time from the ReceiverTime SBF message
  • Epoch is the date and time in Unix epoch format: seconds.milliseconds from midnight UTC January 1st 1970. This is useful when plotting the data against time.
  • Lat is the Latitude in degrees from the PVTGeodetic SBF message (7 decimal places)
  • Lon is the Longitude in degrees from the PVTGeodetic SBF message (7 decimal places)
  • Alt is the Altitude in metres from the PVTGeodetic SBF message (0.1mm resolution)
  • TimeSys is the named TimeSystem from the PVTGeodetic SBF message
  • Error is the Error byte from the PVTGeodetic SBF message. 0 indicates no error
  • Fine is the FINETIME bit from the SyncLevel byte from the ReceiverTime SBF message
  • PPS indicates if the Pulse-Per-Second output is enabled
    • PPS is enabled when the RxClkBias reaches the required accuracy, set by RX Clock Bias Lock Limit
  • Bias is the receiver clock bias in seconds
  • Source is the source of the receiver clock bias reported in Bias
    • By default, this is PVT indicating the source is the composite RxClkBias from the PVTGeodetic SBF message
    • If AtomiChron is enabled and if Prefer non-composite GPS bias or Prefer non-composite Galileo bias has been selected, this will change to GPS or Galileo indicating that the individual non-composite bias from the FugroTimeOffset SBF message is available and is being used
  • TCXO is the 26-bit signed frequency control word written to the SiT5358 TCXO
  • Pk is the PI control loop Proportional term - set in the configuration menu
  • Ik is the PI control loop Integral term - set in the configuration menu
  • Press is the atmospheric pressure in hPa (mbar) : GNSSDO Plus (GNSSDO+) only
  • Temp is the internal temperature in degrees C : GNSSDO Plus (GNSSDO+) only
  • Hum is the relative humidity in %RH : GNSSDO Plus (GNSSDO+) only

Note

The GNSSDO Plus (GNSSDO+) contains a MS8607 pressure, temperature and humidity sensor. The readings are reported in the periodic messages.

The temperature reading will be higher than expected due to the sensor's proximity to the OCXO. The OCXO runs at elevated temperature; heat will be coupled to the sensor by convection, radiation and conduction (through the PCB).

Firmware Upgrade

The /Firmware/Binaries folder contains the firmware binaries. v2.2 is the latest stable release - as at 2-3-26.

You can update or reload the firmware using the SparkFun RTK Firmware Uploader.

See below for details on how to upload with esptool from the command line.

Compiling Firmware - using Docker

To compile the GNSSDO Firmware, you need to use the correct version of the ESP32 Arduino core and of each required Arduino library. It is tedious and error-prone. Especially on Windows. We've lost count of the number of times code compilation fails on our local machines, because we had the wrong ESP32 core installed... It is much easier to sandbox the firmware compilation using an environment like Docker.

Docker is open-source. It is our new favourite thing!

Here is a step-by-step guide for how to install Docker and compile the firmware from scratch:

Clone, fork or download the GNSSDO repo

To build the GNSSDO Firmware, you obviously need a copy of the source code.

Click on the icon below to download a copy of the main (released) branch:

Download ZIP

For the real Wild West experience, you can also download a copy of the release_candidate code branch. This is where the team is actively changing and testing the code, before it becomes a full release. The code there will usually compile and will usually work, but we don't guarantee it! We may be part way through implementing some breaking changes at the time of your download...

Download ZIP - release candidate

Install Docker Desktop

  • (Optional) Head to Docker and create an account. A free "Personal" account will cover occasional compilations of the firmware
  • Download and install Docker Desktop - there are versions for Mac, Windows and Linux. You may need to restart to complete the installation.
  • Run the Desktop
    • You don't need to have an account and you don't need to be signed in
    • You only need to be signed in if you want to store or share your Container on Docker Hub
    • If you don't sign in, Docker Desktop will run in Personal mode - which will cover local compilations of the firmware
  • On Windows, you may see an error saying "WSL needs updating Your version of Windows Subsystem for Linux (WSL) is too old". If you do:
    • Open a command prompt
    • Type wsl --update to update WSL. At the time of writing, this installs Windows Subsystem for Linux 2.6.1
    • Restart the Docker Desktop
  • If you are using Docker for the first time, the "What is a container?" and "How do I run a container?" demos are useful - but not essential
    • On Windows, you may want to give Docker Desktop permission to access to your Network, so it can access (e.g.) HTML ports
    • You can Stop the container and Delete it when you are done
  • You may want to prevent Docker from running when your machine starts up
    • Uncheck "Start Docker Desktop when you sign in to your computer" in the Desktop settings

Using Docker to create the firmware binary

  • Make sure you have Docker Desktop running. You don't need to be signed in, but it needs to be running.
  • Open a Command Prompt and cd into the SparkFun_GNSSDO folder
  • Check you are in the right place. Type dir and hit enter. You should see the following files and folders:
    .gitattributes
    .github
    .gitignore
    CONTRIBUTING.md
    docs
    Firmware
  • cd Firmware and then dir again. You should see:
    app3M_fat9M_16MB.csv
    Binaries
    compile_with_docker.bat
    Dockerfile
    GNSSDO_Firmware
    Utils
  • The file that does most of the work is the Dockerfile

  • Run compile_with_docker.bat to compile the firmware. It does everything for you

  • Type dir again. Hey presto! You have your newly compiled firmware binary!

You can then use (e.g.) the SparkFun RTK Firmware Uploader to upload the binary onto the ESP32.

You may find the .elf file useful if you are trying to debug the code with me-no-dev's Exception Decoder.

Uploading Firmware - using esptool

The SparkFun RTK Firmware Uploader contains a copy of Espressif's esptool. It is esptool that actually performs the code upload.

If you want to upload new firmware manually from the command line, here are the commands:

esptool.py --chip esp32 --port /dev/ttyUSB0 --baud 460800 --before default_reset --after no_reset write_flash -z --flash_mode dio --flash_freq 80m --flash_size detect 0x1000 RTK_Surveyor.ino.bootloader.bin 0x8000 RTK_Surveyor_Partitions_16MB.bin 0xe000 boot_app0.bin 0x10000 GNSSDO_Firmware.ino.bin

followed by:

esptool.py --chip esp32 --port /dev/ttyUSB0 --before default_reset run

On Windows, you can replace esptool.py with esptool.exe. You can find a copy of esptool.exe in the Utils folder.

On Windows, replace /dev/ttyUSB0 with the name of your CH340 COM port: COM1 or similar.

You can find copies of RTK_Surveyor.ino.bootloader.bin, RTK_Surveyor_Partitions_16MB.bin and boot_app0.bin in the Firmware Uploader resource folder.

Enjoy!

  • Your friends at SparkFun

  1. On Linux, the standard Linux CDC-ACM driver is suitable. 

  2. The system requirements and installation instructions are from the RxTools v22.1.0 user manual. This information may change in later iterations of the software suite. Please refer to the user manual (of the version you are utilizing) for the most accurate information. 

  3. Higher data rates will require higher CPU speed and more memory capacity. 

  4. Users will need administrative privileges to install the RxTools software. 

  5. Users may need to extract the RxTools installation files from the downloaded, compressed file. 

  6. Please see the release notes for the issues and limitations of the RxTools applications. 

  7. Requires c privileges. 

  8. Changing these permissions also requires root privileges. 

  9. For the latest USB driver from Septentrio, please install their driver through the RxTools software suite.
    This driver version was archived at the time that the mosaic-T hookup guide was written. Please do not request for the file to be updated.