Introduction
-
SparkFun Qwiic Pocket Development Board - ESP32-C6
SKU: DEV-22925
-
The SparkFun Qwiic Pocket Development Board - ESP32-C6features the ESP32-C6 Mini-1 module from espressif™. The ESP32-C6 SoC is built around a RISC-V single-core processor with 4 MB flash memory and supports 2.4 GHz WiFi 6, Bluetooth® 5 (with Low Energy), Zigbee and Thread 802.15.4 wireless protocols. The module uses an integrated PCB antenna.
The ESP32-C6 includes on-chip serial-to-UART conversion which helps reduce the number of components on the development board so we designed this Qwiic Dev Board to cram as much as we could into the Qwiic system's 1"x1" form factor. It also includes a USB-C connector, 2-pin JST connector for a single-cell LiPo battery along with a charging circuit for a connected battery, a Qwiic connector, and it also breaks out eight GPIO pins (including one UART).Purchase from SparkFun
Required Materials
To follow along with this guide you will need a USB-C cable to connect the dev board to your computer:
You may also want to get a Qwiic cable or kit to connect the Qwiic Dev Board - ESP32-C6 to other Qwiic devices:
Optional Materials
The Qwiic Dev Board - ESP32-C6 includes a 2-pin JST connector and integrated charging circuit for an attached single-cell LiPo battery. Below are a few options for batteries we recommend for battery-powered applications:
If you prefer a soldered connection or want to modify the solder jumpers on this board, you may need some of the products listed below:
Smart Watch Example Materials
This guide also includes a demo using the Qwiic Pocket Development Board - ESP32-C6 with three Qwiic breakouts to create a DIY "smart watch" (sans the wristband) complete with display, pedometer, and motion controls. If you'd like to follow along and build this example, you'll need the following Qwiic breakouts:
You'll also need three Qwiic cables of your choice of length and a set of standoffs to assemble the smart watch. We recommend either the 50mm or 100mm flexible cables as shown below:
Suggested Reading
We designed this board for integration into SparkFun's Qwiic connect system. Click on the banner below to learn more about the SparkFun Qwiic Connect System.
Before getting started with this Hookup Guide, you may want to read through the tutorials below if you are not familiar with the concepts covered in them or want a refresher. If you are using either of the Qwiic Shields linked above, we recommend reading through their respective Hookup Guides before continuing with this tutorial: