![]() |
SparkFun Qwiic Ultrasonic Distance Sensor
v1.2.0-4-ge9b8e35
SparkFun Qwiic Ultrasonic Distance Sensor
|
Arduino Library for the SparkFun SparkFun Ultrasonic Distance Sensor
The SparkFun Ultrasonic Distance Sensor - TCT40 (sen-24805) a user-friendly upgrade to the popular HC-SR04 sensor, offers non-contact distance measurement from 2cm to 400cm with an accuracy of 3mm. This sensor is designed to seamlessly integrate with the Qwiic ecosystem for I2C communication, making it a breeze to add to your existing projects and daisy-chain with other Qwiic components.
If you prefer to bypass the Qwiic connector and I2C, you can also access the VCC, Trigger, Echo, and Ground pins broken out on the board's edge. Please be aware that this ultrasonic sensor comes uncalibrated, and you will need to manipulate the raw output for your specific application.
With its wide range of applications, the SparkFun Qwiic Ultrasonic Distance Sensor is a versatile tool for robotics projects, obstacle avoidance systems, and any application that requires accurate distance measurement without physical contact. Its adaptability makes it a valuable addition to your toolkit.
Looking for the board that matches this library - pick up a SparkFun Ultrasonic Distance Sensor - TCT40 (Qwiic) at www.sparkfun.com.
This library provides a simple interface that enables the following functionality when using the SparkFun Qwiic Ultrasonic Distance Sensor:
The following outlines the general use of the library in an Arduino Sketch.
At the start of your sketch, the library header file is included using the following statement:
Before the arduino setup()
function, create a Ultrasonic Distance Sensor object in your file with the following declaration:
In the Arduino setup()
function, initialize the sensor by calling the begin method. This method is called after the Arduino Wire
(I2C) library is initialized.
The begin method returns true if the sensor is connected and available, and false if it is not.
To read the value from the sensor, the triggerAndRead() method is called on the sensor object.
The value returned is a distance value measured in millimeters
The following examples are provided with the library
The full API and use documentation for this library is provided here. For a quick reference, the main methods available in the library are listed here.
Curious about the hardware this board works with - visit the SparkFun Qwiic Ultrasonic Distance Sensor hardware repository.
The Hookup Guide for the SparkFun Qwiic Ultrasonic Distance Sensor is available here.
This product is open source!
This product is licensed using the MIT Open Source License.