Corrections Priorities
- EVK:
- Facet mosaic:
- Postcard:
- Torch:

RTK Corrections Priorities Menu
To achieve an RTK Fix, SparkFun RTK products must be provided with a correction source. An RTK device can obtain corrections from a variety of sources. Below is the list of possible sources (not all platforms support all sources) and their default priorities. These defaults generally follow the rule that a shorter baseline between Rover and Base leads to more accurate, and therefore more valuable, correction data:
- External Radio (100m OSR Baseline) - Two packet radios communicating directly between a Rover and Base
- ESP-NOW (100m OSR Baseline) - Two RTK devices communicating directly between a Rover and Base over the built-in 2.4GHz radios
- LoRa Radio (1km OSR Baseline) - Two RTK devices communicating directly between a Rover and Base over the built-in LoRa radios (RTK Torch only)
- Bluetooth (10+km OSR/SSR Baseline) - A Rover obtaining corrections over Bluetooth to a phone/tablet that has an NTRIP Client
- USB (10+km OSR/SSR Baseline) - A Rover obtaining corrections over USB to a phone/tablet that has an NTRIP Client
- TCP (NTRIP) (10+km OSR/SSR Baseline) - A Rover obtaining corrections over WiFi to a NTRIP Caster
- L-Band (100km SSR Baseline) - A Rover obtaining corrections from a geosynchronous satellite
- IP (PointPerfect/MQTT) (100+km SSR Baseline) - A Rover obtaining corrections from an SSR type correction service over WiFi or cellular
The Corrections Priorities menu allows a user to specify which correction source should be given priority. For example, if corrections are provided through ESP-NOW and IP PointPerfect simultaneously, the corrections from IP PointPerfect will be discarded because the ESP-NOW source has a higher priority. This prevents the RTK engine from receiving potentially mixed correction signals.

In the serial terminal menu, pressing a letter will increase or decrease the position of a priority. For example, in the image above, pressing G will raise the L-Band priority above TCP (NTRIP).
Additionally, this menu gives visibility into which corrections are currently being received and utilized (marked with the *) by the RTK engine.
The Correction source lifetime in seconds setting dictates how many seconds an active source must be silent before it is marked as inactive.
In the web config page:
- Clicking a source increases its priority
- Clicking the highest priority source makes it the lowest priority
- Clicking 'Reset to Defaults' will restore the priorities to their default setting
- Click 'Save Configuration', then 'Exit and Reset' to save the changes

Please see Correction Sources for a description of where to obtain corrections.
Please also see Corrections Source Icons for details of the corrections source icon displayed on the OLED.