![]() |
Qwiic_Keypad_Py
2.0.0-2-g90d1767
Python for SFE Qwiic Keypad
|
The SparkFun Qwiic Keypad provides a simple and cost effective solution for adding button inputs to your project without tying up GPIO lines. Implementing a SparkFun Qwiic I2C interface, these sensors can be rapidly added to any project with boards that are part of the SparkFun Qwiic ecosystem.
This repository implements a Python package for the SparkFun Qwiic Keypad. This package works with Python, MicroPython and CircuitPython.
This python package enables the user to access the features of the Keypad via a single Qwiic cable. This includes reading keypresses, time of press, and more. The capabilities of the Keypad are each demonstrated in the included examples.
New to qwiic? Take a look at the entire SparkFun qwiic ecosystem.
This Python package supports the following SparkFun qwiic products on Python, MicroPython and Circuit python.
| Python | Platform | Boards |
|---|---|---|
| Python | Linux | Raspberry Pi , NVIDIA Jetson Orin Nano via the SparkFun Qwiic SHIM |
| MicroPython | Raspberry Pi - RP2, ESP32 | SparkFun Pro Micro RP2350, SparkFun IoT RedBoard ESP32, SparkFun IoT RedBoard RP2350 |
| CircuitPython | Raspberry Pi - RP2, ESP32 | SparkFun Pro Micro RP2350, SparkFun IoT RedBoard ESP32, SparkFun IoT RedBoard RP2350 |
[!NOTE] The listed supported platforms and boards are the primary platform targets tested. It is fully expected that this package will work across a wide variety of Python enabled systems.
The first step to using this package is installing it on your system. The install method depends on the python platform. The following sections outline installation on Python, MicroPython and CircuitPython.
The package is primarily installed using the pip3 command, downloading the package from the Python Index - "PyPi".
Note - the below instructions outline installation an Linux-based (Raspberry Pi) system.
First, setup a virtual environment from a specific directory using venv:
You can pass any path as path/to/venv, just make sure you use the same one for all future steps. For more information on venv click here.
Next, install the qwiic package with:
Now you should be able to run any example or custom python scripts that have import qwiic_keypad by running e.g.:
If not already installed, follow the instructions here to install mpremote on your computer.
Connect a device with MicroPython installed to your computer and then install the package directly to your device with mpremote mip.
If you would also like to install the examples for this repository, issue the following mip command as well:
If not already installed, follow the instructions here to install CircUp on your computer.
Ensure that you have the latest version of the SparkFun Qwiic CircuitPython bundle.
Finally, connect a device with CircuitPython installed to your computer and then install the package directly to your device with circup.
If you would like to install any of the examples from this repository, issue the corresponding circup command from below. (NOTE: The below syntax assumes you are using CircUp on Windows. Linux and Mac will have different path seperators (i.e. "/" vs. "\"). See the <a href="https://learn.adafruit.com/keep-your-circuitpython-libraries-on-devices-up-to-date-with-circup/example-command" >CircUp \"example\" command documentation</a> for more information)
@icode{sh}
circup example qwiic_keypad\qwiic_keypad_ex1
circup example qwiic_keypad\qwiic_keypad_ex2
circup example qwiic_keypad\qwiic_keypad_ex3
@endicode
@subsection autotoc_md10 Example Use
Below is a quickstart program to print which button was pressed or a space if '*' is pressed and a newline if '#' is pressed.
See the examples directory for more detailed use examples and <a href="https://github.com/sparkfun/qwiic_keypad_py/blob/main/examples/README.md" >examples/README.md</a> for a summary of the available examples.
@icode{python}
import qwiic_keypad
import time
import sys
def runExample():
print("\nSparkFun qwiic Keypad Example 1
")
myKeypad = qwiic_keypad.QwiicKeypad()
if myKeypad.is_connected() == False:
print("The Qwiic Keypad device isn't connected to the system. Please check your connection", \
file=sys.stderr)
return
myKeypad.begin()
button = 0
while True:
# necessary for keypad to pull button from stack to readable register
myKeypad.update_fifo()
button = myKeypad.get_button()
if button == -1:
print("No keypad detected")
time.sleep(1)
elif button != 0:
# Get the character version of this char
charButton = chr(button)
if charButton == '#':
print()
elif charButton == '*':
print(" ", end="")
else:
print(charButton, end="")
# Flush the stdout buffer to give immediate user feedback
sys.stdout.flush()
time.sleep(.25)
# Development in progress
@endicode
<p align="center">
<img src="https://cdn.sparkfun.com/assets/custom_pages/3/3/4/dark-logo-red-flame.png" alt="SparkFun - Start Something">