![]() |
Qwiic_Soil_Moisture_Sensor_Py
v0.1.0_test1-3-g8d67a0e
Python for SFE Qwiic Soil Moisture Sensor
|
The SparkFun Qwiic Soil Moisture Sensor provides a simple and cost effective solution for adding soil moisture sensing to your project. Implementing a SparkFun Qwiic I2C interface, these sensors can be rapidly added to any project with boards that are part of the SparkFun Qwiic ecosystem.
This repository implements a Python package for the SparkFun Qwiic Soil Moisture Sensor. This package works with Python, MicroPython and CircuitPython.
This python package enables the user to access the features of the Qwiic Soil Moisture Sensor via a single Qwiic cable. This includes reading the moisture level, turning on and off the LED, and more. The capabilities of the moisture sensor are each demonstrated in the included examples.
New to qwiic? Take a look at the entire SparkFun qwiic ecosystem.
This Python package supports the following SparkFun qwiic products on Python, MicroPython and Circuit python.
| Python | Platform | Boards |
|---|---|---|
| Python | Linux | Raspberry Pi , NVIDIA Jetson Orin Nano via the SparkFun Qwiic SHIM |
| MicroPython | Raspberry Pi - RP2, ESP32 | SparkFun Pro Micro RP2350, SparkFun IoT RedBoard ESP32, SparkFun IoT RedBoard RP2350 |
| CircuitPython | Raspberry Pi - RP2, ESP32 | SparkFun Pro Micro RP2350, SparkFun IoT RedBoard ESP32, SparkFun IoT RedBoard RP2350 |
[!NOTE] The listed supported platforms and boards are the primary platform targets tested. It is fully expected that this package will work across a wide variety of Python enabled systems.
The first step to using this package is installing it on your system. The install method depends on the python platform. The following sections outline installation on Python, MicroPython and CircuitPython.
The package is primarily installed using the pip3 command, downloading the package from the Python Index - "PyPi".
Note - the below instructions outline installation an Linux-based (Raspberry Pi) system.
First, setup a virtual environment from a specific directory using venv:
You can pass any path as path/to/venv, just make sure you use the same one for all future steps. For more information on venv click here.
Next, install the qwiic package with:
Now you should be able to run any example or custom python scripts that have import qwiic_soil_moisture_sensor by running e.g.:
If not already installed, follow the instructions here to install mpremote on your computer.
Connect a device with MicroPython installed to your computer and then install the package directly to your device with mpremote mip.
If you would also like to install the examples for this repository, issue the following mip command as well:
If not already installed, follow the instructions here to install CircUp on your computer.
Ensure that you have the latest version of the SparkFun Qwiic CircuitPython bundle.
Finally, connect a device with CircuitPython installed to your computer and then install the package directly to your device with circup.
If you would like to install any of the examples from this repository, issue the corresponding circup command from below. (NOTE: The below syntax assumes you are using CircUp on Windows. Linux and Mac will have different path seperators (i.e. "/" vs. "\"). See the <a href="https://learn.adafruit.com/keep-your-circuitpython-libraries-on-devices-up-to-date-with-circup/example-command" >CircUp \"example\" command documentation</a> for more information)
@icode{sh}
circup example qwiic_soil_moisture_sensor\Example1_GetReadings
circup example qwiic_soil_moisture_sensor\Example2_Change_I2C_Address
@endicode
@subsection autotoc_md11 Example Use
Below is a quickstart program to print moisture level and toggle the LED on the Soil Moisture Sensor.
See the examples directory for more detailed use examples and <a href="https://github.com/sparkfun/qwiic_soil_moisture_sensor_py/blob/main/examples/README.md" >examples/README.md</a> for a summary of the available examples.
@icode{python}
import qwiic_soil_moisture_sensor
import time
import sys
def runExample():
print("\nSparkFun Qwiic Soil Moisture Sensor Example 1
")
mySoilSensor = qwiic_soil_moisture_sensor.QwiicSoilMoistureSensor()
if mySoilSensor.is_connected() == False:
print("The Qwiic Soil Moisture Sensor device isn't connected to the system. Please check your connection", \
file=sys.stderr)
return
mySoilSensor.begin()
print("Initialized.")
while True:
mySoilSensor.read_moisture_level()
print (mySoilSensor.level)
mySoilSensor.led_on()
time.sleep(1)
mySoilSensor.led_off()
time.sleep(1)
if __name__ == '__main__':
try:
runExample()
except (KeyboardInterrupt, SystemExit) as exErr:
print("\nEnding Example 1")
sys.exit(0)
@endicode
<p align="center">
<img src="https://cdn.sparkfun.com/assets/custom_pages/3/3/4/dark-logo-red-flame.png" alt="SparkFun - Start Something">