![]() |
Qwiic_Titan_Gps_Py
2.0.1-1-g86f2d1a
Python for SFE Qwiic Titan Gps
|
The SparkFun Qwiic GPS Receiver TITAN_GPS Module provides a simple and cost effective solution for adding GPS Receiver capabilities to your project. Implementing a SparkFun Qwiic I2C interface, these sensors can be rapidly added to any project with boards that are part of the SparkFun Qwiic ecosystem.
This repository implements a Python package for the SparkFun Qwiic TITAN_GPS. This package works with Python, MicroPython and CircuitPython.
This python package enables the user to access the features of the TITAN_GPS via a single Qwiic cable. This includes reading Latitude and Longitude, reading altiude, reading time and more. The capabilities of the TITAN_GPS are each demonstrated in the included examples.
New to qwiic? Take a look at the entire SparkFun qwiic ecosystem.
This Python package supports the following SparkFun qwiic products on Python, MicroPython and Circuit python.
| Python | Platform | Boards |
|---|---|---|
| Python | Linux | Raspberry Pi , NVIDIA Jetson Orin Nano via the SparkFun Qwiic SHIM |
| MicroPython | Raspberry Pi - RP2, ESP32 | SparkFun Pro Micro RP2350, SparkFun IoT RedBoard ESP32, SparkFun IoT RedBoard RP2350 |
| CircuitPython | Raspberry Pi - RP2, ESP32 | SparkFun Pro Micro RP2350, SparkFun IoT RedBoard ESP32, SparkFun IoT RedBoard RP2350 |
[!NOTE] The listed supported platforms and boards are the primary platform targets tested. It is fully expected that this package will work across a wide variety of Python enabled systems.
The first step to using this package is installing it on your system. The install method depends on the python platform. The following sections outline installation on Python, MicroPython and CircuitPython.
The package is primarily installed using the pip3 command, downloading the package from the Python Index - "PyPi".
Note - the below instructions outline installation on a Linux-based (Raspberry Pi) system.
First, setup a virtual environment from a specific directory using venv:
You can pass any path as path/to/venv, just make sure you use the same one for all future steps. For more information on venv click here.
Next, install the qwiic package with:
Now you should be able to run any example or custom python scripts that have import qwiic_titan_gps by running e.g.:
If not already installed, follow the instructions here to install mpremote on your computer.
Connect a device with MicroPython installed to your computer and then install the package directly to your device with mpremote mip.
If you would also like to install the examples for this repository, issue the following mip command as well:
If not already installed, follow the instructions here to install CircUp on your computer.
Ensure that you have the latest version of the SparkFun Qwiic CircuitPython bundle.
Finally, connect a device with CircuitPython installed to your computer and then install the package directly to your device with circup.
If you would like to install any of the examples from this repository, issue the corresponding circup command from below. (NOTE: The below syntax assumes you are using CircUp on Windows. Linux and Mac will have different path seperators. See the CircUp "example" command documentation for more information)
Below is a quickstart program to print readings from the TITAN_GPS.
See the examples directory for more detailed use examples and examples/README.md for a summary of the available examples.