Qwiic_Twist_Py
Python for SFE Qwiic Twist
|
Python module for the qwiic twist, which is part of the SparkFun Qwiic Twist
This python package is a port of the existing SparkFun Qwiic Twist Arduino Library
This package can be used in conjunction with the overall SparkFun qwiic Python Package
New to qwiic? Take a look at the entire SparkFun qwiic ecosystem.
This driver package depends on the qwiic I2C driver: Qwiic_I2C_Py
The SparkFun qwiic Twist module documentation is hosted at ReadTheDocs
This repository is hosted on PyPi as the sparkfun-qwiic-twist package. On systems that support PyPi installation via pip, this library is installed using the following commands
For all users (note: the user must have sudo privileges):
For the current user:
To install, make sure the setuptools package is installed on the system.
Direct installation at the command line:
To build a package for use with pip:
A package file is built and placed in a subdirectory called dist. This package file can be installed using pip.
See the examples directory for more detailed use examples.