Arduino Print
Methods used to support Arduino Print functionality.
setCursor()
This method is called set the "cursor" position in the device. The library supports the Arduino Print interface, enabling the use of a print() and println() methods. The set cursor position defines where to start text output for this functionality.
| Parameter | Type | Description |
|---|---|---|
| x | uint8_t |
The X coordinate of the cursor |
| y | uint8_t |
The Y coordinate of the cursor |
setColor()
This method is called to set the current color of the system. This is used by the Arduino Print interface functionality
| Parameter | Type | Description |
|---|---|---|
clr |
uint8_t |
The color to set. 0 = black, > 0 = white |
getColor()
This method is called to get the current color of the system. This is used by the Arduino Print interface functionality
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The current color |