Device Operations
Methods to setup the device, get device information and change display options.
Initialization
begin()
This method is called to initialize the OLED library and connection to the OLED device. This method must be called before calling any graphics methods.
| Parameter | Type | Description |
|---|---|---|
wirePort |
TwoWire |
optional. The Wire port. If not provided, the default port is used |
address |
uint8_t |
optional. I2C Address. If not provided, the default address is used. |
| return value | bool |
true on success, false on startup failure |
reset()
When called, this method reset the library state and OLED device to their intial state. Helpful to reset the OLED after waking up a system from a sleep state.
| Parameter | Type | Description |
|---|---|---|
| return value | bool |
true on success, false on startup failure |
Geometry
getWidth()
This method returns the width, in pixels, of the connected OLED device
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The width in pixels of the connected OLED device |
getHeight()
This method returns the height, in pixels, of the connected OLED device
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The height in pixels of the connected OLED device |
Display Modes
invert()
This method inverts the current graphics on the display. This results of this command happen immediatly.
| Parameter | Type | Description |
|---|---|---|
bInvert |
bool |
true - the screen is inverted. false - the screen is set to normal |
flipVertical()
When called, the screen contents are flipped vertically if the flip parameter is true, or restored to normal display if the flip parameter is false.
| Parameter | Type | Description |
|---|---|---|
bFlip |
bool |
true - the screen is flipped vertically. false - the screen is set to normal |
flipHorizontal()
When called, the screen contents are flipped horizontally if the flip parameter is true, or restored to normal display if the flip parameter is false.
| Parameter | Type | Description |
|---|---|---|
bFlip |
bool |
true - the screen is flipped horizontally. false - the screen is set to normal |
displayPower()
Used to turn the OLED display on or off.
| Parameter | Type | Description |
|---|---|---|
bEnable |
bool |
true - the OLED display is powered on (default). false - the OLED dsiplay is powered off. |