Scrolling
Methods for device scrolling
scrollStop()
If the device is in a scrolling mode, calling this method stops the scroll, and restores the device to normal display operation. This action is performed immediately.
| Parameter | Type | Description |
|---|---|---|
| NONE |
scrollRight()
This method is called to start the device scrolling the displayed graphics to the right. This action is performed immediately.
The screen will scroll until the scrollStop() method is called.
| Parameter | Type | Description |
|---|---|---|
start |
uint8_t |
The start page address of the scroll - valid values are 0 thru 7 |
stop |
uint8_t |
The stop/end page address of the scroll - valid values are 0 thru 7 |
interval |
uint8_t |
The time interval between scroll step - values listed below |
Defined values for the interval parameter:
| Defined Symbol | Time Interval Between Steps |
|---|---|
SCROLL_INTERVAL_2_FRAMES |
2 |
SCROLL_INTERVAL_3_FRAMES |
3 |
SCROLL_INTERVAL_4_FRAMES |
4 |
SCROLL_INTERVAL_5_FRAMES |
5 |
SCROLL_INTERVAL_25_FRAMES |
25 |
SCROLL_INTERVAL_64_FRAMES |
64 |
SCROLL_INTERVAL_128_FRAMES |
128 |
SCROLL_INTERVAL_256_FRAMES |
256 |
scrollVertRight()
This method is called to start the device scrolling the displayed graphics vertically and to the right. This action is performed immediately.
The screen will scroll until the scrollStop() method is called.
| Parameter | Type | Description |
|---|---|---|
start |
uint8_t |
The start page address of the scroll - valid values are 0 thru 7 |
stop |
uint8_t |
The stop/end page address of the scroll - valid values are 0 thru 7 |
interval |
uint8_t |
The time interval between scroll step - values listed in scrollRight |
scrollLeft()
This method is called start to the device scrolling the displayed graphics to the left. This action is performed immediately.
The screen will scroll until the scrollStop() method is called.
| Parameter | Type | Description |
|---|---|---|
start |
uint8_t |
The start page address of the scroll - valid values are 0 thru 7 |
stop |
uint8_t |
The stop/end page address of the scroll - valid values are 0 thru 7 |
interval |
uint8_t |
The time interval between scroll step - values listed in scrollRight |
scrollVertLeft()
This method is called to start the device scrolling the displayed graphics vertically and to the left. This action is performed immediately.
The screen will scroll until the scrollStop() method is called.
| Parameter | Type | Description |
|---|---|---|
start |
uint8_t |
The start page address of the scroll - valid values are 0 thru 7 |
stop |
uint8_t |
The stop/end page address of the scroll - valid values are 0 thru 7 |
interval |
uint8_t |
The time interval between scroll step - values listed in scrollRight |