Skip to content

Configuration

Each BlueSMiRF v2 firmware comes with a set of AT commands to read or change the configuration. The following set of AT commands are similar to previous BlueSMiRF AT commands. Let's go over some of these commands!

AT Commands

Note

Command mode cannot be entered for 60 seconds after power-on or resetting the device. This setting can be changed with the AT-MaxCommandTimeMs command.

BlueSMiRF radios are very flexible. By default, the radio is looking for serial communication at 115200 bps. Open the terminal of your choice. Then enter $$$ and wait for an OK. Both the CONNECT and STATUS LEDs will fade in and fade out whenever the board is in Command Mode. At this point, the radio is now ready for an AT command.

Entering Command Mode

Response acknowledging user is in command mode.

Note

Depending on your serial terminal's settings, you may not see the characters that are being sent. You can try turning on the local echo to view the characters. However, keep in mind that any characters sent when the BlueSMiRF v2 is in command mode will already be echoed back.

Note

The device can also be configured by connecting over Bluetooth and entering $$$.

Below is a brief list of commands. The BlueSMiRF will recognize commands with capital and lower case letters since the commands are not case sensitive.

AT Command Command Description
$$$ Enter Command Mode
AT Reports OK
AT? Display this help text
ATA Display all settings
ATB Display Bluetooth settings
ATC Check for new firmware
ATD Display the debug settings
ATF Restore factory settings
ATM Display MAC address
ATP Start pairing process
ATS Display serial settings
ATU Update Firmware
ATV Display firmware version
ATW Save current settings to NVM
ATX Exit command mode
ATY Display system settings
ATZ Reboot the system
AT-<Param>=<value> Set parameter's value to xxx by name (Param)
AT-<Param>? Print parameter's current value by name (Param)
AT-? Display the setting values

A parameter <Param> is set using the AT- prefix, followed by the name of the command with an equals sign and the value to set. For example, sending AT-SerialSpeed=115200 followed by the Enter key (or a carriage return) will change the serial interface speed to 115200bps. This setting can be stored in NVM (non-volatile memory) by sending the ATW command.

To query a setting, send the AT command without a value and the device will respond with the current value. For example, sending AT-SerialSpeed followed by the Enter key will generate the response 115200 followed by OK.

The commands are best discussed in groups:

Bluetooth Commands

Below is a table for Bluetooth commands, a short description of the command, and its factory default value (if applicable). Right after the table, there is also a list which provides a detailed explanation of each parameter as well.

AT Command Command Description Factory Default Value
AT-BluetoothConnectRetries Number of retries of a paired connection 5
AT-BluetoothConnectTimeoutMs Milliseconds before a paired connection attempt times out 3000
AT-BluetoothEscapeCharacter The character received from the remote system, sought to enter command mode $
AT-BluetoothNickname User configurable name to broadcast over Bluetooth during discovery BlueSMiRF-ABCD, where ABCD is the last four digits of the MAC address
AT-BluetoothPairedMac MAC address of the unit that the user wants to connect to at startup
AT-BluetoothPairedName Name of the unit that the user wants to connect to at startup
AT-BluetoothPin Pin to enter during pairing - only required for older Bluetooth devices 1234
AT-BluetoothRxSize Bluetooth receive buffer size 2048
AT-BluetoothTxSize Bluetooth write buffer size 1024
AT-BluetoothType Bluetooth protocol used for communication 0
  • BluetoothConnectRetries
    If this device has a paired MAC or name, at power up it will attempt to connect to this paired device. A connection is not guaranteed, and the connection will be re-tried this number of times before going into passive, discoverable mode.
  • BluetoothConnectTimeoutMs
    When this device is connecting to a paired device, if this number of milliseconds expires before a connection is made, the device will attempt to reconnect to the paired device.
  • BluetoothEscapeCharacter
    This is the character that must be transmitted by a remote device to enter command mode remotely over the Bluetooth connection.

    Note

    Escape characters are ignored after MaxCommandTimeMs number of milliseconds and within MinEscapeTimeMs of other incoming characters.

  • BluetoothNickname
    The name that is broadcast when other devices are scanning for devices to pair to.
  • BluetoothPairedMac
    The MAC address of the BlueSMiRF that this device should pair to at power-on. Use the ATM command on the remote device to display its MAC address. This command is not normally used; use the button pairing method for an easier way to pair two devices.
  • BluetoothPairedName
    The name of the BlueSMiRF that this device should pair to at power-on. Use the BluetoothNickname command on the remote device to change its paired name. This command is not normally used; use the button pairing method for an easier way to pair two devices.
  • BluetoothPin
    The pin that is needed during pairing. Only needed on very old Bluetooth USB dongles.
  • BluetoothRxSize
    The size of the Bluetooth receive buffer. Increase if a large amount of data is coming into the BlueSMiRF over Bluetooth, before the speed of the serial interface can output it.
  • BluetoothTxSize
    The size of the Bluetooth transmit buffer. Increase if a large amount of data needs to be transmitted over Bluetooth but the connection between devices is poor and multiple retransmissions occur.
  • BluetoothType
    Controls the Bluetooth protocol. This parameter accepts a 0, 1, and 2 for the Bluetooth Protocol as listed below. Note that only the SPP protocol supports pairing.
    • Protocol 0 = Serial Port Profile (SPP)
    • Protocol 1 = Bluetooth Low-Energy (BLE)
    • Protocol 2 = Radio off

Serial Commands

Below is a table for serial commands, a short description of the command, and its factory default value (if applicable). Right after the table, there is also a list which provides a detailed explanation of each parameter as well.

AT Command Command Description Factory Default Value
AT-FlowControl Enable the use of CTS/RTS flow control signals 0
AT-InvertCts Invert the input of CTS 0
AT-InvertRts Invert the output of RTS 0
AT-PartialFrameTimeoutMs Send partial buffer if time expires 50
AT-RtsStartSendingPercent Percent of serialReceiveBuffer that is free when RTS is asserted 25
AT-RtsStopSendingPercent Percent of serialReceiveBuffer that is free when RTS is deasserted 5
AT-SerialReceiveBufferSize Serial receive buffer size 51200
AT-SerialSpeed The baud rate that the BlueSmiRF operates at. 115200
AT-SerialTransmitBufferSize Buffer size to receive bytes from Bluetooth 10240
  • FlowControl - If flow control is enabled, the BlueSMiRF v2 will send data when its CTS pin is driven low (the host system is telling the radio to transmit). If flow control is enabled, BlueSMiRF v2 will drive its RTS low if its serial buffer is full (the radio is telling the host system to hold its horses). By default, flow control is turned off.
  • InvertCts - By default, InvertCts is false and CTS is high when data is allowed to flow. Enable InvertCts to do the opposite.
  • InvertRts - By default, InvertRts is false and RTS is high when data is allowed to flow. Enable InvertRts to do the opposite.
  • PartialFrameTimeoutMs - The number of milliseconds of timeout before a partial packet is sent. For example, if a partial frame of 12 bytes is received, the radio will wait this amount for more bytes before initiating a transmission.
  • RtsStartSendingPercent - Percent of serialReceiveBuffer that is free when RTS is asserted. Default of 25% of serialReceiveBuffer.
  • RtsStopSendingPercent - Percent of serialReceiveBuffer that is free when RTS is deasserted. Default of 5% of serialReceiveBuffer.
  • SerialReceiveBufferSize - Buffer size to receive serial data from the serial port, to be sent over Bluetooth. The default is 51200.
  • SerialSpeed - The baud rate that the BlueSMiRF operates at. Discrete values 2400, 4800, 9600, 14400, 19200, 38400, 57600, 115200 (default), 230400, 460800, and 921600bps are allowed. - SerialTransmitBufferSize - Buffer size to receive bytes from Bluetooth, waiting to be printed out the UART. The default is 10240.

System Commands

Below is a table for system commands, a short description of the command, and its factory default value (if applicable). Right after the table, there is also a list which provides a detailed explanation of each parameter as well.

AT Command Command Description Factory Default Value
AT-EscapeCharacter The character sought to enter command mode $
AT-EscapeCharacterCount The number of escape characters required to enter command mode 3
AT-LedStyle Controls the behavior of the Status and Connect LEDs 0
AT-MaxCommandTimeMs After this time in milliseconds, command mode cannot be entered 60000
AT-MinEscapeTimeMs Serial traffic must stop this amount of milliseconds before an escape character is recognized 2000
AT-WiFiPassword Password for the SSID, used for over-the-air-updates
AT-WiFiSSID SSID used for over-the-air-updates
  • EscapeCharacter
    The character that must be entered a number of times (EscapeCharacterCount) to enter configuration mode. An escape character must be entered before the max time of MaxCommandTimeMs and after MinEscapeTimeMs.
  • EscapeCharacterCount
    The number of escape characters needed before command mode is entered. Set to 0 to disable.
  • LedStyle - Controls how the LEDs behave: CLASSIC = 0, SERIAL_TRAFFIC = 1, OFF = 2.
    • CLASSIC mode (default) = 0
      The STATUS LED blinks with TX/RX traffic.
    • SERIAL_TRAFFIC mode = 1
      The CONNECT LED blinks with TX traffic and the STATUS LED blinks with RX traffic.
    • OFF mode = 2
      The CONNECT and STATUS LEDs are turned off.
  • MaxCommandTimeMs
    Once this number of milliseconds has passed, command mode cannot be entered. This is used as a method to prevent a remote system from accidentally entering command mode.
  • MinEscapeTimeMs
    This number of milliseconds must pass between the last serial character received and an escape character. This is used as a method to prevent a remote system from accidentally entering command mode.
  • WiFiPassword
    The password for the local WiFi used for firmware updates.
  • WiFiSSID
    The SSID for the local WiFi used for firmware updates.