Example 2 - Pair Two BlueSMiRFs
In this example, we will connect two BlueSMiRF v2 boards to two separate serial ports. We will then send characters from one serial terminal to a second serial terminal.
The image below on the left shows the Serial Basic (CH340, USB-C) connected to the BlueSMiRF v2 Header using M/F jumper wires. Headers were used to easily remove and reconnect the BlueSMiRF v2 with headers. The image to the right shows the Serial Basic (CH340, micro-B) connected to the BlueSMiRF v2 PTH using M/F jumper wires. A row of female headers were soldered on the board. Extra long headers were placed between the female headers to easily remove and reconnect the BlueSMiRF v2 PTH as well.
USB-to-Serial Converter (CH340) to BlueSMiRF v2 Header with an Additional Stackable Header
USB-to-Serial Converter (CH340) to BlueSMiRF v2 PTH
Note
To distinguish between the two BlueSMiRFs, try labeling the two board. In this case, we chose had the one with male headers and the other one with female headers.
Connect the first BlueSMiRF v2 to your computer's COM port. In this case, it was COM13. Press and hold the PAIR button between 4 to 8 seconds. The Status and Connect LEDs will slowly blink back and forth. The Connect LED will begin to fade in and out after a few seconds. Open a serial terminal and connect to the first BlueSMiRF at 115200 baud.
First Serial Terminal
At this point, connect the second BlueSMiRF v2 to your computer's COM port. In this case, it was COM18. Press and hold the second BlueSMiRF's PAIR button between 4 to 8 seconds. The second BlueSMiRF will scan the area for another BlueSMiRF and connect. Once connected, the Connect LEDs on both boards will remain solid. Open a second serial terminal, and connect to the second BlueSMiRF at 115200 baud. Move both serial terminals side by side.
Second Serial Terminal
Start typing characters in the first serial terminal. You should see them in the second serial terminal!
Type a message in the second terminal window. You should see them in the first serial terminal!