Skip to main content

Hardware Overview

In this section, we will highlight the hardware and pins that are broken out on the SparkFun DataLogger IoT. At the time of writing, we highlighted the SparkFun DataLogger IoT - 9DoF. However, this also applies for the SparkFun DataLogger IoT.

Datalogger Iot - 9dof (Top View)

DataLogger IoT - 9DoF

The SparkFun DataLogger is pretty much the same with the exception of the following features listed below. We'll include notes highlighting the differences in each section.

  • No built - in 6DoF IMU - ISM330DHCX
  • No built - in magnetometer - MMC5983
  • The addressable RGB LED - WS2812 is replaced with the side emitting addressable RGB LED - B3DQ3BRG
  • No IMU INT2 jumper
  • No Mag INT jumper
  • Included MEAS PTH Jumper
  • The "35 / A7" PTH on the edge of the board is replace with a "5" PTH.

Datalogger IoT (Top View)

DataLogger IoT

ESP32-WROOM Module​

The DataLogger IoT is populated with Espressif's ESP32-WROOM-32E module. Espressif's ESP32 WROOM ubiquitous IoT microcontroller is a powerful WiFi, BT, and BLE MCU module that targets a wide variety of applications. For the DataLogger IoT, the firmware currently utilizes the WiFi feature.

ESP32-Wroom Highlighted On The Datalogger Iot - 9dof

ESP32 WROOM Module on the DataLogger

Power​

There are a variety of power and power-related nets broken out to connectors and through hole pads. Below list a few methods of powering the board up. There are protection diodes for the USB-C, 5V pin, and single cell LiPo battery. Power is regulated down to 3.3V for the system voltage. Depending on the settings and what is connected to the DataLogger IoT, the board can pull a minimum of 200µA in low power mode by itself.

  • USB-C
  • 5V Pin
  • Single Cell LiPo Battery
  • 3V3 Pin

USB-C and 5V​

The DataLogger IoT comes equipped with a USB type C socket which you can use to connect it to your computer to view the output and configuration through the serial terminal, or plug in a USB-C power supply. The DataLogger IoT includes the configuration channel resistors needed to tell the power supply to deliver 5V. You can use your USB-C laptop charger as the power source should you need to, even though it normally delivers a much higher voltage.

There is also a 5V power input pin. You can use this to feed in 5V power from an external source. The maximum voltage is 6.0V. The 5V pin is diode-protected and so is the USB-C power input, so it is OK to have both connected at the same time. This pin is ideal if you want to power your DataLogger from regulated solar power or a different type of power supply. You can not use the 5V pin as an output.

USB C Connector, 3.3V Voltage Regulator, 5V PTH

DataLogger IoT Power- USB-C and 5v

Voltage from the USB is regulated down to the XC6222 3.3V/700mA voltage regulators for the system voltage and Qwiic-enabled devices. USB power is also connected to the MCP73831 to charge a single cell LiPo battery at a default rate of 500mA.

For customers in North America, our NEMA Raspberry Pi Wall Adapter is a perfect choice. You can power the DataLogger IoT from our USB Battery Pack / Power Bank - TOL-15204 but you will need a USB-C cable too:

LiPo Battery Input, Charger, and Fuel Gauge​

But of course you’re going to want to use the DataLogger IoT to log sensor data while on the move too. You can connect one of our standard single cell LiPo batteries to the DataLogger IoT and power it for hours, days or weeks depending on what sensors you have attached and how often you log data.

The DataLogger IoT uses the built-in MCP73831 charger too which will charge your battery at 500mA when USB-C is connected. Please make sure your battery capacity is at least 500mAh (0.5Ah).

The board also includes the MAX17048 LiPo Fuel Gauge which allows you to determine how much power your LiPo battery has available.

The 2-pin JST connector pins are broken out to PTHs on the edge of the board if you decide to solder a single cell LiPo battery directly to the board or power another device.

Battery Polarity

Make sure that you use one of our recommended Lithium Ion batteries. Some batteries use the same JST connector as ours but have the opposite polarity. Connecting one of these to your DataLogger IoT will destroy it. If you are going to use your own battery, it is up to you to ensure it has the correct polarity.

LiPo Charger And Fuel Gauge Circuit Highlighted On The Datalogger IoT

LiPo Charger, Fuel Guage and Battery Connections

3V3 Pins​

For those going the old school route, you can also bypass the voltage regulators by soldering directly to the 3V3 and GND pin to provide power if your application has a regulated 3.3V. Note that this is only connected to the system voltage. You will also need to provide power to the 3V3 SWCH or Qwiic-enabled devices should you decide to bypass the voltage regulator.

3.3V Voltage Regulators, PTHs, and Qwiic Connectors Highlighted on the DataLogger IoT

3.3V Voltage Regulators, PTHs, and Qwiic Connectors

CH340 USB-to-Serial Converter​

The top side of the board includes a CH340 USB-to-Serial Converter. The chip can be used to send serial data between the device and computer. You can view the output or configure the device through a serial terminal.

CH340 highlighted on the DataLogger IoT

CH340 USB-to-Serial Converter IC

The driver should automatically install on most operating systems. However, there is a wide range of operating systems out there. You may need to install drivers the first time you connect the chip to your computer's USB port or when there are operating system updates. For more information, check out our How to Install CH340 Drivers Tutorial.

UART​

The hardware serial UART pins are broken out on the edge of the board. For more information about Serial UART, check out the tutorial about Serial Communication for more information.

  • TXD: UART transmit pin. This is connected to pin 16.
  • RXD: UART receive pin. This is connected to pin 17.

Uart Pins Highlighted On The Datalogger Iot

UART Pins Highlighted On The DataLogger IoT

Qwiic​

SparkFun's Qwiic Connect System uses 4-pin JST style connectors to quickly interface development boards with I2C sensors and more. No soldering required and there's no need to worry about accidentally swapping the SDA and SCL wires. The Qwiic connector is polarized so you know you’ll have it wired correctly every time, right from the start. Qwiic boards are daisy chain-able too so you can connect multiple sensors to the DataLogger IoT and log readings from all of them.

Vertical qwiic Connector

You may notice a thin film over the vertial Qwiic connector. This is used by a pick-and-place machine when populating the component on the board before it goes through the reflow oven. Remove this film before using the vertical qwiic connector

The board is populated with vertical and horizontal Qwiic connectors. These are also broken out to PTHs on the edge of the board.

Qwiic Connector And I2C PTH Highlighted

Qwiic Connector And I2C PTH Highlighted

PinDescription
SCLI2C clock pin. This is connected to pin 22 and a 2.2kΩ pull-up resistor.
SDAI2C data pin. This is connected to pin 21 and a 2.2kΩ pull-up resistor.
3V3 SWThe 3.3v pin is connected to the XC6222 voltage regulator's output to power the Qwiic devices.
GNDCommon, ground voltage (0V reference) for the system

Connected to the line I2C line is the MAX17048 LiPo fuel gauge (7-bit unshifted address = 0x36).

Sometimes you might want to connect more than one of the same type of sensor to the DataLogger IoT. On the I2C bus, each device needs to have a unique address. On many of our boards, there are jumpers links which you can use to change the address and some have addresses that can be configured in software. But there are some where you cannot change the address. Typically, one would use a multiplexor. However, we currently do not have the DataLogger IoT configured to work with any multiplexors (i.e. Qwiic Mux Breakout).

The DataLogger IoT includes a dedicated 3.3V regulator for the Qwiic connector. This has several advantages including:

  • The DataLogger IoT can completely power-down the I2C sensors during sleep to prolong your battery life
  • There’s no risk of the Qwiic bus gulping too much current and causing problems for the ESP32

SPI​

The SPI pins are broken out on the edge of the board. For those that are unfamiliar to PICO and POCI, check out the SPI tutorial for more information.

PinDescription
SCKSPI clock pin. This is connect to pin 18.
PICOSPI Peripheral In Controller Out. This is connected to pin 23.
POCISPI Peripheral Out Controller In. This is connected to pin 19.

SPI Pins Highlighted on the Datalogger IoT

SPI Pins Highlighted

Not shown in the image are the chip select (CS) pins. The 6DoF IMU's CS pin is connected to pin 5. The magnetometer's CS pin is connected to pin 27 which is not broken out.

On the DataLogger IoT, the IMU and magnetometer are not connected to the SPI port since they are not included on the board. Instead of pin "35 / A7" being broken out, pin "5" is broken out on the edge of the board.

Pin 5 highlighted on the DataLogger IoT Pin 5 Highlighted on the DataLogger IoT

MicroSD Card Socket​

The DataLogger IoT supports full 4-bit SDIO for fast logging and uses common microSD cards to record clear text, comma separated files. Flip over the DataLogger IoT and you'll see the latching microSD card socket. You probably already have a microSD card laying around. However, if you need any additional units, we have plenty in the SparkFun catalog. The DataLogger can use any size microSD card and supports FAT32 cards in addition to FAT16. Please ensure that your SD card is formatted correctly; we recommend the Raspberry Pi Imager Tool.

MicroSD Card

MicroSD Card

Slide in your formatted SD card and it will click neatly into place. The edge of the SD card will stick out on the edge of the circuit board when it is inserted correctly.

You should only insert or remove the SD card while the power is turned off or disconnected. Removing the card while the DataLogger IoT is logging will almost certainly corrupt your data.

DataLogger IoT - 9DoF (9 Degrees of Freedom)​

As stated earlier, included on every DataLogger IoT - 9DoF is a 6DoF Inertial Measurement Unit (IMU) for built-in logging of triple-axis accelerometer and gyro. There is also a built-in triple-axis magnetometer for a complete 9 degrees of freedom. Beside each IC is a silkcreen showing the reference axis. Both are connected to the ESP32 via the SPI port. Combined, you have 9 degrees of inertial measurement! Whereas the original 9DOF Razor used the old MPU-9250, this uses the ISM330DHCX and MMC5983MA. Oh, and if that wasn’t enough, it comes with a built-in temperature sensor on each IC too. So if you want to use the DataLogger IoT as a transportation logger, it will do that straight out of the anti-static bag!

Accelerometer, Gyro, and Magnetometer

DataLogger IoT - 9DOF - Accelerometer, Gyro, and Magnetometer

Analog Pins​

There are three 12-bit analog pins available and broken out on edge of the board.

PinDescription
36 / A0Analog A0. This is connected to pin 36.
39 / A3Analog A3. This is connected to pin 39.
35 / A7Analog A7. This is connected to pin 35.

Analog Pins Highlighted on the DataLogger IoT

Analog Pins Highlighted

Reset and Boot Buttons​

There are two buttons available on the board for reset and boot. These are also broken out on the edge of the board as PTHs. If you have your DataLogger IoT mounted in an enclosure, you can also attach an external boot or reset switch too. Any Single Pole Normally-Open Push-To-Close momentary switch will do. Solder pin headers or wires to the RST and GND breakout pins and connect your external switch to those.

ButtonDescription
RESETPressing this button will pull the pin LOW and reset the program running on the ESP32 without unplugging the board.
BOOTThe boot button usually allows users to force the ESP32 into bootloader mode to manually flash new firmware to the ESP32. The ESP32 will remain in this mode until there is a power cycle or the reset button is pressed. As of firmware v01.00.02, this button has an extra function: pressing down on the user button for 20 seconds will erase on-board preference storage and restart the board. This is connected to pin 0 on the ESP32.

Reset and Boot Buttons (and Associated PTHs) Highlighted on the DataLogger IoT

Reset and Boot Buttons (and Associated PTHs) Highlighted

note

You may notice a thin film over buttons. This is used by a pick-and-place machine when populating the component on the board before it goes through the reflow oven. This can be removed.

Like other ESP32 development boards, these buttons are populated so that users can place the ESP32 module in bootloader mode. For users that need to place the board in bootloader mode when powered, you will need to:

  1. Press the BOOT button.
  2. While holding on the BOOT button, press the RESET button momentarily.
  3. Finally, release the BOOT button.

Most of the time, users will simply have the board executing the firmware that is loaded on the ESP32 module and updating through the configuration menu either through the microSD card or OTA.

Overwriting the Build-In Firmware​

Please think very carefully before uploading any Arduino sketches to your DataLogger IoT.

Uploading Arduino Sketches

You will overwrite the DataLogger IoT firmware, leaving it unable to update or restore itself.

The DataLogger IoT comes pre-programmed with amazing firmware which can do so much. It is designed to be able to update itself and restore itself if necessary. But it can not do that if you overwrite the firmware with any Arduino sketch. It is just like erasing the restore partition on your computer hard drive. Do not do it - unless you really know what you are doing.

LEDs​

There are three LEDs populated on the board. These can be disabled with their respective jumpers on the back of the board.

LEDDescription
STATThe status LED is connected to pin 25.
RGBThe WS2812-2020 RGB addressable LED is connected to pin 26. In addition to being disabled through the jumper on the back, you can also disable the LED through software.
CHGThe on-board yellow CHG LED can be used to get an indication of the charge status of your battery. Below is a table of other status indicators depending on the state of the charge IC.

RGB LED Color Values​

The following colors represent different states that the board is in.

ColorDescription
WhiteA solid white LED indicates that the board is currently being configured through the configuration menu.
GreenA solid green LED indicates that the board is initializing. As of firmware v01.00.02, the LED blinks green when on battery power indicating that the battery level is VBATT > 50%.
BlueA blinking blue LED indicates that the board is reading sensor data and logging the values.
YellowA solid yellow LED indicates that a firmware update is in progress. As of firmware v01.00.02, the LED blinks yellow when on battery power indicating that the battery level is between 50% > VBATT > 10%.
RedAs of firmware v01.00.02, the LED blinks red when on battery power indicating that the battery level is VBATT < 10%.

Charge LED Values​

StateLED Status
No BatteryOff
ShutdownOff - may flicker
ChargingOn
Charge CompleteOff

LEDs

LEDs and PTHs Connected to LEDs

Jumpers​

There are seven jumpers on the back of the DataLogger IoT - 9DoF. For more information, check out our tutorial on working with jumper pads and PCB traces should you decide to cut the traces with a hobby knife.

JumperDescription
SHLDThis jumper connects the USB Type C connector's shield pin to GND. Cut this to isolate the USB Type C connector's shield pin.
I2CThis three way jumper labeled as I2C are closed by default. By cutting the jumpers, it will disconnect the 2.2kΩ pull-up resistors for the I2C
STATThis jumper connects the status LED to pin 25 and it is closed by default. Open the jumper to disable the LED.
RGBThis jumper connects the WS2812-2020 RGB addressable LED to pin 26 and it is closed by default. Open the jumper to disable the LED.
CHG*This jumper connects the charge LED on the MCP73831 charge IC and it is closed by default. Open the jumper to disable the LED.
IMU INT2This jumper connects the ISM330DHCX IMU's interrupt pin to pin 35 and it is open by default. Add a solder jumper to connect.
MAG INTThis jumper connects the MMC5983MA magnetometer's interrupt pin to pin 35 and it is open by default. Add a solder jumper to connect.

Jumpers

Jumper Locations

On the DataLogger IoT, the IMU INT2 or MAG INT jumpers are not included since it does not have the built in 6DoF IMU or magnetometer. With the extra real estate on the board, we were able to include a MEAS PTH and jumper on the board. By default, the jumper is closed. You can cut this jumper on the bottom side of the board to measure the DataLogger IoT’s current draw from external power.

Meas jumper on the datalogger iot

Measurment Jumpers

Board Dimensions​

The overall length and width with the antenna connector is about 1.66" x 2.00". There are four mounting holes in the center of the board. Due to the size of the board and the ESP32 module, the mounting holes are positioned in a way for users to add two Qwiic enabled boards with a width of 1.0" instead of one Qwiic board.

DataLogger IoT Board Dimensions

DataLogger IoT Board Dimensions