Skip to content

Interrupt Trigger

This option is used to setup an external interrupt as a trigger for a logging event. By connecting an external device that will trigger an interrupt to a GPIO pin on the DataLoggerIoT, an external device can cause an log event to occur.

When this menu item is selected, the following settings menu is displayed:

Logging Interrupt Menu

Logger Interrupt Menu Options

Settings

The settings for this feature are the following:

Enabled

Use this setting to enable/disable this functionality

Event Name

A string that represents the "name" of the logging event. This name can be displayed using the "event source" option of the Logger.

Interrupt Pin

The DataLoggerIoT GPIO Pin to use to detect the external interrupt. Valid pins are: 33 and 36 and selected in the options menu.