Hardware Overview

Introduction
-
SparkPNT GNSS Flex Module - LG290P & IM19 IMU
SKU: GPS-29469
Tilt Compensation
The IM19 attitude module from Feyman (FMI) fuses MEMS IMU sensor data and GNSS RTK positioning to deliver high-precision attitude compensated measurements, with roll and pitch accurate to within 0.05 degrees. This kind of superb accuracy has widespread uses in industrial applications such as tilt RTK surveys (where RTK poles need not be held straight vertical as the IM19 can calculate a virtual digital level at any tilt angle), agriculture machine automation, and dead reckoning.
When configured, fed with the LG290P Pulse-Per-Second signal and NMEA GGA, RMC, and GST messages; once calibrated, the IM19 will output proprietary NMEA messages containing the compensated position and roll, pitch and yaw. By default, the LG290P
COM3TXis linked to the IM19UART2RXto carry the required NMEA messages. However, this can be changed via jumper links on the Flex Module, if necessary. -
SparkPNT GNSS Flex modules are plug-in boards featuring different GNSS receivers. They are designed to be easily swapped for repairs and pin-compatible for upgrades. The boards have two 2x10-pin, 2mm pitch female headers connecting to carrier boards. For the LG290P GNSS receiver, these pins will break out the UART (x2) and I2C* interfaces, along with the PPS and event signals using a standardized pinout. Additionally, these pins break out the two UART interfaces of the IM19 IMU.
This SparkPNT GNSS Flex module combines the Quectel LG290P GNSS receiver with the IM19 Inertial Measurement Unit for tilt compensation or dead reckoning. The LG290P module is a quad-band, multi-constellation, high-precision, RTK GNSS receiver. The module can simultaneously receive signals from the
L1,L2,L5, andL6/E6frequency bands of the GPS, GLONASS, Galileo, BDS, QZSS, and NavIC GNSS constellations. In addition, the module supports SBAS augmentation systems (WASS, EGNOS, BDSBAS, MSAS, GAGAN, and SDCM), PPP services* (BDS PPP-B2b, QZSS CLAS, MADOCA-PPP, and Galileo HAS), RTCM, and RTK corrections for precision navigation with a fast convergence time and reliable performance.The built-in NIC anti-jamming unit provides professional-grade interference signal detection and elimination algorithms, effectively mitigating multiple narrow-band interference sources and significantly improving signal reception performance in complex electromagnetic environments. Additionally, the embedded algorithms ensure reliable positioning in complex scenarios such as urban environments and deep tree cover.
Features Under Development
- I2C/SPI - Currently, only the UART interface is supported by the module.
- PPP Services - Corrections for some of the PPP services have not been implemented.
Design Files
-
Design Files
- Schematic
- KiCad Files
- STEP File
- Board Dimensions:
- 1.75" x 1.25" (44.45mm x 31.75mm)
-
Manipulate 3D Model
Controls Mouse Touchscreen Zoom Scroll Wheel 2-Finger Pinch Rotate Left-Click & Drag 1-Finger Drag Move/Translate Right-Click & Drag 2-Finger Drag
Dimensions of the LG290P GNSS Flex module. Need more measurements?
For more information about the board's dimensions, users can download the KiCad files for this board. These files can be opened in KiCad and additional measurements can be made with the measuring tool.
KiCad - Free Download!
KiCad is free, open-source CAD program for electronics. Click on the button below to download their software. (*Users can find out more information about KiCad from their website.)
Measuring Tool
This video demonstrates how to utilize the dimensions tool in KiCad, to include additional measurements:
Board Layout
The GNSS Flex system is designed around two 2x10-pin, 2mm pitch headers used mate the two types of boards. A standardized pin layout, keeps the ecosystem pin-compatible for upgrades and allows board to be easily swapped for repairs. Depending on the capabilities of the GNSS receiver, these pins will breakout the USB, UART (x4), I2C, and SD card interfaces along with any PPS or event signals of the GNSS receiver.
The LG290P GNSS Flex module has the following features:
-
- LG290P GNSS Receiver
- The Quectel LG290P GNSS receiver
-
- GNSS Flex Headers
- Two sets of 2x10 pin, 2mm pitch female headers for connecting a GNSS Flex module to carrier boards
-
- IM19 IMU (optional)
- An optional Feyman IM19 attitude module to provide tilt compensation in surveying applications
-
Antenna L1/L2/L5/E6U.FL Connector- An U.FL connector for attaching an external GNSS antenna
LG290P GNSS Receiver
One of the centerpieces of the GNSS Flex module, is the LG290P GNSS receiver from Quectel. The LG290P is a low-power, multi-band, multi-constellation GNSS receiver capable of delivering centimeter-level precision at high update rates. The built-in NIC anti-jamming unit provides professional-grade interference signal detection and elimination algorithms, which effectively mitigate against multiple narrow-band interference sources and significantly improves the signal reception performance in complex electromagnetic environments. With its performance advantages of high-precision and power consumption, this board is an ideal choice for high-precision navigation applications, such as intelligent robots, UAVs, precision agriculture, mining, surveying, and autonomous navigation.
Features:
- Supply Voltage: 3.15–3.45V
- Tracking Channels: 1040
- Concurrent signal reception: 5 + QZSS
L1,L2,L5,E6frequency bands
- Sensitivity:
- Acquisition: -146dBm
- Tracking: -160dBm
- Reacquisition: -155dBm
- Antenna Power: External or Internal
- GNSS Constellations and SBAS Systems:
- USA: GPS + WASS
- Russia: GLONASS + SDCM
- EU: Galileo + EGNOS
- China: BDS + BDSDAS
- Japan: QZSS + MSAS
- India: NavIC + GAGAN
- Accuracy of 1PPS Signal: 5ns (RMS)
- Update Rate:
- Default: 10Hz
- Max: 20Hz
- Time to First Fix (without AGNSS):
- Cold Start: 28s
- Warm Start: 28s
- Hot Start: 1.7s
- RTK Convergence Time: 5s
- Dynamic Performance:
- Maximum Altitude: 10000m
- Maximum Velocity: 490m/s
- Maximum Acceleration: 4g
- Built-in NIC anti-jamming unit
- Interfaces
- Operating temperature: -40°C to +85°C
Power Consumption
The power consumption of the LG290P GNSS receiver depends on the GNSS signals enabled and the positioning mode.
| Mode | Power (mW) | Current (mA) |
|---|---|---|
| Acquisition | 300.3 | 91 |
| Tracking | 300.3 | 91 |
| Backup | 39.6 | 0.012 |
Power Modes
- Acquisition:
- Module searches for satellites and to determine visible satellites, coarse frequency, and the code phase of satellite signals
- Tracking:
- Once acquisition is completed, the module tracks satellites and demodulates the navigation data from specific satellites
- Backup Mode:
- Reduces power consumption. Only backup domain is active and keeps track of time.
Frequency Bands
The LG290P module is a multi-band, multi-constellation GNSS receiver. Below, is a chart illustrating the frequency bands utilized by all the global navigation satellite systems; along with a list of the frequency bands and GNSS systems supported by the LG290P GNSS receiver.
Frequency bands of the global navigation satellite systems. (Source: Tallysman)
Supported Frequency Bands:
Supported GNSS Constellations:
- GPS (USA)
- GLONASS (Russia)
- Galileo (EU)
- BDS (China)
- QZSS (Japan)
- NavIC (India)
Supported SBAS Systems:
- WASS (USA)
- SDCM (Russia)
- EGNOS (EU)
- BDSBAS (China)
- MSAS (Japan)
- GAGAN (India)
Info
For a comparison of the frequency bands supported by the LG290P GNSS receivers, refer to sections 1.2, 1.5, and 1.6 of the hardware design manual.
What are Frequency Bands?
A frequency band is a section of the electromagnetic spectrum, usually denoted by the range of its upper and lower limits. In the radio spectrum, these frequency bands are usually regulated by region, often through a government entity. This regulation prevents the interference of RF communication; and often includes major penalties for any interference with critical infrastructure systems and emergency services.
However, if the various GNSS constellations share similar frequency bands, then how do they avoid interfering with one another? Without going too far into detail, the image above helps illustrate some of the characteristics, specific to the frequency bands of each system. With these characteristics in mind, along with other factors, the chart can help users to visualize how multiple GNSS constellations might co-exist with each other.
For more information, users may find these articles of interest:
Position Accuracy
The accuracy of the position reported from the LG290P GNSS receiver, can be improved based upon the correction method being employed. Currently, RTK corrections provide the highest level of accuracy; however, users should be aware of certain limitations of the system:
- RTK technique requires real-time correction data from a reference station or network of base stations.
- RTK corrections usually come from RTCM messages that are signal specific (i.e. an RTK network may only provide corrections for specific signals; only
E5band notE5a).
- RTK corrections usually come from RTCM messages that are signal specific (i.e. an RTK network may only provide corrections for specific signals; only
- The range of the base stations will vary based upon the method used to transmit the correction data.
- The reliability of RTK corrections are inherently reduced in multipath environments.
| Correction Method | Horizontal | Vertical | Velocity |
|---|---|---|---|
| Standalone | 0.7m ~2.3' |
2.5m ~8.2' |
3cm/s (0.108kph) ~1.2in/s (0.067mph) |
| RTK | 0.8cm (+1ppm) ~0.3" |
1.5cm (+1ppm) ~.6" |
IM19 Attitude Module
When configured and calibrated, the IM19 attitude module can fuses IMU sensor and GNSS RTK positioning data to deliver compensated position. The accuracy, displayed in the table below, should also be considered when implemented.
| Tilt Angle | Accuracy |
|---|---|
| 0° - 30° | 1cm |
| <60° | 2cm |
RTK Corrections
To understand how RTK works, users will need a more fundamental understanding of the signal error sources.
Tip
For the best performance, we highly recommend that users configure the module to utilize/provide RTK corrections with a compatible L1/L2/L5/L6 GNSS antenna and utilize a low-loss cable.
IM19 IMU (Optional)
The other centerpiece of the GNSS Flex module is the IM19 attitude module from Feyman Inc., which fuses MEMS sensor and GNSS RTK positioning data to deliver high-precision attitude measurement, with roll and pitch accurate to within 0.05 degrees. This kind of superb accuracy has widespread uses in industrial applications such as tilt RTK surveys (where RTK poles need not be held straight vertical as the IM19 can calculate a virtual digital level at any tilt angle), agriculture machine automation, and dead reckoning.
When configured, fed with the LG290P Pulse-Per-Second signal and NMEA GGA, RMC, and GST messages; once calibrated, the IM19 will output proprietary NMEA messages containing the compensated position and roll, pitch and yaw. By default, the LG290P COM3 TX is linked to the IM19 UART2 RX to carry the required NMEA messages. However, this can be changed via jumper links on the Flex Module, if necessary.
Features:
- Self-calibration Technique
- Initialization: <2s
- Power: 0.33W
- Data Rate: 100Hz
- Attitude Accuracy: ±0.05° (Pitch/Roll)
- Heading Accuracy: ±0.5° (Yaw)
- Gyroscope
- Bias Stability: ±0.2°/s
- Range: ±1000°/s
- Accelerometer
- Bias Stability: ±5mg
- Range: ±8g
Info
Please refer to the hookup guide linked below, for the operation of the IM19 attitude module in tilt-compensation applications:
Position Accuracy
When configured and calibrated, the IM19 attitude module can fuses its IMU sensor data with the received GNSS RTK positioning data to deliver a tilt compensated position.
| Tilt Angle | Accuracy |
|---|---|
| 0° - 30° | 1cm |
| <60° | 2cm |
LG290P GNSS Receiver
The accuracy of the position reported from the LG290P GNSS receiver, can be improved based upon the correction method being employed. Currently, RTK corrections provide the highest level of accuracy. Its accuracy, displayed in the table below, should also be considered when implemented.
| Correction Method | Horizontal | Vertical | Velocity |
|---|---|---|---|
| Standalone | 0.7m ~2.3' |
2.5m ~8.2' |
3cm/s (0.108kph) ~1.2in/s (0.067mph) |
| RTK | 0.8cm (+1ppm) ~0.3" |
1.5cm (+1ppm) ~.6" |
GNSS Flex Headers
The GNSS Flex system is designed around two 2x10-pin, 2mm pitch headers used mate the two types of boards. A standardized pin layout, keeps the ecosystem pin-compatible for upgrades and allows boards to be easily swapped for repairs. For the LG290P GNSS receiver, these pins will breakout the UART (x2) and I2C interfaces along with a PPS, event, and LED status indication signals from the GNSS receiver. Additionally, these pins break out the two UART interfaces of the IM19 attitude module.
Below, are the features that are available from the LG290P GNSS receiver.
Supported Interfaces:
- One of the three UART ports is piped to the IM19 module
Below, are the features that are available from the IM19 attitude module.
Supported Interfaces:
- UART (x2)
- Timing Signal (1)
- The timing signal comes from the LG290P GNSS receiver
The headers of the GNSS Flex system supports up to four UART ports. On this GNSS Flex module, these are connected to both the GNSS receiver and IM19 attitude module.
LG290P
The LG290P GNSS receiver has three UART ports, which can be operated and configured separately.
- The
UART1andUART2ports of the LG290P GNSS receiver are broken out to the headers of the GNSS Flex system. These can be used to interact with the LG290P. - The
TXpin of theUART3port from the LG290P GNSS receiver is piped directly to theRXpin of the IM19 attitude module'sUART2port.
Default Configuration
By default, the UART ports are configured with the following settings:
- Baudrate: 460800bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
- Flow Control: None
- Protocols:
NMEA 0183RTCM 3.x
| LG290P | Pins of GNSS Flex Headers |
|---|---|
UART1 |
TXD1/RXD1 |
UART2 |
TXD2/RXD2 |
UART Protocols
UART Protocols
By default, these UART ports are configured to transmit and receive NMEA 0183, RTCM 3.x, and/or QGC messages. These messages are generally used for transmitting PNT data; providing or receiving RTK corrections; and receiving PPP data, respectively. Quectel also implements a system of proprietary messages (PQTM) for users to configure the LG290P that follows a data format similar to the NMEA protocol. The expected structure of these proprietary messages is shown below:
A full list of compatible NMEA 0183 v4.11 messages, is provided in section 2.2. Standard Messages of the GNSS Protocol Specification manual. This protocol is used for outputting GNSS data, as detailed by the National Marine Electronics Association organization.
List of Standard NMEA Messages
| Message | Type Mode | Message Description |
|---|---|---|
| RMC | Output | Recommended Minimum Specific GNSS Data |
| GGA | Output | Global Positioning System Fix Data |
| GSV | Output | GNSS Satellites in View |
| GSA | Output | GNSS DOP and Active Satellites |
| VTG | Output | Course Over Ground & Ground Speed |
| GLL | Output | Geographic Position – Latitude/Longitude |
| GBS | Output | GNSS Satellite Fault Detection |
| GNS | Output | GNSS Fix Data |
| GST | Output | GNSS Pseudorange Error Statistics |
| ZDA | Output | UTC Time & Date |
| HDT | Output | True Vessel Heading |
| THS | Output | True, Heading, and Status |
A full list of PQTM messages (proprietary NMEA messages defined by Quectel) supported by LG290P, is provided in section 2.3. PQTM Messages of the GNSS Protocol Specification manual. This protocol is used to configure or read the settings for the LG290P GNSS receiver.
List of Proprietary Quectel Messages
| Message | Type Mode | Message Description |
|---|---|---|
| PQTMVER | Output | Outputs the firmware version |
| PQTMCOLD | Command | Performs a cold start |
| PQTMWARM | Command | Performs a warm start |
| PQTMHOT | Command | Performs a hot start |
| PQTMSRR | Command | Performs a system reset and reboots the receiver |
| PQTMUNIQID | Command | Queries the module unique ID |
| PQTMSAVEPAR | Command | Saves the configurations into NVM |
| PQTMRESTOREPAR | Command | Restores the parameters configured by all commands to their default values |
| PQTMVERNO | Command | Queries the firmware version |
| PQTMCFGUART | Set/Get | Sets/gets the UART interface |
| PQTMCFGPPS | Set/Get | Sets/gets the PPS feature |
| PQTMCFGPROT | Set/Get | Sets/gets the input and output protocol for a specified port |
| PQTMCFGNMEADP | Set/Get | Sets/gets the decimal places of standard NMEA messages |
| PQTMEPE | Output | Outputs the estimated position error |
| PQTMCFGMSGRATE | Set/Get | Sets/gets the message output rate on the current interface |
| PQTMVEL | Output | Outputs the velocity information |
| PQTMCFGGEOFENCE | Set/Get | Sets/gets geofence feature |
| PQTMGEOFENCESTATUS | Output | Outputs the geofence status |
| PQTMGNSSSTART | Command | Starts GNSS engine |
| PQTMGNSSSTOP | Command | Stops GNSS engine |
| PQTMTXT | Output | Outputs short text messages |
| PQTMCFGSVIN | Set/Get | Sets/gets the Survey-in feature |
| PQTMSVINSTATUS | Output | Outputs the Survey-in status |
| PQTMPVT | Output | Outputs the PVT (GNSS only) result |
| PQTMCFGRCVRMODE | Set/Get | Sets/gets the receiver working mode |
| PQTMDEBUGON | Command | Enables debug log output |
| PQTMDEBUGOFF | Command | Disables debug log output |
| PQTMCFGFIXRATE | Set/Get | Sets/gets the fix interval |
| PQTMCFGRTK | Set/Get | Sets/gets the RTK mode |
| PQTMCFGCNST | Set/Get | Sets/gets the constellation configuration |
| PQTMDOP | Output | Outputs dilution of precision |
| PQTMPL | Output | Outputs protection level information |
| PQTMCFGODO | Set/Get | Sets/gets the odometer feature |
| PQTMRESETODO | Command | Resets the accumulated distance recorded by the odometer |
| PQTMODO | Output | Outputs the odometer information |
| PQTMCFGSIGNAL | Set/Get | Sets/gets GNSS signal mask |
| PQTMCFGSAT | Set/Get | Sets/gets GNSS satellite mask |
| PQTMCFGRSID | Set/Get | Sets/gets the reference station ID |
| PQTMCFGRTCM | Set/Get | Sets/gets RTCM |
| PQTMCFGSBAS | Set/Get | Configures SBAS |
| PQTMCFGNMEATID | Set/Get | Configures the NMEA Talker ID |
| PQTMTAR | Output | Outputs the time and attitude |
| PQTMCFGBLD | Set/Get | Configures the baseline distance |
| PQTMCFGRTKSRCTYPE | Set/Get | Configures RTK differential source type |
| PQTMSN | Command | Reads the SN of module |
| PQTMCFGANTINF | Set/Get | Configures the antenna information |
| PQTMCFGANTDELTA | Set/Get | Configures the delta between antennas |
| PQTMCFGSIGGRP | Set/Get | Configures the GNSS signal group |
| PQTMCFGSIGNAL2 | Set/Get | Configures GNSS signal mask for second antenna |
| PQTMCFGGEOSEP | Set/Get | Configures geoidal separation |
| PQTMCFGCNRTHD | Set/Get | Configures the CNR threshold for position engine |
| PQTMCFGELETHD | Set/Get | Configures the elevation threshold for position engine |
| PQTMNAV | Output | Outputs the navigation information |
| PQTMEOE | Output | Outputs the end of epoch information |
| PQTMCFGWN | Set/Get | Configures the reference start week number |
| PQTMANTENNASTATUS | Output | Reports the antenna status |
A full list of QGC messages (proprietary protocol defined by Quectel) supported by LG290P, is provided in section 3. QGC Protocol of the GNSS Protocol Specification manual. This protocol is used to output the PPP raw data.
List of Proprietary Quectel Messages
| GQC Message Name | Message Group | Message Number | Type | Description |
|---|---|---|---|---|
| RAW-PPPB2B | 0x0A | 0xB2 | Output | BDS PPPB2B binary raw messages |
| RAW-QZSSL6 | 0x0A | 0xB6 | Output | QZSSL6 binary raw messages |
| RAW-HASE6 | 0x0A | 0xE6 | Output | Galileo HASE6 binary raw messages |
A full list of compatible RTCM v3 messages, is provided in section 4. RTCM Protocol of the GNSS Protocol Specification manual. This protocol is used for transferring GNSS raw measurement data, as detailed by the Radio Technical Commission for Maritime Services organization.
List of Supported RTCMv3 (MSM) Messages
| Message | Type Mode | Message Description |
|---|---|---|
| 1005 | Input/Output | Stationary RTK Reference Station ARP |
| 1006 | Input/Output | Stationary RTK Reference Station ARP with height |
| 1019 | Input/Output | GPS Ephemerides |
| 1020 | Input/Output | GLONASS Ephemerides |
| 1041 | Input/Output | NavIC/IRNSS Ephemerides |
| 1042 | Input/Output | BDS Satellite Ephemeris Data |
| 1044 | Input/Output | QZSS Ephemerides |
| 1046 | Input/Output | Galileo I/NAV Satellite Ephemeris Data |
| 1073 | Input/Output | GPS MSM3 |
| 1074 | Input/Output | GPS MSM4 |
| 1075 | Input/Output | GPS MSM5 |
| 1076 | Input/Output | GPS MSM6 |
| 1077 | Input/Output | GPS MSM7 |
| 1083 | Input/Output | GLONASS MSM3 |
| 1084 | Input/Output | GLONASS MSM4 |
| 1085 | Input/Output | GLONASS MSM5 |
| 1086 | Input/Output | GLONASS MSM6 |
| 1087 | Input/Output | GLONASS MSM7 |
| 1093 | Input/Output | Galileo MSM3 |
| 1094 | Input/Output | Galileo MSM4 |
| 1095 | Input/Output | Galileo MSM5 |
| 1096 | Input/Output | Galileo MSM6 |
| 1097 | Input/Output | Galileo MSM7 |
| 1113 | Input/Output | QZSS MSM3 |
| 1114 | Input/Output | QZSS MSM4 |
| 1115 | Input/Output | QZSS MSM5 |
| 1116 | Input/Output | QZSS MSM6 |
| 1117 | Input/Output | QZSS MSM7 |
| 1123 | Input/Output | BDS MSM3 |
| 1124 | Input/Output | BDS MSM4 |
| 1125 | Input/Output | BDS MSM5 |
| 1126 | Input/Output | BDS MSM6 |
| 1127 | Input/Output | BDS MSM7 |
| 1133 | Input/Output | NavIC/IRNSS MSM3 |
| 1134 | Input/Output | NavIC/IRNSS MSM4 |
| 1135 | Input/Output | NavIC/IRNSS MSM5 |
| 1136 | Input/Output | NavIC/IRNSS MSM6 |
| 1137 | Input/Output | NavIC/IRNSS MSM7 |
IM19
The IM19 attitude module has two UART ports, which operate separately.
- The
UART1port of the IM19 module is broken out to the headers of the GNSS Flex system, on pinsTXD3andRXD3. These pins should be used to configure the IM19 module. - The
UART2port of the IM19 module is used to receive GNSS data from the GNSS receiver and output the tilt compensated data.- By default, the
RXpin receives data from theUART3port of the LG290P GNSS receiver.- Users can modify the jumpers on the top of the GNSS Flex module, to utilize the
TXD1,TXD2, orRXD4pins (of the GNSS Flex headers) instead.
- Users can modify the jumpers on the top of the GNSS Flex module, to utilize the
- Once IM19 module is configured and calibrated, the
TXpin outputs the tilt compensated data to theTXD4pin on the GNSS Flex headers.
- By default, the
Default Configuration
By default, the UART ports are configured with the following settings:
- Baudrate: 115200bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
- Flow Control: None
- Protocols:
- AT Commands
- Proprietary Data Formats
- MEMS Raw data protocol
- GNSS Raw data protocol
- Binary NAVI positioning data protocol
| IM19 | Pins of GNSS Flex Headers |
|---|---|
UART1 |
TXD3/RXD3 |
UART2 |
TXD4 |
From the module, the PPS output signal is a 3.3V signal output. In order to receive tilt-compensated data from the IM19 attitude module, this pin needs to be configured to provide a timing pulse at the same rate as the PVT solutions.
The RTK pin operates as both the RTK_LED status indicator for the RTK positioning and ANT_ON power control for the external LNA or active antenna power.
RTK_LED pin on the LG290P GNSS Flex module.
In this configuration, the pin is set to a high level at startup.
- If the pin output is high, it indicates the module has entered the RTK fixed mode.
- If the pin output is low, it indicates that the module exited the RTK fixed mode.
- If the pin outputs an alternating pin level, it indicates that the module received the correct RTCM data and did not enter the RTK fixed mode.
In this configuration, the pin is used to control the external LNA or active antenna power supply.
- When the pin is high, the antenna is powered.
- When the pin is low, the antenna is not powered.
U.FL Connector
Users will need to connect a compatible GNSS antenna to the Antenna L1/L2/L5/E6 U.FL connector. The type of antenna used with the LG290P module affects the overall accuracy of the positions calculated by the GNSS receiver.
- Passive antennas are not recommended for the LG290P GNSS receiver.
- To mitigate the impact of out-of-band signals, utilize an active antenna whose SAW filter is placed in front of the LNA in the internal framework.
- DO NOT select an antenna with the LNA placed in the front.
- There is no need to inject an external DC voltage for the GNSS antenna. Power is already provided from the LG290P module for the LNA of an active antenna.
The U.FL connector to attach an external GNSS antenna to the LG290P GNSS Flex module.
Tip
For the best performance, we recommend users choose a compatible L1/L2/L5/E6 GNSS antenna and utilize a low-loss cable. Also, don't forget that GNSS signals are fairly weak and can't penetrate buildings or dense vegetation. The GNSS antenna should have an unobstructed view of the sky.
Jumpers
The are four jumpers on top of the LG290P GNSS Flex module that can be modified to change the source of the GNSS data for the IM19 attitude module.
Never modified a jumper before?
Check out our Jumper Pads and PCB Traces tutorial for a quick introduction!
-
Feature Under Development
Currently, only the UART interface is supported by the module. Support for the I2C and SPI interfaces are still under development.
-
Feature Under Development
Support for the
L1Cfrequency band has not been implemented. -
Feature Under Development
Corrections for some of the PPP services have not been implemented.