Hardware Overview

Introduction
-
SparkPNT GNSS Flex Module - LG580P
SKU: GPS-28870
-
SparkPNT GNSS Flex modules are plug-in boards featuring different GNSS receivers. They are designed to be easily swapped for repairs and pin-compatible for upgrades. The boards have two 2x10-pin, 2mm pitch female headers connecting to carrier boards. For the LG580P GNSS receiver, these pins will break out the USB, UART (x3), and I2C* interfaces, along with the PPS and event signals using a standardized pinout.
This SparkPNT GNSS Flex module is an upgraded version of the LG290P GNSS Flex module. It features the Quectel LG580P quad-band, multi-constellation, high-precision, RTK and heading GNSS receiver with two antenna inputs for instantaneous heading determination down to 0.1°. In traditional navigation systems, such as those used on your phone or car, previous navigation points are utilized to determine the course heading. This is the reason why the arrow indicator will spin or be oriented in the wrong directions when the navigation system first boots or has been stationary for extended periods of time. However, with the LG580 GNSS receiver, users are provided with a dedicated heading without relying on previous course data points, magnetometers/compasses, or gyroscopes in IMUs, which can introduce small errors.
The LG580P module offers a diverse choice of interfaces including UART, SPI*, I2C*, and CAN*. Additionally, the module is capable of simultaneously receiving signals from the
L1,L2,L5, andL6/E6frequency bands of the GPS, GLONASS, Galileo, BDS, QZSS, and NavIC GNSS constellations. In addition, the module supports SBAS augmentation systems (WAAS, EGNOS, BDSBAS, MSAS, GAGAN, KASS, ASECNA, SouthPAN, and SDCM), PPP services* (BDS PPP-B2b, QZSS CLAS, MADOCA-PPP, and Galileo HAS), RTCM, and RTK corrections for precision navigation with a fast convergence time and reliable performance.The built-in professional-grade interference signal detection and elimination algorithms, effectively mitigate multiple narrow-band interference sources and significantly improve signal reception performance in complex electromagnetic environments. In addition, the RTK and heading algorithms ensure reliable positioning in challenging scenarios such as urban environments and deep tree cover. With its high-precision, low power consumption and a high positioning and heading update rate of up to 20 Hz, this board is ideal for high-precision navigation applications, such as intelligent robots, precision agriculture, ADAS, and autonomous driving.
Features Under Development
- I2C/SPI/CAN - Currently, only the UART interface is supported by the module.
- PPP Services - Corrections for some of the PPP services have not been implemented.
Design Files
-
Design Files
- Schematic
- KiCad Files
- STEP File
- Board Dimensions:
- 1.75" x 1.25" (44.45mm x 31.75mm)
-
Manipulate 3D Model
Controls Mouse Touchscreen Zoom Scroll Wheel 2-Finger Pinch Rotate Left-Click & Drag 1-Finger Drag Move/Translate Right-Click & Drag 2-Finger Drag
Dimensions of the LG580P GNSS Flex module. Need more measurements?
For more information about the board's dimensions, users can download the KiCad files for this board. These files can be opened in KiCad and additional measurements can be made with the measuring tool.
KiCad - Free Download!
KiCad is free, open-source CAD program for electronics. Click on the button below to download their software. (*Users can find out more information about KiCad from their website.)
Measuring Tool
This video demonstrates how to utilize the dimensions tool in KiCad, to include additional measurements:
Board Layout
The GNSS Flex system is designed around two 2x10-pin, 2mm pitch headers used mate the two types of boards. A standardized pin layout, keeps the ecosystem pin-compatible for upgrades and allows board to be easily swapped for repairs. Depending on the capabilities of the GNSS receiver, these pins will breakout the USB, UART (x4), I2C, and SD card interfaces along with any PPS or event signals of the GNSS receiver.
The LG580P GNSS Flex module has the following features:
-
- LG580P GNSS Receiver
- The Quectel LG580P GNSS receiver
-
- GNSS Flex Headers
- Two sets of 2x10 pin, 2mm pitch female headers for connecting a GNSS Flex module to carrier boards
-
- U.FL Connectors
- Two U.FL connectors for attaching external GNSS antennas
LG580P GNSS Receiver
The centerpiece of the LG580P GNSS Flex module, is the LG580P GNSS receiver from Quectel. The LG580P is a low-power, multi-band, multi-constellation GNSS receiver capable of delivering centimeter-level precision at high update rates. The built-in professional-grade interference signal detection and elimination algorithms, effectively mitigate multiple narrow-band interference sources and significantly improve signal reception performance in complex electromagnetic environments. In addition, the RTK and heading algorithms ensure reliable positioning in challenging scenarios such as urban environments and deep tree cover. With its performance advantages of high-precision and power consumption, this board is an ideal choice for high-precision navigation applications, such as intelligent robots, UAVs, precision agriculture, mining, surveying, and autonomous navigation.
Features:
- Supply Voltage: 3.0–3.6V
- Tracking Channels: 1040
- Concurrent signal reception: 5 + QZSS
L1,L2,L5,E6frequency bands
- Sensitivity:
- Acquisition: -145dBm
- Tracking: -160dBm
- Reacquisition: -155dBm
- Antenna Power: External
- GNSS Constellations and SBAS Systems:
- USA: GPS + WASS
- Russia: GLONASS + SDCM
- EU: Galileo + EGNOS
- China: BDS + BDSDAS
- Japan: QZSS + MSAS
- India: NavIC + GAGAN
- Korea: KASS
- Africa: ASECNA
- Auz/NZ: SouthPAN
- Accuracy of 1PPS Signal: 5ns
- Update Rate:
- Default: 10Hz
- Max: 20Hz
- Time to First Fix (without AGNSS):
- Cold Start: 28s
- Warm Start: 28s
- Hot Start: 1.8s
- RTK Convergence Time: 5s
- Dynamic Performance:
- Maximum Altitude: 10000m
- Maximum Velocity: 490m/s
- Maximum Acceleration: 4g
- Interfaces
- Operating temperature: -40°C to +85°C
- Footprint: 21mm × 16mm × 2.7mm
- Weight: 1.4g
Power Consumption
The power consumption of the LG580P GNSS receiver depends on the GNSS signals enabled and the positioning mode.
| Mode | Power (mW) | Current (mA) |
|---|---|---|
| Acquisition | 323.4 | 98 |
| Tracking | 382.8 | 116 |
| Backup | 59.4 | 0.018 |
Power Modes
- Acquisition:
- Module searches for satellites and to determine visible satellites, coarse frequency, and the code phase of satellite signals
- Tracking:
- Once acquisition is completed, the module tracks satellites and demodulates the navigation data from specific satellites
- Backup Mode:
- Reduces power consumption. Only backup domain is active and keeps track of time.
Frequency Bands
The LG580P modules are multi-band, multi-constellation GNSS receivers. Below, is a chart illustrating the frequency bands utilized by all the global navigation satellite systems; along with a list of the frequency bands and GNSS systems supported by the LG580P GNSS receiver.
Frequency bands of the global navigation satellite systems. (Source: Tallysman)
Supported Frequency Bands:
- GPS:
L1 C/A,L5,L2C - GLONASS:
L1,L2 - Galileo:
E1,E5a,E5b,E6 - BDS:
B1I,B1C,B2a,B2b,B2I,B3I - QZSS:
L1 C/A,L5,L2C,L6 - NavIC:
L5 - SBAS:
L1 - L-band PPP2:
- PPP:
B2b - QZSS:
L6 - Galileo HAS:
E6
- PPP:
Supported GNSS Constellations:
- GPS (USA)
- GLONASS (Russia)
- Galileo (EU)
- BDS (China)
- QZSS (Japan)
- NavIC (India)
Supported SBAS Systems:
- WASS (USA)
- SDCM (Russia)
- EGNOS (EU)
- BDSBAS (China)
- MSAS (Japan)
- GAGAN (India)
- KASS (Korea)
- ASECNA (Africa)
- SouthPAN (Aus/NZ)
Info
For a comparison of the frequency bands supported by the LG580P GNSS receivers, refer to sections 1.2, 1.5, and 1.6 of the hardware design manual.
What are Frequency Bands?
A frequency band is a section of the electromagnetic spectrum, usually denoted by the range of its upper and lower limits. In the radio spectrum, these frequency bands are usually regulated by region, often through a government entity. This regulation prevents the interference of RF communication; and often includes major penalties for any interference with critical infrastructure systems and emergency services.
However, if the various GNSS constellations share similar frequency bands, then how do they avoid interfering with one another? Without going too far into detail, the image above illustrates the frequency bands of each system with a few characteristics specific to their signals. Wit these characteristics in mind, along with other factors, the chart can help users to visualize how multiple GNSS constellations might co-exist with each other.
For more information, users may find these articles of interest:
Position Accuracy
The accuracy of the position reported from the LG580P GNSS receiver, can be improved based upon the correction method being employed. Currently, RTK corrections provide the highest level of accuracy; however, users should be aware of certain limitations of the system:
- RTK technique requires real-time correction data from a reference station or network of base stations.
- RTK corrections usually come from RTCM messages that are signal specific (i.e. an RTK network may only provide corrections for specific signals; only
E5band notE5a).
- RTK corrections usually come from RTCM messages that are signal specific (i.e. an RTK network may only provide corrections for specific signals; only
- The range of the base stations will vary based upon the method used to transmit the correction data.
- The reliability of RTK corrections are inherently reduced in multipath environments.
| Correction Method | Horizontal | Vertical | Heading | Velocity |
|---|---|---|---|---|
| Standalone | 1.0m ~3.3' |
1.5m ~4.9' |
3cm/s (0.108kph) ~1.2in/s (0.067mph) |
|
| RTK | 0.8cm (+1ppm) ~0.3" |
1.5cm (+1ppm) ~0.6" |
0.1° |
RTK Corrections
To understand how RTK works, users will need a more fundamental understanding of the signal error sources.
Tip
For the best performance, we highly recommend that users configure the module to utilize/provide RTK corrections with a compatible L1/L2/L5/L6 GNSS antenna and utilize a low-loss cable.
GNSS Flex Headers
The GNSS Flex system is designed around two 2x10-pin, 2mm pitch headers used mate the two types of boards. A standardized pin layout, keeps the ecosystem pin-compatible for upgrades and allows boards to be easily swapped for repairs. For the LG580P GNSS receiver, these pins will breakout the UART interface along with three of the programmable I/O pins; the LNA enable pin is not broken out and the safe-boot pin is only exposed as a test point on this board.
The LG580P GNSS receiver has three UART ports, which can be operated and configured separately.
UART Settings
The UART ports have the following configuration settings:
- Logic Level: 3.3V
- Baudrate: 9600bps, 115200bps, 230400bps, 460800bps, 921600bps, and 3000000bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
- Flow Control: N/A
- Supported Protocols:
NMEA 0183(PQTM)RTCM 3.xQGC
Additional Support
All of the UART ports support firmware updates through their interface. In addition, the UART1 port also supports debugging data and the UART3 interface can be multiplexed for the CAN bus interface1.
UART Protocols
UART Protocols
By default, these UART ports are configured to transmit and receive NMEA 0183, RTCM 3.x, and/or QGC messages. These messages are generally used for transmitting PNT data; providing or receiving RTK corrections; and receiving PPP data, respectively. Quectel also implements a system of proprietary messages (PQTM) for users to configure the LG580P that follows a data format similar to the NMEA protocol. The expected structure of these proprietary messages is shown below:
A full list of compatible NMEA 0183 v4.11 messages, is provided in section 2.2. Standard Messages of the GNSS Protocol Specification manual. This protocol is used for outputting GNSS data, as detailed by the National Marine Electronics Association organization.
List of Standard NMEA Messages
| Message | Type Mode | Message Description |
|---|---|---|
| RMC | Output | Recommended Minimum Specific GNSS Data |
| GGA | Output | Global Positioning System Fix Data |
| GSV | Output | GNSS Satellites in View |
| GSA | Output | GNSS DOP and Active Satellites |
| VTG | Output | Course Over Ground & Ground Speed |
| GLL | Output | Geographic Position – Latitude/Longitude |
| GBS | Output | GNSS Satellite Fault Detection |
| GNS | Output | GNSS Fix Data |
| GST | Output | GNSS Pseudorange Error Statistics |
| ZDA | Output | UTC Time & Date |
| HDT | Output | True Vessel Heading |
| THS | Output | True, Heading, and Status |
A full list of PQTM messages (proprietary NMEA messages defined by Quectel) supported by LG580P, is provided in section 2.3. PQTM Messages of the GNSS Protocol Specification manual. This protocol is used to configure or read the settings for the LG580P GNSS receiver.
List of Proprietary Quectel Messages
| Message | Type Mode | Message Description |
|---|---|---|
| PQTMVER | Output | Outputs the firmware version |
| PQTMCOLD | Command | Performs a cold start |
| PQTMWARM | Command | Performs a warm start |
| PQTMHOT | Command | Performs a hot start |
| PQTMSRR | Command | Performs a system reset and reboots the receiver |
| PQTMUNIQID | Command | Queries the module unique ID |
| PQTMSAVEPAR | Command | Saves the configurations into NVM |
| PQTMRESTOREPAR | Command | Restores the parameters configured by all commands to their default values |
| PQTMVERNO | Command | Queries the firmware version |
| PQTMCFGUART | Set/Get | Sets/gets the UART interface |
| PQTMCFGPPS | Set/Get | Sets/gets the PPS feature |
| PQTMCFGPROT | Set/Get | Sets/gets the input and output protocol for a specified port |
| PQTMCFGNMEADP | Set/Get | Sets/gets the decimal places of standard NMEA messages |
| PQTMEPE | Output | Outputs the estimated position error |
| PQTMCFGMSGRATE | Set/Get | Sets/gets the message output rate on the current interface |
| PQTMVEL | Output | Outputs the velocity information |
| PQTMCFGGEOFENCE | Set/Get | Sets/gets geofence feature |
| PQTMGEOFENCESTATUS | Output | Outputs the geofence status |
| PQTMGNSSSTART | Command | Starts GNSS engine |
| PQTMGNSSSTOP | Command | Stops GNSS engine |
| PQTMTXT | Output | Outputs short text messages |
| PQTMCFGSVIN | Set/Get | Sets/gets the Survey-in feature |
| PQTMSVINSTATUS | Output | Outputs the Survey-in status |
| PQTMPVT | Output | Outputs the PVT (GNSS only) result |
| PQTMCFGRCVRMODE | Set/Get | Sets/gets the receiver working mode |
| PQTMDEBUGON | Command | Enables debug log output |
| PQTMDEBUGOFF | Command | Disables debug log output |
| PQTMCFGFIXRATE | Set/Get | Sets/gets the fix interval |
| PQTMCFGRTK | Set/Get | Sets/gets the RTK mode |
| PQTMCFGCNST | Set/Get | Sets/gets the constellation configuration |
| PQTMDOP | Output | Outputs dilution of precision |
| PQTMPL | Output | Outputs protection level information |
| PQTMCFGODO | Set/Get | Sets/gets the odometer feature |
| PQTMRESETODO | Command | Resets the accumulated distance recorded by the odometer |
| PQTMODO | Output | Outputs the odometer information |
| PQTMCFGSIGNAL | Set/Get | Sets/gets GNSS signal mask |
| PQTMCFGSAT | Set/Get | Sets/gets GNSS satellite mask |
| PQTMCFGRSID | Set/Get | Sets/gets the reference station ID |
| PQTMCFGRTCM | Set/Get | Sets/gets RTCM |
| PQTMCFGSBAS | Set/Get | Configures SBAS |
| PQTMCFGNMEATID | Set/Get | Configures the NMEA Talker ID |
| PQTMTAR | Output | Outputs the time and attitude |
| PQTMCFGBLD | Set/Get | Configures the baseline distance |
| PQTMCFGRTKSRCTYPE | Set/Get | Configures RTK differential source type |
| PQTMSN | Command | Reads the SN of module |
| PQTMCFGANTINF | Set/Get | Configures the antenna information |
| PQTMCFGANTDELTA | Set/Get | Configures the delta between antennas |
| PQTMCFGSIGGRP | Set/Get | Configures the GNSS signal group |
| PQTMCFGSIGNAL2 | Set/Get | Configures GNSS signal mask for second antenna |
| PQTMCFGGEOSEP | Set/Get | Configures geoidal separation |
| PQTMCFGCNRTHD | Set/Get | Configures the CNR threshold for position engine |
| PQTMCFGELETHD | Set/Get | Configures the elevation threshold for position engine |
| PQTMNAV | Output | Outputs the navigation information |
| PQTMEOE | Output | Outputs the end of epoch information |
| PQTMCFGWN | Set/Get | Configures the reference start week number |
| PQTMANTENNASTATUS | Output | Reports the antenna status |
A full list of QGC messages (proprietary protocol defined by Quectel) supported by LG580P, is provided in section 3. QGC Protocol of the GNSS Protocol Specification manual. This protocol is used to output the PPP raw data.
List of Proprietary Quectel Messages
| GQC Message Name | Message Group | Message Number | Type | Description |
|---|---|---|---|---|
| RAW-PPPB2B | 0x0A | 0xB2 | Output | BDS PPPB2B binary raw messages |
| RAW-QZSSL6 | 0x0A | 0xB6 | Output | QZSSL6 binary raw messages |
| RAW-HASE6 | 0x0A | 0xE6 | Output | Galileo HASE6 binary raw messages |
A full list of compatible RTCM v3 messages, is provided in section 4. RTCM Protocol of the GNSS Protocol Specification manual. This protocol is used for transferring GNSS raw measurement data, as detailed by the Radio Technical Commission for Maritime Services organization.
List of Supported RTCMv3 (MSM) Messages
| Message | Type Mode | Message Description |
|---|---|---|
| 1005 | Input/Output | Stationary RTK Reference Station ARP |
| 1006 | Input/Output | Stationary RTK Reference Station ARP with height |
| 1019 | Input/Output | GPS Ephemerides |
| 1020 | Input/Output | GLONASS Ephemerides |
| 1041 | Input/Output | NavIC/IRNSS Ephemerides |
| 1042 | Input/Output | BDS Satellite Ephemeris Data |
| 1044 | Input/Output | QZSS Ephemerides |
| 1046 | Input/Output | Galileo I/NAV Satellite Ephemeris Data |
| 1073 | Input/Output | GPS MSM3 |
| 1074 | Input/Output | GPS MSM4 |
| 1075 | Input/Output | GPS MSM5 |
| 1076 | Input/Output | GPS MSM6 |
| 1077 | Input/Output | GPS MSM7 |
| 1083 | Input/Output | GLONASS MSM3 |
| 1084 | Input/Output | GLONASS MSM4 |
| 1085 | Input/Output | GLONASS MSM5 |
| 1086 | Input/Output | GLONASS MSM6 |
| 1087 | Input/Output | GLONASS MSM7 |
| 1093 | Input/Output | Galileo MSM3 |
| 1094 | Input/Output | Galileo MSM4 |
| 1095 | Input/Output | Galileo MSM5 |
| 1096 | Input/Output | Galileo MSM6 |
| 1097 | Input/Output | Galileo MSM7 |
| 1113 | Input/Output | QZSS MSM3 |
| 1114 | Input/Output | QZSS MSM4 |
| 1115 | Input/Output | QZSS MSM5 |
| 1116 | Input/Output | QZSS MSM6 |
| 1117 | Input/Output | QZSS MSM7 |
| 1123 | Input/Output | BDS MSM3 |
| 1124 | Input/Output | BDS MSM4 |
| 1125 | Input/Output | BDS MSM5 |
| 1126 | Input/Output | BDS MSM6 |
| 1127 | Input/Output | BDS MSM7 |
| 1133 | Input/Output | NavIC/IRNSS MSM3 |
| 1134 | Input/Output | NavIC/IRNSS MSM4 |
| 1135 | Input/Output | NavIC/IRNSS MSM5 |
| 1136 | Input/Output | NavIC/IRNSS MSM6 |
| 1137 | Input/Output | NavIC/IRNSS MSM7 |
From the module, the PPS output signal is a 3.3V signal output.
PPS signal's output on the LG580P GNSS Flex module.
Use Case
- Users could use this signal in conjunction with the event pins to synchronize two modules with each other.
- Users could use this signal to create their own Stratum 0 source for the NTP on a primary time server.
The RTK pin operates as the RTK_STAT status indicator for the RTK positioning.
RTK_LED pin on the LG580P GNSS Flex module.
Info
The RTK_STAT pin is used to indicate RTK status. The pin is at high level during startup.
- If the pin output is high, it indicates the module has entered the RTK fixed mode.
- If the pin output is low, it indicates that the module exited the RTK fixed mode or is in backup mode.
- If the pin outputs an alternating pin level, it indicates that the module received the correct RTCM data and did not enter the RTK fixed mode. The default frequency is 10Hz.
U.FL Connectors
Users will need to connect compatible GNSS antennas to the Primary Antenna and Secondary Antenna U.FL connectors. The type of antenna used with the LG580P module affects the overall accuracy of the position and attitude calculated by the GNSS receiver.
- Passive antennas are not recommended for the LG580P GNSS receiver.
- To mitigate the impact of out-of-band signals, utilize an active antenna whose SAW filter is placed in front of the LNA in the internal framework.
- DO NOT select an antenna with the LNA placed in the front.
- There is no need to inject an external DC voltage for the GNSS antenna. Power is already provided from the LG580P module for the LNA of an active antenna.
The U.FL connectors to attach external GNSS antennas to the LG580P GNSS Flex module.
Tip
For the best performance, we recommend users choose compatible L1/L2/L5/L6/L-Band GNSS antennas and utilize a low-loss cables. Also, don't forget that GNSS signals are fairly weak and can't penetrate buildings or dense vegetation. The GNSS antennas should have an unobstructed view of the sky.
-
Feature Under Development
Currently, only the UART interface is supported by the module. Support for the I2C, SPI, and CAN interfaces are still under development.
-
Feature Under Development
Corrections for some of the PPP services have not been implemented.
-
Feature Under Development
The event trigger has not been implemented.