Software Overview
QGNSS Software
Windows Only
Currently, the QGNSS software is only available for Windows operating systems.
QGNSS is highly intuitive GNSS evaluation software that is easy to use, personalized, and compatible with leading Quectel technologies. The software allows users to define or apply GNSS product configurations for specific use cases. Saving, restoring, or sharing configurations between different products and users is easy. The software supports product evaluation with a choice of views to observe static and dynamic behavior of the connected a Quectel GNSS receiver.
System Requirements
Operating System: Windows
Connecting to the LG580P
In order to connect to the LG580P properly, users will need to specify the settings of the UART port.
Click the button to configure the UART settings.
Before users can connect to the LG580P GNSS Flex module, they will need to specify the connection settings in QGNSS. Once configured, users can select the OK button and QGNSS will automatically attempt to connect to the GNSS receiver.
- Select the
LG580P(03)from the drop-down menu to configure theModelof the GNSS receiver being connected. - Below, is a list of the default settings for
UARTports of the LG580P. These settings should be selected in theDevice Informationmenu, unless configured differently. - For the
Port, select the port associated with the connected USB-to-Serial converter.
Specify the settings for the UART port in QGNSS.
Configure the LG580P
By default, the UART ports are configured to transmit and receive NMEA 0183 and/or RTCM 3.x messages. These messages are generally used for transmitting PNT data; and providing or receiving RTK corrections, respectively. Quectel also implements a system of proprietary messages (PQTM) for users to configure the LG580P, following the data format of the NMEA protocol.
Data Format - PQTM Messages
The expected structure of the data in the proprietary PQTM messages is shown below:
NMEA protocol.
<Checksum>:
- Checksum field follows the checksum delimiter character
*. - Checksum is the 8-bit exclusive OR of all characters in the sentence, including
,the field delimiter, between but not including the$and the*delimiters.
<CR> & <LF>: Carriage return; followed by a new line
- Depending on the terminal emulator, these may be options configured in the program settings.
- Otherwise, users may need to add the
\rand\ncharacters at the end of the message.
In the QGNSS software, users can click on the Advance button, at the bottom of the QConsole window, to configure the settings for the messages sent to the LG580P. Selecting NMEA and CRLF from the drop-down menu of the Checksum Type and Suffix options, will automatically calculate and append the <checksum> value, carriage return, and line follow to the end of the message entered in the Data Input field.
The settings for the messages transmitted from the QConsole.
Display the QConsole Toolbar
There is a toolbar for the QConsole, which has a bunch of tools that users may find useful. This includes, a search function, scroll-lock button, pause/clear the message feed, etc. To open/close the toolbar inside the QConsole, right-click on the mouse and select the Show Tool option from the drop-down menu or utilize the keyboard shortcut: Ctrl + Q.
Show Tool option, inside the QConsole.
Example - PQTMCFGUART Message
As an example, try utilizing the PQTMCFGUART PQTM message. Enter $PQTMCFGUART,R* into the Data Input field of the QConsole. DOn't forget to select the NMEA and CRLF options from Advance settings menu. If entered and configured properly, the value 36 should pop up in the Checksum field of the QConsole; then, click on the button to send the message.
Once the message has been sent, keep a close watch of the messages in the console. It may help to click on the button to disable auto-scrolling, when trying to locate the message response. Additionally, the response may not appear right away, it could be appended to the end of the next data packet, as shown in the image below.
Firmware Update
In the event that users need to update the firmware on the LG580P module, please refer to the instructions in Quectel's reference manual. For the latest firmware, users should reach out to Quectel through their forum page.
Synchronization Step
In the reference manual, Step 9 instructs users to wait for a synchronization process. If users refer to an earlier section of the manual, this process requires the LG580P module to receive a SYNC_WORD1 within 500ms of powering up. Therefore, users must restart the module during the synchronization step. In the QGNSS software (+v2.1), this can be performed with the reboot button.
Example - Step-by-Step Instructions
- Connect to the LG580P
-
From the Tools drop down menu, select Firmware Update
Tools > Firmware Update
-
Click the button to select the receiver firmware
- Click to choose the firmware upgrade package whose name is identifiable by the presence of
*.pkgfile extension - Click on the button to reboot the GNSS receiver
- Click the button to start the firmware upgrade process and wait for it to complete
- If the GNSS receiver wasn't rebooted prior initializing the upgrade, the process will wait for the synchronization step. The user will then have 20 seconds to manually reboot the GNSS receiver; otherwise, the firmware upgrade process will fail.
- Wait for the process to complete
- After the firmware upgrade is complete, the module will automatically reboot
PyGPSClient
As an alternative to QGNSS, we recommend PyGPSClient for users with computers that run on MacOS or Linux.
Resources
For additional information, users can refer to the following resources for the PyGPSClient software:
Installation
There are a variety of installation methods detailed in the GitHub repository's README.md file. However, we recommend utilizing the pip installation method.
Installation Commands
Depending on how Python is installed on the computer, one of the following commands should allow users to install the software.
System Requirements
This installation method requires an internet connection. Additionally, users will also need administrative privileges (or root access sudo) for the installation.
Connecting to the LG580P
Before users can connect to the LG580P GNSS Flex module, they will need to specify the settings of the UART port in PyGPSClient. Once configured, users can select the button and PyGPSClient will automatically attempt to connect to the GNSS receiver.
- For the
Serial Port, select the port associated with the GNSS receiver.
Specify the settings for the UART port in QGNSS.
Terminal Emulator
Another viable option for connecting to the LG580P GNSS Flex module, is to utilize a terminal emulation program. While reading the data sent from the LG580P is relatively trivial, users will need to be more selective when choosing an emulator to configure the LG580P GNSS receiver. This is due to the unique data structure of the proprietary messages that Quectel implements to configure the LG580P (see the Configure the LG580P section, above).
Arduino Library
The SparkFun LG290P Quadband RTK GNSS Arduino Library can be installed from the library manager in the Arduino IDE by searching for:
SparkFun LG290P Quadband RTK GNSS Arduino Library
Manually Download the Arduino Library
For users who would like to manually download and install the library, the *.zip file can be accessed from the GitHub repository or downloaded by clicking the button below.