Skip to content

Troubleshooting Tips

Need Help?

If you need technical assistance or more information on a product that is not working as you expected, we recommend heading on over to the SparkFun Forums.

Account Registration Required

If this is your first visit to our forum, you'll need to create a Forum Account to post questions.

Electrostatic Discharge

The mosaic-X5 GNSS receiver is sensitive to ESD. Use a proper grounding system to make sure that the working surface and the components are at the same electric potential.

ESD Precaution

As recommended by the manufacturer, we highly recommend that users take the necessary precautions to avoid damaging their module.

QR code to product video

USB Driver

A USB driver is only required for Windows PCs (see the USB Driver section).

GNSS antenna

Power Input

Active Antenna

Never inject an external DC voltage into the SMA connector for the GNSS antenna, as it may damage the mosaic-X5 GNSS receiver. For instance, when using a splitter to distribute the antenna signal to several GNSS receivers, make sure that no more than one output of the splitter passes DC. Use DC-blocks otherwise.

Supported Frequency Bands

For the best performance, we recommend users choose a compatible L1/L2/L5/L6 GNSS antenna and utilize a low-loss cable. Utilizing an antenna that doesn't match all the supported frequency bands of the mosaic-X5, will result in reduced performance and capabilities.

Data Logging

For data logging issues, here are some simple troubleshooting tips:

  • Make sure that your SD card is formatted to a FAT32 file system.
    • The FAT32 file system also limits the maximum capacity of the card to less than 32GB (i.e. a 256GB SD card will not work).
  • Make sure that the mosaic-X5 GNSS receiver has a configured data stream output.
  • Use the mosaic-X5 web page to verify that the SD card is mounted as a storage drive.