Web Interface
Firmware Update
Users can easily upgrade the firmware for the mosaic-X5 module through its webserver interface. This is useful for updating various features, such as the antenna calibration list.
-
To check for the latest firmware published by Septentrio, please visit their product page for the mosaic-X5 module. Users can click on the button below, to be redirected to the latest firmware for the mosaic-X5.
-
Currently, at the time that this board was released, the firmware for the mosaic-X5 module was v4.15.01. Users can download version 4.15.0 of the firmware, by clicking on the button below.
Latest Firmware
For the latest firmware released by Septentrio, please visit their product page for the mosaic-X5 module.
Record GNSS Data
RTK Corrections
IP Server/Client
For users with multiple RTK capable GNSS receivers, users can configure their mosaic-X5 as a rover or base station.
NTRIP Client
Without having to setup a personal base station, users can receive RTK corrections through the internet from 3rd-party services, like an NTRIP server.
Polaris RTK
The Polaris RTK Corrections Network, provided by PointOne, is an example of a 3rd-party correction service. For users interested in enabling this RTK subscription service, they can check out the documentation from their website and the video below:
Sharing Internet Access
By default, the mosaic-X5 GNSS receiver is not configured to access the internet through the USB interface. In order to receive or cast RTK corrections to/from a RTK network, such as NTRIP, users will need to enable capability.
- Users will need to use the web interface or RxTool software suite to enable the
Outgoing Internet Access Over USB
from the Communication > USB drop-down menu of the navigation tabs. - This also requires users to allow Internet sharing through their computer as well. The procedure to do so depends on your operating system.
- On a Windows PC, users must enable
Allow other network users to connect through this computer's Internet connection
, through the properties option of the network adapter with internet access. - On a Linux computer, users will likely need to configure a network bridge.
- On a Windows PC, users must enable
New IP Address
Once a network bridge is enabled, the receiver will receive its IP address from the computer's DHCP server. Depending on the routing table, the module may no longer be reachable at its default IP address (192.168.3.1
).
More Videos
Users can find other instructional videos on Septentrio's YouTube Channel. Feel free to check out their playlists as well:
Other Videos

-
For the latest firmware published by Septentrio, please visit their product page.
This is firmware version, was archived at the time that this guide was written. Please do not request for the file to be updated; instead visit the product page to download the latest firmware. ↩