Skip to content

Hardware Overview

Design Files

The SparkFun LG580P Quad-band GNSS RTK breakout board's dimensions, pin layout, and connectors are similar to our very popular SparkFun GPS-RTK-SMA Breakout - ZED-F9P (Qwiic) and SparkFun Quadband GNSS RTK Breakout - LG290P (Qwiic) boards, featuring a compact design and convenient Qwiic connectors.

Drop-in Replacement

Depending on your appication, this board could potentially function as a drop-in replacement. However, we advise users to verify the pin compatibility of this board with their current installation.

  • Design Files


  • Manipulate 3D Model
    Controls Mouse Touchscreen
    Zoom Scroll Wheel 2-Finger Pinch
    Rotate Left-Click & Drag 1-Finger Drag
    Move/Translate Right-Click & Drag 2-Finger Drag

    Board Dimensions
    Dimensions of the LG580P GNSS breakout board.

    Need more measurements?

    For more information about the board's dimensions, users can download the KiCad files for this board. These files can be opened in KiCad and additional measurements can be made with the measuring tool.

    KiCad - Free Download!

    KiCad is free, open-source CAD program for electronics. Click on the button below to download their software. (*Users can find out more information about KiCad from their website.)

    📏 Measuring Tool

    This video demonstrates how to utilize the dimensions tool in KiCad, to include additional measurements:

    QR code to play video

Board Layout

The SparkFun LG580P Quad-band GNSS RTK breakout board features the following:

Layout

Layout of the major components on the breakout board.

  1. USB-C Connector
    The primary inteface for powering and interacting with the board
  2. LG580P GNSS Module
    The Quectel LG580P GNSS module
  3. Header Pins
    Exposes pins to power the board and breaks out the interfaces of the LG580P GNSS module
  4. BlueSMiRF Header Pins
    Exposes the UART2 port of the LG580P GNSS module
  5. JST Connector
    Exposes the UART3 port of the LG580P GNSS module
  6. Qwiic Connectors
    Exposes the I2C interface of the LG580P GNSS module
  7. Status LEDs
    LED status indicators for the LG580P GNSS module
  8. Antenna L1/2/5/6 RF Connectors
    SMA connectors for an external GNSS antennas
  9. Backup Battery
    Backup power to maintain ephemeris data on the LG580P GNSS module for warm starts

USB-C Connector

The USB connector is provided to power and communicate with the LG580P GNSS receiver. For most users, it will be the primary method for interfacing with the LG580P.

USB-C Connector

USB-C connector on the Quad-band GNSS RTK breakout board.

CH342 Converter

The CH342 serial-to-USB converter allows users to interface with the UART1 port of the LG580P GNSS module through the USB-C connector. Although the CH342 provides a dual-channel UART interface, only a single channel is utilized to communicate with the LG580P GNSS module. To utilize the CH342, users may need to install a USB driver, which can be downloaded from the manufacturer website.

Once the USB driver is installed:

  • Two virtual COM ports will be emulated, which can be used as standard COM ports to access the receiver.
  • Users should select UART port with the enumeration labeled as Channel A.
USB Drivers

Linux

A USB driver is not required for Linux based operating systems.

Power

The Quad-band GNSS RTK breakout board only requires 3.3V to power the board's primary components. The simplest method to power the board is through the USB-C connector. Alternatively, the board can also be powered through the other connectors and PTH pins.

Power connections

Quad-band GNSS RTK breakout board's power connections.

Below, is a general summary of the power circuitry for the board:

  • 5V - The voltage from the USB-C connector, usually 5V.
    • Can be utilized as the primary power source for the entire board.
  • 3V3 - 3.3V power rail, which powers the LG580P GNSS module, backup battery, and the power LED.
    • Power can also be distributed to/from any of the 3V3 PTH pins or JST connectors (Qwiic or UART3).
      • For power that is supplied through these connections, the LG580P requires a supply voltage of 3.0–3.6V.
    • A regulated 3.3V is supplied by the RT9080, when powered from the 5V PTH pin or USB connector
      • Input Voltage Range: 1.2 to 5.5V (1)
      • The RT9080 LDO regulator can source up to 600mA.
  • 3V3_EN - Controls the power output from the RT9080 voltage regulator.
    • By default, the pin is pulled-up to 5V and to enable the RT9080 output voltage.
  • RST - Used to reset the LG580P GNSS module
    • Connected to the RESET_N pin of the LG580P module, a system pin with an internal pull-up resistor.
    • Driving the pin LOW for at least 100ms and releasing it, triggers a hard reset.
  • GND - The common ground or the 0V reference for the voltage supplies.
  • Backup Battery - Provides backup power to the GNSS module to maintain ephemeris data
  1. While the RT9080 LDO regulator has an input voltage range of 1.2 - 5.5V, a minimum supply voltage of 3.5V is recommended for a 3.3V output.

JST Connector

The VCC pin of the JST connector is designed to operate as a voltage output. However, an input voltage can be supplied through the pin, but users should be mindful of any voltage contention issues.

Additionally, the VSEL jumper can be modified to change to output voltage level of the VCC pin.

BlueSMiRF Header

The 3V3 pin of the BlueSMiRF header is designed to operate as a voltage output. However, an input voltage can be supplied through the pin, but users should be mindful of any voltage contention issues.

Additionally, the BT-VCC jumper can be modified to change to output voltage level of the 3V3 pin.

Info

For more details, users can reference the schematic and the datasheets of the individual components on the board.

Power Modes

Acquisition:
Module searches for satellites and to determine visible satellites, coarse frequency, and the code phase of satellite signals
Tracking:
Once acquisition is completed, the module tracks satellites and demodulates the navigation data from specific satellites
Backup Mode:
Reduces power consumption. Only backup domain is active and keeps track of time.

Power Consumption

The power consumption of the LG580P GNSS module depends on the GNSS signals enabled and the positioning mode.

Current Consumption:

  • Acquisition: 98mA (323.4mW)
  • Tracking: 116mA (382.8mW)
  • Backup Mode: 18μA (59.4μW)

Backup Battery

While charged, the backup battery allows the GNSS module to maintain valid ephemeris data (time and GNSS orbital trajectories) that was stored. Otherwise, the GNSS module must restart acquiring and tracking satellites.

Time to First Fix:

  • Cold Start: 28s
  • Warm Start: 28s
  • Hot Start: 1.8s

  LG580P GNSS

The centerpiece of the Quad-band GNSS RTK breakout board, is the LG580P GNSS module from Quectel. The LG580P is a low-power, multi-band, multi-constellation GNSS receiver capable of delivering centimeter-level precision at high update rates. The built-in professional-grade interference signal detection and elimination algorithms, effectively mitigate multiple narrow-band interference sources and significantly improve signal reception performance in complex electromagnetic environments. In addition, the RTK and heading algorithms ensure reliable positioning in challenging scenarios such as urban environments and deep tree cover. With its performance advantages of high-precision and power consumption, this board is an ideal choice for high-precision navigation applications, such as intelligent robots, UAVs, precision agriculture, mining, surveying, and autonomous navigation.

LG580P GNSS module

The LG580P module on the Quad-band GNSS RTK breakout board.

QR code to product video

General Features
  • Supply Voltage: 3.0–3.6V
  • Tracking Channels: 1040
  • Concurrent signal reception: 5 + QZSS
    • L1, L2, L5, E6 frequency bands
  • Sensitivity:
    • Acquisition: -145dBm
    • Tracking: -160dBm
    • Reacquisition: -155dBm
  • Antenna Power: External
  • GNSS Constellations and SBAS Systems:
    • USA: GPS + WASS
    • Russia: GLONASS + SDCM
    • EU: Galileo + EGNOS
    • China: BDS + BDSDAS
    • Japan: QZSS + MSAS
    • India: NavIC + GAGAN
    • Korea: KASS
    • Africa: ASECNA
    • Auz/NZ: SouthPAN
  • Accuracy of 1PPS Signal: 5ns
  • Update Rate:
    • Default: 10Hz
    • Max: 20Hz
  • Time to First Fix (without AGNSS):
    • Cold Start: 28s
    • Warm Start: 28s
    • Hot Start: 1.8s
  • RTK Convergence Time: 5s
  • Dynamic Performance:
    • Maximum Altitude: 10000m
    • Maximum Velocity: 490m/s
    • Maximum Acceleration: 4g
  • Interfaces
    • UART (x3)
      • Baud Rate: 9600–3000000bps
        • Default: 460800bps
      • Protocol: NMEA 0183/RTCM 3.x/QGC
    • SPI1 (x1)
    • I2C1 (x1)
    • CAN1 (x1)
  • Operating temperature: -40°C to +85°C
  • Footprint: 21mm × 16mm × 2.7mm
  • Weight: 1.4g

Frequency Bands

The LG580P modules are multi-band, multi-constellation GNSS receivers. Below, is a chart illustrating the frequency bands utilized by all the global navigation satellite systems; along with a list of the frequency bands and GNSS systems supported by the LG580P GNSS module.

GNSS frequency bands

Frequency bands of the global navigation satellite systems. (Source: Tallysman)

Supported Frequency Bands:

  • GPS: L1 C/A, L5, L2C
  • GLONASS: L1, L2
  • Galileo: E1, E5a, E5b, E6
  • BDS: B1I, B1C, B2a, B2b, B2I, B3I
  • QZSS: L1 C/A, L5, L2C, L6
  • NavIC: L5
  • SBAS: L1
  • L-band PPP2:
    • PPP: B2b
    • QZSS: L6
    • Galileo HAS: E6

Supported GNSS Constellations:

  • GPS (USA)
  • GLONASS (Russia)
  • Galileo (EU)
  • BDS (China)
  • QZSS (Japan)
  • NavIC (India)

Supported SBAS Systems:

  • WASS (USA)
  • SDCM (Russia)
  • EGNOS (EU)
  • BDSBAS (China)
  • MSAS (Japan)
  • GAGAN (India)
  • KASS (Korea)
  • ASECNA (Africa)
  • SouthPAN (Aus/NZ)

Info

For a comparison of the frequency bands supported by the LG580P GNSS modules, refer to sections 1.2, 1.5, and 1.6 of the hardware design manual.

What are Frequency Bands?

A frequency band is a section of the electromagnetic spectrum, usually denoted by the range of its upper and lower limits. In the radio spectrum, these frequency bands are usually regulated by region, often through a government entity. This regulation prevents the interference of RF communication; and often includes major penalties for any interference with critical infrastructure systems and emergency services.

GNSS frequency bands
Frequency bands of the global navigation satellite systems. (Source: ESA)

However, if the various GNSS constellations share similar frequency bands, then how do they avoid interfering with one another? Without going too far into detail, the image above helps illustrate some of the characteristics, specific to the frequency bands of each system. With these characteristics in mind, along with other factors, the chart can help users to visualize how multiple GNSS constellations might co-exist with each other.

For more information, users may find these articles of interest:

GNSS Accuracy

The accuracy of the position reported from the LG580P GNSS module, can be improved based upon the correction method being employed. Currently, RTK corrections provide the highest level of accuracy; however, users should be aware of certain limitations of the system:

  • RTK technique requires real-time correction data from a reference station or network of base stations.
    • RTK corrections usually come from RTCM messages that are signal specific (i.e. an RTK network may only provide corrections for specific signals; only E5b and not E5a).
  • The range of the base stations will vary based upon the method used to transmit the correction data.
  • The reliability of RTK corrections are inherently reduced in multipath environments.
Correction Method Horizontal Vertical Heading Velocity
Standalone 1.0m
~3.3'
1.5m
~4.9'
3cm/s (0.108kph)
~1.2in/s (0.067mph)
RTK 0.8cm (+1ppm)
~0.3"
1.5cm (+1ppm)
~0.6"
0.1°
RTK Corrections

To understand how RTK works, users will need a more fundamental understanding of the signal error sources.

Peripherals and I/O Pins

The LG580P GNSS features several peripheral interfaces and I/O pins. Some of these are broken out as pins on the Quad-band GNSS RTK breakout board; whereas, others are broken out to their specific interface (i.e. USB connector, JST connector, etc.). Additionally, some of their connections are tied to other components on the board.

Header pins

The I/O pins on the Quad-band GNSS RTK breakout board.

Interfaces:

  • UART (x3)
  • SPI1
  • I2C1
  • CAN1
  • Event Trigger3
  • PPS Signal
  • RTK Signal
  • Module Reset

The LG580P GNSS has three UART ports, which can be operated and configured separately.

UART interface
The UART ports on the Quad-band GNSS RTK breakout board.

Pin Connections

When connecting to the UART pins to another device, the signals should be connected based upon the flow of their data.

Board RX TX GND
UART Device TX RX GND

UART Settings

The UART ports have the following configuration settings:

  • Logic Level: 3.3V
  • Baudrate: 9600bps, 115200bps, 230400bps, 460800bps, 921600bps, and 3000000bps
  • Data Bits: 8
  • Parity: No
  • Stop Bits: 1
  • Flow Control: N/A
  • Supported Protocols:
    • NMEA 0183 (PQTM)
    • RTCM 3.x
    • QGC
Additional Support

All of the UART ports support firmware updates through their interface. In addition, the UART1 port also supports debugging data and the UART3 interface can be multiplexed for the CAN bus interface1.

UART1 can only be accessed from the USB-C connector, through the CH342 serial-to-USB converter. For Windows and MacOS computers, a USB driver must be installed in order to communicate with the LG580P module through the CH342 converter; however for Linux operating systems, the standard Linux CDC-ACM driver is suitable. Once the USB driver has been installed:

  • Two virtual COM ports are emulated, which can be used as standard COM ports to access the receiver.
  • Users should select COM port with the lower enumeration or listed as Channel A.

UART2 is available through the breakout PTH pins or the BlueSMiRF header pins. The pin layout of the BlueSMiRF header is pin compatible with many of our serial devices (i.e. UART adapters, serial data loggers, BlueSMiRF transceivers).

UART3 is available through the JST connector. The pin layout of the 4-pin locking JST-GH connector is compatible with many of our serial radios and adapter cables.

UART Protocols

UART Protocols

By default, these UART ports are configured to transmit and receive NMEA 0183, RTCM 3.x, and/or QGC messages. These messages are generally used for transmitting PNT data; providing or receiving RTK corrections; and receiving PPP data, respectively. Quectel also implements a system of proprietary messages (PQTM) for users to configure the LG580P that follows a data format similar to the NMEA protocol. The expected structure of these proprietary messages is shown below:

NMEA data structure
The data structure of Quectel messages for the NMEA and PQTM protocols.

QGC data structure
The data structure of Quectel messages for the QGC protocol.

A full list of compatible NMEA 0183 v4.11 messages, is provided in section 2.2. Standard Messages of the GNSS Protocol Specification manual. This protocol is used for outputting GNSS data, as detailed by the National Marine Electronics Association organization.

List of Standard NMEA Messages
Message Type Mode Message Description
RMC Output Recommended Minimum Specific GNSS Data
GGA Output Global Positioning System Fix Data
GSV Output GNSS Satellites in View
GSA Output GNSS DOP and Active Satellites
VTG Output Course Over Ground & Ground Speed
GLL Output Geographic Position – Latitude/Longitude
GBS Output GNSS Satellite Fault Detection
GNS Output GNSS Fix Data
GST Output GNSS Pseudorange Error Statistics
ZDA Output UTC Time & Date
HDT Output True Vessel Heading
THS Output True, Heading, and Status

A full list of PQTM messages (proprietary NMEA messages defined by Quectel) supported by LG580P, is provided in section 2.3. PQTM Messages of the GNSS Protocol Specification manual. This protocol is used to configure or read the settings for the LG580P GNSS module.

List of Proprietary Quectel Messages
Message Type Mode Message Description
PQTMVER Output Outputs the firmware version
PQTMCOLD Command Performs a cold start
PQTMWARM Command Performs a warm start
PQTMHOT Command Performs a hot start
PQTMSRR Command Performs a system reset and reboots the receiver
PQTMUNIQID Command Queries the module unique ID
PQTMSAVEPAR Command Saves the configurations into NVM
PQTMRESTOREPAR Command Restores the parameters configured by all commands to their default values
PQTMVERNO Command Queries the firmware version
PQTMCFGUART Set/Get Sets/gets the UART interface
PQTMCFGPPS Set/Get Sets/gets the PPS feature
PQTMCFGPROT Set/Get Sets/gets the input and output protocol for a specified port
PQTMCFGNMEADP Set/Get Sets/gets the decimal places of standard NMEA messages
PQTMEPE Output Outputs the estimated position error
PQTMCFGMSGRATE Set/Get Sets/gets the message output rate on the current interface
PQTMVEL Output Outputs the velocity information
PQTMCFGGEOFENCE Set/Get Sets/gets geofence feature
PQTMGEOFENCESTATUS Output Outputs the geofence status
PQTMGNSSSTART Command Starts GNSS engine
PQTMGNSSSTOP Command Stops GNSS engine
PQTMTXT Output Outputs short text messages
PQTMCFGSVIN Set/Get Sets/gets the Survey-in feature
PQTMSVINSTATUS Output Outputs the Survey-in status
PQTMPVT Output Outputs the PVT (GNSS only) result
PQTMCFGRCVRMODE Set/Get Sets/gets the receiver working mode
PQTMDEBUGON Command Enables debug log output
PQTMDEBUGOFF Command Disables debug log output
PQTMCFGFIXRATE Set/Get Sets/gets the fix interval
PQTMCFGRTK Set/Get Sets/gets the RTK mode
PQTMCFGCNST Set/Get Sets/gets the constellation configuration
PQTMDOP Output Outputs dilution of precision
PQTMPL Output Outputs protection level information
PQTMCFGODO Set/Get Sets/gets the odometer feature
PQTMRESETODO Command Resets the accumulated distance recorded by the odometer
PQTMODO Output Outputs the odometer information
PQTMCFGSIGNAL Set/Get Sets/gets GNSS signal mask
PQTMCFGSAT Set/Get Sets/gets GNSS satellite mask
PQTMCFGRSID Set/Get Sets/gets the reference station ID
PQTMCFGRTCM Set/Get Sets/gets RTCM
PQTMCFGSBAS Set/Get Configures SBAS
PQTMCFGNMEATID Set/Get Configures the NMEA Talker ID
PQTMTAR Output Outputs the time and attitude
PQTMCFGBLD Set/Get Configures the baseline distance
PQTMCFGRTKSRCTYPE Set/Get Configures RTK differential source type
PQTMSN Command Reads the SN of module
PQTMCFGANTINF Set/Get Configures the antenna information
PQTMCFGANTDELTA Set/Get Configures the delta between antennas
PQTMCFGSIGGRP Set/Get Configures the GNSS signal group
PQTMCFGSIGNAL2 Set/Get Configures GNSS signal mask for second antenna
PQTMCFGGEOSEP Set/Get Configures geoidal separation
PQTMCFGCNRTHD Set/Get Configures the CNR threshold for position engine
PQTMCFGELETHD Set/Get Configures the elevation threshold for position engine
PQTMNAV Output Outputs the navigation information
PQTMEOE Output Outputs the end of epoch information
PQTMCFGWN Set/Get Configures the reference start week number
PQTMANTENNASTATUS Output Reports the antenna status

A full list of QGC messages (proprietary protocol defined by Quectel) supported by LG580P, is provided in section 3. QGC Protocol of the GNSS Protocol Specification manual. This protocol is used to output the PPP raw data.

List of Proprietary Quectel Messages
GQC Message Name Message Group Message Number Type Description
RAW-PPPB2B 0x0A 0xB2 Output BDS PPPB2B binary raw messages
RAW-QZSSL6 0x0A 0xB6 Output QZSSL6 binary raw messages
RAW-HASE6 0x0A 0xE6 Output Galileo HASE6 binary raw messages

A full list of compatible RTCM v3 messages, is provided in section 4. RTCM Protocol of the GNSS Protocol Specification manual. This protocol is used for transferring GNSS raw measurement data, as detailed by the Radio Technical Commission for Maritime Services organization.

List of Supported RTCMv3 (MSM) Messages
Message Type Mode Message Description
1005 Input/Output Stationary RTK Reference Station ARP
1006 Input/Output Stationary RTK Reference Station ARP with height
1019 Input/Output GPS Ephemerides
1020 Input/Output GLONASS Ephemerides
1041 Input/Output NavIC/IRNSS Ephemerides
1042 Input/Output BDS Satellite Ephemeris Data
1044 Input/Output QZSS Ephemerides
1046 Input/Output Galileo I/NAV Satellite Ephemeris Data
1073 Input/Output GPS MSM3
1074 Input/Output GPS MSM4
1075 Input/Output GPS MSM5
1076 Input/Output GPS MSM6
1077 Input/Output GPS MSM7
1083 Input/Output GLONASS MSM3
1084 Input/Output GLONASS MSM4
1085 Input/Output GLONASS MSM5
1086 Input/Output GLONASS MSM6
1087 Input/Output GLONASS MSM7
1093 Input/Output Galileo MSM3
1094 Input/Output Galileo MSM4
1095 Input/Output Galileo MSM5
1096 Input/Output Galileo MSM6
1097 Input/Output Galileo MSM7
1113 Input/Output QZSS MSM3
1114 Input/Output QZSS MSM4
1115 Input/Output QZSS MSM5
1116 Input/Output QZSS MSM6
1117 Input/Output QZSS MSM7
1123 Input/Output BDS MSM3
1124 Input/Output BDS MSM4
1125 Input/Output BDS MSM5
1126 Input/Output BDS MSM6
1127 Input/Output BDS MSM7
1133 Input/Output NavIC/IRNSS MSM3
1134 Input/Output NavIC/IRNSS MSM4
1135 Input/Output NavIC/IRNSS MSM5
1136 Input/Output NavIC/IRNSS MSM6
1137 Input/Output NavIC/IRNSS MSM7

While not implemented yet, the I2C interface is available through the breakout PTH pins or the Qwiic connectors.

I2C interface
The I2C interface on the Quad-band GNSS RTK breakout board.

I2C Settings

By default, the UART ports are configured with the following settings:

  • Logic Level: 3.3V
  • I2C Address: N/A
  • Bitrate: up to 400kbps
  • Protocols:
    • NMEA
    • PQTM
    • RTCM
  • Built-in 2.2kΩ pull-up resistors

While not implemented yet, the SPI interface is available through the breakout PTH pins.

SPI interface
The SPI interface on the Quad-band GNSS RTK breakout board.

SPI Settings

By default, the UART ports are configured with the following settings:

  • Logic Level: 3.3V
  • Baudrate: 1Mbps – 3Mbps
  • Protocols:
    • NMEA
    • PQTM
    • Firmware updates

SRDY Pin

The SDRY pin functions as the interrupt output for the SPI interface. By default, the pin is LOW.

From the module, the PPS output signal is a 3.3V signal output that can be accessed from the PPS PTH pin. The signal is also connected to the PPS LED, which can be used as a visual indicator for its operation.

I/O for PPS signal
The timing signal's outputs on the Quad-band GNSS RTK breakout board.

Jumpers

See the Jumpers section for more details.

  • There is a jumper attached to the PPS LED. For low power applications, the jumper can be cut to disable the PPS LED.

Use Case

  • Users could use this signal in conjunction with the event pins to synchronize two modules with each other.
  • Users could use this signal to create their own Stratum 0 source for the NTP on a primary time server.

The RTK PTH pin operates as the RTK_STAT status indicator for the RTK positioning. The pin is also connected to the RTK LED, which can be used as a visual indicator for its operation.

I/O for RTK signal
The RTK signal's outputs on the Quad-band GNSS RTK breakout board.

Info

The RTK_STAT pin is used to indicate RTK status. The pin is at high level during startup.

  1. If the pin output is high, it indicates the module has entered the RTK fixed mode.
  2. If the pin output is low, it indicates that the module exited the RTK fixed mode or is in Backup mode.
  3. If the pin outputs an alternating pin level, it indicates that the module received the correct RTCM data and did not enter the RTK fixed mode. The default frequency is 10Hz.
Jumpers

See the Jumpers section for more details.

  • There is a jumper attached to the RTK LED. For low power applications, the jumper can be cut to disable the RTK LED.

The EVENT pin provides event inputs with adjustable input frequentness and polarity.

Reset Pin
The EVENT pin on the Quad-band GNSS RTK breakout board.

Use Case

Users could use this pin in conjunction with the PPS signal to synchronize two modules with each other.

The RST pin can be used to reset the LG580P module if it enters an abnormal state. To reset the GNSS module, the pin must be low for more than 100ms.

Reset Pin
The RST pin on the Quad-band GNSS RTK breakout board.

SMA Connectors

There are two SMA connectors on the Quad-band GNSS RTK breakout board. The Antenna-1 connector is the primary input for a GNSS antenna for the LG580P GNSS receiver. The Antenna-2 connector operates as a secondary GNSS antenna input to provide a heading and pitch solution from the LG580P GNSS receiver.

SMA Connectors

The SMA connectors for an external GNSS antennas on the Quad-band GNSS RTK breakout board.

Antenna Specifications

  • Passive antennas are not recommended for the LG580P GNSS module.
  • To mitigate the impact of out-of-band signals, utilize an active antenna whose SAW filter is placed in front of the LNA in the internal framework.
    • DO NOT select and antenna with the LNA placed in the front.
  • There is no need to inject an external DC voltage into the SMA connector for the GNSS antenna. Power is already provided from the LG580P module for the LNA of an active antenna.

Tip

For the best performance, we recommend users choose compatible L1/L2/L5/L6/L-Band GNSS antennas and utilize a low-loss cables. Also, don't forget that GNSS signals are fairly weak and can't penetrate buildings or dense vegetation. The GNSS antennas should have an unobstructed view of the sky.

JST Connector

The Quad-band GNSS RTK breakout features a 4-pin JST GH connector, which is polarized and locking. Users can access pins of the UART3 port with our breadboard cable. Otherwise, the connector's pin layout is compatible with any of our serial radios and adapter cables.

JST connector

The JST connector on the Quad-band GNSS RTK breakout board.

Pin Connections

Pin Connections

When connecting the Quad-band GNSS RTK breakout board to other products, users need to be aware of the pin connections between the devices.

Pin Number 1
(Left Side)
2 3 4
Label VCC TX3 RX3 GND
Function Voltage Output
- Default: 3.3V
- Selectable: 3.3V or 5V
UART3 - Receive UART3 - Transmit Ground

When connecting the Quad-band GNSS RTK breakout board to our radios, the pin connections should follow the table below. If the flow control is not enabled, the only the RX, TX, and GND pins are utilized.

Board RX TX GND
Radio TX RX GND

As documented in the LoRaSerial product manual, the pin connections between a host system (i.e. Quad-band GNSS RTK breakout board) and the LoRaSerial Kit radio is outlined in the image below.

Flow Control
The COM ports on the Quad-band GNSS RTK breakout board.

Jumpers

By default, the VSEL jumper is connected to 3V3 pad for a regulated 3.3V output on the 4-pin JST-GH connector.

BlueSMiRF Header

The Quad-band GNSS RTK breakout features a 6-pin BlueSMiRF PTH header for UART2. The pin layout of which, is compatible with many of our serial devices (i.e. UART adapters, serial data loggers, BlueSMiRF transceivers).

BlueSMiRF header

The 6-pin BlueSMiRF PTH header on the Quad-band GNSS RTK breakout board.

Jumpers

By default, the BT_VCC jumper provides a regulated 3.3V output to the BlueSMiRF header.

Status LEDs

There are four status LEDs on the Quad-band GNSS RTK breakout board:

Status LEDs

The status LED indicators on the Quad-band GNSS RTK breakout board.

  • PWR - Power (Red)
    • Turns on once 3.3V power is supplied to the board
  • PPS - Pulse-Per-Second Signal (Yellow)
    • Indicates when there is a pulse-per-second signal (see the PPS Output section)
  • PVT - Position-Velocity-Time Solution (Blue)
    • On: Indicates the module has entered PVT mode
    • Off: Indicates that the module has exited PVT mode or is in Backup mode.
  • RTK - Real-Time Kinematic Mode (White)
    • Indicates when an RTK fix has been established or when the correct RTCM data is being received (see the RTK section)
  • HEAD - Heading Solution (Green)
    • On: Indicates the module has entered Heading fixed mode
    • Off: Indicates that the module has exited Heading fixed mode or is in Backup mode.

Info

Jumpers

There are jumper attached to the LEDs. For low power applications, these jumpers can be cut to disable their respective LED. See the Jumpers section for more details.

Jumpers

Never modified a jumper before?

Check out our Jumper Pads and PCB Traces tutorial for a quick introduction!

There are seven jumpers on the back of the board that can be used to easily modify the hardware connections on the board. From which, there are three jumpers that control power to the status LEDs on the board. By default, all the jumpers are connected, to power the status LEDs. For low power applications, users can cut the jumpers to disconnect power from each of the LEDs.

Jumpers

The jumpers on the back of the Quad-band GNSS RTK breakout board.

  • VSEL - This jumper can be modified to configure/disconnect the VCC pin of the 4-pin locking JST connector to/from 3V3 or 5V power.
  • BT_VCC - This jumper can be cut to disconnect the 3V3 BlueSMiRF header pin from the 3.3V output of the RT9080 LDO regulator.
  • PWR - This jumper can be cut to remove power from the red, power LED.
  • PPS - This jumper can be cut to remove power from the yellow PPS LED, indicating when there is a PPS signal.
  • PVT - This jumper can be cut to remove power from the blue PVT LED, indicating a PVT solution or operation in PVT mode.
  • RTK - This jumper can be cut to remove power from the white RTK LED, indicating RTK fix or operation in RTK mode.
  • HEADING - This jumper can be cut to remove power from the green HEAD LED, indicating a heading solution or operation in Heading fixed mode.
  • SHLD - This jumper can be cut to disconnect the shielding of the USB-C connector from the GND plane of the board

Info

  • By default, the VSEL jumper is connected to 3V3 pad for a regulated 3.3V output on the 4-pin JST-GH connector.
  • By default, the BT_VCC jumper provides a regulated 3.3V output to the BlueSMiRF header.

  1. Feature Under Development

    Currently, only the UART interface is supported by the module. Support for the I2C, SPI, and CAN interfaces are still under development.

  2. Feature Under Development

    Corrections for some of the PPP services have not been implemented.

  3. Feature Under Development

    The event trigger has not been implemented.