Hardware Assembly
USB Programming
The USB connection is utilized for configuration and communication with the ZED-X20P GNSS module. Users only need to connect their ZED-X20P GNSS breakout board to a computer using a USB-C cable.
The ZED-X20P GNSS breakout board with a USB-C cable attached.
External Antenna
In order to receive GNSS signals, users will need to connect a compatible antenna.
Attaching a GNSS antenna to the SMA connector on the ZED-X20P GNSS breakout board.
Tip
For the best performance, we recommend users choose a compatible L1/L2/L5/L-band GNSS antenna and utilize a low-loss cable. Also, don't forget that GNSS signals are fairly weak and can't penetrate buildings or dense vegetation. The GNSS antenna should have an unobstructed view of the sky.
U.FL Connector
Users have the option of utilizing the U.FL connector to attach an external GNSS antenna. An external antenna can be connected to the U.FL connector on the board with an U.FL to SMA adapter cable. In order to utilize the U.FL connector, the RF jumper must be modified to change the signal path.
Never modified a jumper before?
Check out our Jumper Pads and PCB Traces tutorial for a quick introduction!
Breakout Pins
The PTH pins on the ZED-X20P GNSS breakout board are broken out into 0.1"-spaced pins on the outer edges of the board.
New to soldering?
If you have never soldered before or need a quick refresher, check out our How to Solder: Through-Hole Soldering guide.
Headers
When selecting headers, be sure you are aware of the functionality you require.
Soldering headers to the ZED-X20P GNSS breakout board.
BlueSMiRF Header Pins
One of the three sets of PTH pins on the ZED-X20P GNSS breakout board is labeled BlueSMiRF. This set of header pins breaks out the UART2 interface of the ZED-X20P module, which can be connected to a microcontroller or RF transceiver; such as the BlueSMiRF v2, Bluetooth® serial link. The BlueSMiRF v2 comes in two variations, with PTH pins or male header pins. Users can directly solder the PTH variant to the board with male headers, for a more permanent installation; otherwise, for more flexibility, a stackable header can be utilized.
Connecting the BlueSMiRF serial link with a stackable header to the ZED-X20P GNSS breakout board.
Connecting the BlueSMiRF serial link in a more compact orientation.
Default Settings
- Baudrate: 38400bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
When connecting the ZED-X20P GNSS breakout board to another device, users need to be aware of the pin connections and voltage ranges of the products. Below, is a table of the pin connections that users can reference.
| Pin Number |
1 (Left Side) |
2 | 3 | 4 | 5 |
6 (Right) |
|---|---|---|---|---|---|---|
| Label | NC |
TXD |
RXD |
3V3 |
NC |
GND |
| Function | UART - Transmit | UART - Receive | Output Voltage: 3.3V | Ground |
JST Connector
The BlueSMiRF header pins and JST connector, both break out the UART2 interface of the ZED-X20P module. The JST connector can be used to attach to the SiK Telemetry Radio V3 for RTK corrections.
Connecting the SiK Telemetry Radio V3 to the ZED-X20P GNSS breakout board.
Operating the ZED-X20P GNSS breakout board as an RTK base station, transmitting RTK corrections with the SiK Telemetry Radio V3.
Default Settings
- Baudrate: 38400bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
When connecting the ZED-X20P GNSS breakout board to another device, users need to be aware of the pin connections and voltage ranges of the products. Below, is a table of the pin connections that users can reference.
| Pin Number |
1 (Left Side) |
2 | 3 |
4 (Right) |
|---|---|---|---|---|
| Label | 3V3 |
TXD |
RXD |
GND |
| Function | Output Voltage: 3.3V | UART - Transmit | UART - Receive | Ground |
Qwiic Devices
The Qwiic system allows users to effortlessly prototype with a Qwiic compatible I2C device without soldering. Users can attach ZED-X20P GNSS breakout board along with other Qwiic sensors or boards to any Qwiic compatible microcontroller, with just a few Qwiic cables. (*The example below, is for demonstration purposes and is not pertinent to the board functionality or this tutorial.)
Several Qwiic devices and microcontroller connected to the ZED-X20P GNSS breakout board.