Quick Start
In this guide we'll cover how to setup the ZED-X20P GNSS breakout board. To follow along with this tutorial, at a minimum, users will need the following items:
- Computer with an operating system (OS) that is compatible with all the software installation requirements
- USB 3.1 Cable A to C - 3 Foot - Used to interface with the ZED-X20P GNSS Breakout (1)
- SparkFun Allband GNSS RTK Breakout - ZED-X20P (Qwiic)
- GNSS Multi-Band L1/L2/L5 Surveying Antenna
- If your computer doesn't have a USB-A slot, then choose an appropriate cable or adapter.
Board Layout
The SparkFun Allband GNSS RTK Breakout - ZED-X20P (Qwiic) features the following:
-
- USB-C Connector
- The primary inteface for powering and interacting with the board
-
- ZED-X20P GNSS Module
- The u-blox ZED-X20P GNSS module
-
- Header Pins
- Exposes pins to power the board and breaks out the interfaces of the ZED-X20P GNSS module
-
- BlueSMiRF Header Pins
- Exposes the
UART2interface of the ZED-X20P GNSS module
-
- JST Connector
- Exposes the
UART2interface of the ZED-X20P GNSS module
-
- Qwiic Connectors
- Exposes the I2C interface of the ZED-X20P GNSS module
-
- Status LEDs
- LED status indicators for the ZED-X20P GNSS module
-
Antenna L1/2/5/6RF Connectors- SMA and U.FL (optional) connectors for an external GNSS antenna
USB Programming
The USB connection is utilized for configuration and communication with the ZED-X20P GNSS module. Users only need to connect their ZED-X20P GNSS breakout board to a computer using a USB-C cable.
The ZED-X20P GNSS breakout board with a USB-C cable attached.
External Antenna
In order to receive GNSS signals, users will need to connect a compatible antenna.
Attaching a GNSS antenna to the SMA connector on the ZED-X20P GNSS breakout board.
Tip
For the best performance, we recommend users choose a compatible L1/L2/L5/L-band GNSS antenna and utilize a low-loss cable. Also, don't forget that GNSS signals are fairly weak and can't penetrate buildings or dense vegetation. The GNSS antenna should have an unobstructed view of the sky.
u-center 2 Software
u-center 2 is u-blox's software application for configuration, evaluation, and debugging of u-blox GNSS receivers and services. The software provides a relatively, simple graphics user interface to assess and test u-blox GNSS modules for navigation and positioning performance. It also allows users to define or apply GNSS product configurations for specific use cases. Saving, restoring, or sharing configurations between different products is easy.
Installation
Installation of the u-center 2 software is straight forward; simply, click on the button below to download the software. User should be aware that the first time the software accessed, they will need to either create or login to their existing u-blox account. If necessary, users can follow the video below or reference the user manual for more instructions.

System Requirements
Operating Systems
- Windows 10 or 11
User Account Required
The first time that users access the software, they will need to either create or login to their existing u-blox account. This requires internet access to login through a web browser. Once the account has been verified, users will no longer need to login again; unless they log out from the u-center 2 software.
Getting Started
Users should reference the user manual for more information on the u-center 2 software.