Software Overview
u-center 2 Software
u-center 2 is u-blox's software application for configuration, evaluation, and debugging of u-blox GNSS receivers and services. The software provides a relatively, simple graphics user interface to assess and test u-blox GNSS modules for navigation and positioning performance. It also allows users to define or apply GNSS product configurations for specific use cases. Saving, restoring, or sharing configurations between different products is easy.

Firmware Updates
As of HPG v2.02, firmware updates can be performed with the UART1, I2C, and SPI interfaces of the ZED-X20P. Additionally, when in the safe boot, the ZED-X20P requires an the training sequence to be enabled during the firmware update process.
Product Compatibility
Gen 10 and later u-blox GNSS modules
Installation
Installation of the u-center 2 software is straight forward; simply, click on the button below to download the software. User should be aware that the first time the software accessed, they will need to either create or login to their existing u-blox account. If necessary, users can follow the video below or reference the user manual for more instructions.

System Requirements
Operating Systems
- Windows 10 or 11
User Account Required
The first time that users access the software, they will need to either create or login to their existing u-blox account. This requires internet access to login through a web browser. Once the account has been verified, users will no longer need to login again; unless they log out from the u-center 2 software.
Video Tutorials
Users should reference the user manual for more information on the u-center 2 software. However, we have also linked their webinar and some videos from their Youtube playlist on u-blox's u-center 2 software application.




PyGPSClient
As an alternative to u-center 2, we recommend PyGPSClient for users with computers that run on MacOS or Linux.
Resources
For additional information, users can refer to the following resources for the PyGPSClient software:
Installation
There are a variety of installation methods detailed in the GitHub repository's README.md file. However, we recommend utilizing the pip installation method.
Installation Commands
Depending on how Python is installed on the computer, one of the following commands should allow users to install the software.
System Requirements
This installation method requires an internet connection. Additionally, users will also need administrative privileges (or root access sudo) for the installation.
Connecting to the ZED-X20P
Before users can connect to the ZED-X20P GNSS Flex module, they will need to specify the settings of the UART port in PyGPSClient. Once configured, users can select the button and PyGPSClient will automatically attempt to connect to the GNSS module.
- Below, is a list of the default settings for
UARTports of the ZED-X20P. These settings should be selected in the configuration menu. - For the
Serial Port, select the port associated with the attached UART interface.
Default Settings
The UART ports of the ZED-X20P GNSS module will have the following default configuration:
- Baudrate: 38400bps
- Data Bits: 8
- Parity: No
- Stop Bits: 1
- Flow Control: None
Arduino IDE
Tip
For first-time users, who have never programmed before and are looking to use the Arduino IDE, we recommend beginning with the SparkFun Inventor's Kit (SIK), which is designed to help users get started programming with the Arduino IDE.
Most users may already be familiar with the Arduino IDE and its use. However, for those of you who have never heard the name Arduino before, feel free to check out the Arduino website. To get started with using the Arduino IDE, check out our tutorials below:
SparkFun u-blox GNSS v3 Library
The SparkFun u-blox GNSS v3 library can be installed from the library manager in the Arduino IDE by searching for:
SparkFun u-blox GNSS v3
Manually Download the Arduino Library
For users who would like to manually download and install the library, the *.zip file can be accessed from the GitHub repository or downloaded by clicking the button below.