Introduction
-
GNSS Timing Breakout - mosaic-T
SKU: GPS-28731
-
At the heart of our Timing GNSS Breakout is Septentrio's mosaic-T, a compact, ultra-low power, multi-band, multi-constellation, high-precision GNSS timing receiver. It can acheive a timing precision of 5ns (5 billionths of a second), or better than 1ns with an optional subscription to the Fugro AtomiChron® L-band timing service. Event accuracy is better than 20ns. It also features Septentrio's unique AIM+ technology for interference mitigation and anti-spoofing, ensuring best-in-class reliability and accuracy.
This board provides easy access to the mosaic-T's reference clock to create your own GNSS disciplined oscillator. You can use the computed
RxClkBiasfrom thePVTCartesianorPVTGeodeticSBF blocks of the mosaic-T to discipline your own 10MHz oscillator. The EXT REF SMA connector accepts 50Ω, 10MHz signals within a range of -14dBm (min) to +14dBm (max). TheINT/EXTslide switch selects the internal or external oscillator.The mosaic-T is a sophisticated timing receiver running an internal web server that can be accessed through the USB interface with a standard browser using a Linux/Windows computer. Septentrio also provides dozens of video tutorials to guide users through the configuration settings of their GNSS receivers utilizing the web interface.
Beyond the capabilities of the mosaic-T module, this board is seamless to operate with no programming skills required. Gone are the times when a microcontroller was required to interface with the GNSS receiver and log data to an SD card and when users had to carry around an SD card reader to extract the data from the SD card. The Timing GNSS Breakout - mosaic-T can start/stop logging data or mount/unmount the SD card, without a single line of code, just utilizing a simple button. For the users who prefer a command-line interface, Septentrio has you covered. Users can still control and configure the mosaic-T module through a CLI, which is useful for scenarios such as production line testing (in fact, that is how we tested this board).
This breakout board is a perfect middle ground for users who would like to integrate the mosaic-T module into a project/enclosure with access to a majority of the module's available pins, similar to Septentrio's developer kit, but in the smaller form factor of their evaluation kit. Or maybe... you just needed a very accurate PPS output at a 3.3V logic level. Please, check out the rest of our hookup guide for more details on the capabilities of this board (that we couldn't fit in this product description).
RTK Not Supported
The mosaic-T is a superb GNSS module designed for highly accurate timing applications. But it does not support RTK. It can not be configured as a RTK Rover or Base. RTCM output is not supported.
Important: Read Before Use!
ESD Sensitivity
The mosaic-T module is sensitive to ESD. Use a proper grounding system to make sure that the working surface and the components are at the same electric potential.
Active Antenna
Never inject an external DC voltage into the SMA connector for the GNSS antenna, as it may damage the mosaic-T module. For instance, when using a splitter to distribute the antenna signal to several GNSS receivers, make sure that no more than one output of the splitter passes DC. Use DC-blocks otherwise.
Product Comparison
Below is a simple comparison table between our breakout board and Septentrio's development and evaluation kits:
mosaic-T Development Kit
|
mosaic-T GNSS Breakout
|
GNSS Disciplined Oscillator
|
|
|---|---|---|---|
| GNSS Antenna | Dual | Single | Single |
| USB Connector | micro-B | Type-C | Type-C |
| Ethernet |
Yes 10/100 Base-T |
No |
Yes 10/100 Base-T |
| WiFi | No | No |
Yes - Network Bridge 10 Base-T |
| COM Ports | 4 | 4 |
1 - mosaic-T 1 - ESP32 |
| µSD Card Slot | Yes | Yes | Yes |
| Reset/Log Buttons | Yes | Yes | Yes |
| Logic-Level |
1.8V 3.3V |
3.3V |
3.3V 5V |
| PPS Signal | Header Pin | PTH Pad | SMA Connector |
| External Ref. Signal | SMA Connector | SMA Connector | SMA Connector |
| Enclosure Material | N/A | N/A | Aluminum |
| Dimensions | N/A | 63.5 x 50.8 x 0.8cm |
180.6 x 101.8 x 4.1cm Enclosure Only |
| Weight | N/A | 23g |
415g Enclosure Only |
In this guide we'll cover how to setup the mosaic-T Timing GNSS breakout board. Additionally, we also provide some guidelines for creating a GNSS disciplined oscillator, based upon our work with the SparkPNT GNSSDO. To follow along with this tutorial, at a minimum, users will need the following items:
-
Computer with an operating system (OS) that is compatible with all the software installation requirements (1)
Software Compatibility
The RxTools software suite from Septentrio, automatically installs the required USB-over-Ethernet driver and provides users with an interface for the receiver configuration, monitoring, data logging, and analysis. However, it only appears to be available for Windows and Linux operating systems.
-
USB 3.1 Cable A to C - 3 Foot - Used to interface with the mosaic-T GNSS Breakout (2)
- SparkFun GNSS Timing Breakout - mosaic-T (3)
- GNSS Multi-Band L1/L2/L5 Surveying Antenna
- A list of the compatible GNSS receiver software, is provided on the Septentrio website.
- If your computer doesn't have a USB-A slot, then choose an appropriate cable or adapter.
- For the best performance, use a compatible L1/L2/L5/L-Band GNSS antenna.
-
USB 3.1 Cable A to C - 3 Foot
CAB-14743 -
GNSS Timing Breakout - mosaic-T
GPS-28731 -
GNSS Multi-Band L1/L2/L5 Surveying Antenna - TNC (SPK6618H)
GPS-21801 -
Reinforced Interface Cable - SMA Male to TNC Male (10m)
CAB-21740 -
GNSS Magnetic Antenna Mount - 5/8" 11-TPI
PRT-21257 -
iFixit Anti-Static Wrist Strap
TOL-25572ESD Protection
The Septentrio mosaic-T module is sensitive to ESD. As recommended by the manufacturer, we highly recommend that users take the necessary precautions to avoid damaging their module. Use a proper grounding system to make sure that the working surface and the components are at the same electric potential.
Section Topics
This guide is divided into three sections:
- The Hardware section has two sub-sections that provide:
- An overview of the board's design, major components, and interfaces. Refer to this page for information on the connectors, breakout pins, and jumpers.
- Assembly instructions for this product's interfaces.
- The Software section has several sub-sections. The mosaic-T module has numerous capabilities and a multitude of ways to configure and interface with them. Without regurgitating all the information that is documented in Septentrio's user manuals and videos, we have tried to highlight a good majority of the module's aspects.
- In the Resources and Support sections, users can find the design files (KiCad files & schematic), relevant documentation (datasheets, white papers, etc.) and other helpful links on the Resources page. Lastly, the Troubleshooting Tips page includes helpful tips and instructions for how to receive technical support from SparkFun.