microSD Card
Not all microSD cards are created equal. The capacity, read/write speed, and format vary depending on the manufacturer. In order to log data to the microSD card, you will need to ensure that your memory card is formatted as FAT32. You can also use FAT16. If the memory card is formatted as a different memory card, the DataLogger IoT will not be able to recognize the microSD card.
Checking MicroSD Card Format
While you can simply insert the microSD card into your SparkFun IoT Node for LoRaWAN® and start logging, there may be a chance that the it will not recognize the memory card due to the format.
Checking MicroSD Card Format - Windows
To check to see if it is the correct format on a Windows you could head to the drive, right click, and select Properties.
microSD Card Properties
Once the properties are open, you should be able to tell what file system that the memory card uses. In this case, it was exFAT which is not compatible with the DataLogger IoT. You will need to reformat the memory card since it is not formatted as FAT32.
Check File System Windows
Checking MicroSD Card Format - macOS
To check to see if it is the correct format on a macOS, you could head to the drive on your desktop. Then right click, and select Get Info.
Get Info on MicroSD Card
A window will pop up indicating the microSD card properties. Under General: > Format:, you should be able to tell what file system that the memory card uses. In this case, it was exFAT which is not compatible with the DataLogger IoT. You will need to reformat the memory card since it is not formatted as FAT32.
exFAT
Download Raspberry Pi Imager
There are a few methods and programs available to reformat your microSD card as a FAT32. We found it easier to use the Raspberry Pi Imager Tool. Of course, you will only be using the tool to erase the contents of the microSD card and formatting it as a FAT32 system. You will not actually flash any image to the memory card. Click on the button below to download the tool from the Raspberry Pi Foundation. It is supported on Windows, macOS, and Ubuntu for x86.
Formatting as FAT32 using the Raspberry Pi Imager
After downloading and installing the software, open the Raspberry Pi Imager.
Raspberry Pi Imager
Under "Operating System", select "Erase" to "format card as FAT32."
Raspberry Pi Imager - Erase : Format as FAT32
Under "Storage", select the drive that the microSD card appeared as on your computer.
Raspberry Pi Imager - Select Storage Drive
When ready, select "Write". After a few minutes, the microSD card should be formatted with FAT32.
Raspberry Pi Imager - Write
Once the memory card has finished formatting, eject the microSD from your computer. To check to see if the microSD card is formatted as FAT32, you can check its properties as explained earlier with your operating system. Below shows a screenshot from a Windows and macOS showing that the microSD card reformatted as a FAT32 file system.
Check File System Windows
Check File System macOS