Quick Start Guide
-
SparkFun IoT Node for LoRaWAN®
SKU: WRL-26060
-
The SparkFun IoT Node for LoRaWAN® development board brings an entirely new level of usability to the often convoluted and configuration-intensive effort to set up a LoRaWAN®-based IoT Device. Combining the ease of LoRaWAN® setup and configuration delivered by the Digi X-ON™ system with the rapid prototyping provided by the SparkFun Qwiic ecosystem, the SparkFun IoT Node for LoRaWAN® development board accelerates IoT end-node creation and deployment.
Purchase from SparkFun
Getting Started with Digi
To get started, you'll need to have access to an HX15 Gateway (NA or EU version) and a Digi Account. If you've purchased the kit, a Gateway will be included. Digi has a great "Getting Started" video here. The kit also has a welcome card included that contains a QR Code. Scanning this code will take you to a URL where you can register for an account.
Register the LoRaWAN® Node
To provision a device, go to the following link, log in if necessary, and scan the Data Matrix on the XBee. We recommend using the camera on a mobile device/phone to scan the Data Matrix.
Data Matrix on the XBee
Note
If your DataMatrix scan is too blurry to work, wait a few moments and a manual entry will appear. From here you can manually enter the serial number to register your device. Alternatively, the mobile version has a zoom slider.
Digi Devices
Once you've registered your SparkFun IoT Node for LoRaWAN® board, you'll see it in your devices. Go to Network Dashboard -> Devices
Devices on Digi
Make sure you've got the correct Application selected like so:
Application on Digi
You'll see your device here.
Devices on Digi
Plug in a Qwiic Sensor
Our Qwiic Ecosystem has an array of plug and play sensors. For the pre-programmed firmware, you'll need the SparkFun Environmental Combo Breakout - ENS160/BME280 (Qwiic); plug it into the Qwiic port as shown here:
Connecting a Qwiic Sensor to the SparkFun IoT Node for LoRaWAN® Board
Reading Firmware
The SparkFun IoT Node for LoRaWAN® comes with Firmware that allows for a number of settings. By default, you can leave this be, but if you're interested in changing settings or verifying that everything is working you can pull up your favorite terminal (Putty, TeraTerm, etc), connect via serial to the port your LoRaWAN® has enumerated on, and you should see something like the following:
Connecting with TeraTerm
There are a number of different menus and settings you can scroll through at your leisure. Head over to the Firmware Tutorial for more information.
Reading Data
If nothing is entered in the above window, the LoRaWAN® will use default settings and start running.
Reading Data
This data will upload to your Digi Account via your gateway and can be seen here under Dashboard / Devices / Device Details:
Data Packets
Device Details and Management
Clicking on your device's EUI will take you to a page with Device Details, including the packets sent and gateway strength.
Device Details Page