Quick Start Guide
Header Pins
The primary function of the Pico Add-On Flipper is to flip the pin connections between its headers, on the top and bottom of the board.
Pin connections between the top and bottom headers of the Pico Add-On Flipper.
Board Orientation
The Pico Add-On Flipper can be connected above any of the Raspberry Pi Pico boards, as long as the USB silkscreen or Qwiic connector aligned with the USB connector of the Raspberry Pi Pico. This specific orientation must be utilized because of the pull-up resistors on the I2C pin and the RESET button connection to the RUN pin.
Pin connections between the top and bottom of the Pico Add-On Flipper.
XRP Controller Board
Below, is a demonstration of the Pico Add-On Flipper being utilized with the Experiential Robotics Platform (XRP) kit.
A demo of the Pico Add-On Flipper being utilized with the XRP kit.
Pico HAT
Pico Add-On Flipper can be utilized to connect multiple Pico HATs to any of the Raspberry Pi Pico boards.
A demo of the Pico Add-On Flipper being utilized with two Pico HATs.