SparkFun Qwiic Buzzer  v1.1.0-16-gb717328
Library for the SparkFun Qwiic Buzzer
Loading...
Searching...
No Matches
QwiicBuzzer Member List

This is the complete list of members for QwiicBuzzer, including all inherited members.

_theBussfDevBuzzerprotected
address()sfDevBuzzer
begin(const uint8_t address=SFE_QWIIC_BUZZER_DEFAULT_ADDRESS, TwoWire &wirePort=Wire)QwiicBuzzerinline
sfDevBuzzer::begin(sfTkII2C *theBus=nullptr)sfDevBuzzer
configureBuzzer(const uint16_t toneFrequency=SFE_QWIIC_BUZZER_RESONANT_FREQUENCY, const uint16_t duration=0, const uint8_t volume=4)sfDevBuzzer
deviceId(uint8_t &deviceId)sfDevBuzzer
firmwareVersionMajor(uint8_t &versionMajor)sfDevBuzzer
firmwareVersionMinor(uint8_t &versionMinor)sfDevBuzzer
isConnected()QwiicBuzzerinline
off()sfDevBuzzer
on()sfDevBuzzer
playSoundEffect(const uint8_t soundEffectNumber, const uint8_t volume)sfDevBuzzer
saveSettings()sfDevBuzzer
setAddress(const uint8_t &address)sfDevBuzzer
sfDevBuzzer()sfDevBuzzerinline