Arduino Setup
Arduino
This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-on, please review the following tutorials.
SparkFun FPC2534 Arduino Library
The SparkFun FPC2534 Arduino Library examples demonstrating how to use the FPC2534's main features including fingerprint enrollment, fingerprint template management and navigation over either I2C or UART. You can install the library with the Arduino Library manager tool by searching for "SparkFun FPC2534". If you'd prefer a manual install, you can download a ZIP of the library here.
Supported Boards
The I2C (Qwiic) interface for the SparkFun Fingerprint Sensor - FPC2534 Pro board is currently only supported on ESP32 and Raspberry RP2 (RP2040, RP2350) boards. The I2C Implemention of the FPC2534 device performs a dynamic payload transmission that is not supported by the Arduino Wire library. Because of this, a custom implementation is provided by this library for the ESP32 and RP2 platforms.