The Example2_Interrupts.ino example file can be accessed from the File > Examples > SparkFun TMAG5273 Arduino Library > Example2_Interrupts drop-down menu. This example builds upon the previous code in Example1_BasicReadings.ino. Instead of constantly streaming the sensor values from the TMAG5273, the microcontroller enables a magnetic threshold interrupt on the x-axis. Then, it waits until an interrupt is triggered on the INT pin before the data is retrieved through the I2C interface.
Example2_Interrupts.inoCode Verification
The code modification was last verified to be functional under the following parameters:
Arduino IDE Version: 2.2.1
Arduino Library Version: 1.0.3
Hardware Platform:
- SparkFun RedBoard Plus
- SparkFun Linear 3D Hall-Effect Sensor - TMAG5273 (Qwiic)
- SparkFun Mini Linear 3D Hall-Effect Sensor - TMAG5273 (Qwiic)
Required Modification
This code was developed to be utilized with the ESP32 on the IoT Motor Driver. Users will need to modify the example code, to utilize the interrupt pins of the ATmega328P on the RedBoard Plus. Replace uint8_t intPin = 4; with uint8_t intPin = 2; to utilize the D2 pin on the RedBoard Plus, which can handle interrupts.
Original Code:
// Interrupt pin used// NOTE: This pin is specific to the SparkFun IoT Motor Driveruint8_tintPin=4;
Modified Code:
// Interrupt pin used// NOTE: This pin is specific to the SparkFun IoT Motor Driveruint8_tintPin=2;
#include<Wire.h> // Used to establish serial communication on the I2C bus#include"SparkFun_TMAG5273_Arduino_Library.h" // Used to send and recieve specific information from our sensorTMAG5273sensor;// Initialize hall-effect sensor// I2C default addressuint8_ti2cAddress=TMAG5273_I2C_ADDRESS_INITIAL;// Interrupt pin used// NOTE: This pin is specific to the SparkFun IoT Motor Driveruint8_tintPin=4;// Start the flag as falseboolinterruptFlag=false;// ISR to print what interrupt was triggeredvoidisr1(){interruptFlag=true;}voidsetup(){Wire.begin();// Start serial communication at 115200 baudSerial.begin(115200);// Configure Interrupt PinpinMode(intPin,INPUT);// Attach interrupt to pin 4 as a digital, falling pinattachInterrupt(digitalPinToInterrupt(intPin),isr1,CHANGE);// Begin example of the magnetic sensor code (and add whitespace for easy reading)Serial.println("TMAG5273 Example 2: Interrupts");Serial.println("");// If begin is successful (0), then start exampleif(sensor.begin(i2cAddress,Wire)==true){Serial.println("Begin");}else// Otherwise, infinite loop{Serial.println("Device failed to setup - Freezing code.");while(1);// Runs forever}// Set interrupt through !INTsensor.setInterruptMode(TMAG5273_INTERRUPT_THROUGH_INT);// Set the !INT pin state - pulse for 10ussensor.setIntPinState(true);// Enable the interrupt response for the thresholdssensor.setThresholdEn(true);//int pinStatus = sensor.getInterruptPinStatus();pinMode(intPin,INPUT);// Set X, Y, Z, and T Thresholds for interrupt to be triggeredsensor.setXThreshold(5);// mT//sensor.setYThreshold(5); // mT//sensor.setZThreshold(5); // mT//sensor.setTemperatureThreshold(50); // CSerial.print("X Threshold Set: ");Serial.println(sensor.getXThreshold());}/* To use the other thresholds, simply change the names and use the other functions: - sensor.getYThreshold();- sensor.getZThreshold();- sensor.getTemperatureThreshold();*/voidloop(){if(interruptFlag==true){interruptFlag=false;Serial.println("X Threshold Reached!");intxThresh=sensor.getXThreshold();Serial.print("X Threshold: ");Serial.println(xThresh);if(sensor.getMagneticChannel()!=0)// Checks if mag channels are on - turns on in setup{floatmagX=sensor.getXData();floatmagY=sensor.getYData();floatmagZ=sensor.getZData();floattemp=sensor.getTemp();Serial.print("(");Serial.print(magX);Serial.print(", ");Serial.print(magY);Serial.print(", ");Serial.print(magZ);Serial.println(") mT");Serial.print(temp);Serial.println(" °C");}else{Serial.println("Mag Channels disabled, stopping..");while(1);}}else{Serial.println("Checking for Interrupts...");}delay(500);}
Hardware Connections
For this example, users simply need to connect their Qwiic Hall-Effect Sensor board to their microcontroller, utilizing the I2C interface and interrupt pin. Users can easily connect the I2C interface with the Qwiic connection system on their boards. To connect the interrupt pin, we recommend utilizing an IC-hook for a temporary connection.
For users with a development board without a Qwiic connector, the table below illustrates the required pin connections. Make sure that the logic-level of the sensor is compatible with the development board that is being connected.
Sensor Pin
Microcontroller Pin
RedBoard/Uno
INT
Interrupt Pin
D2
SCL
I2C - Serial Clock
SCL/A5
SDA
I2C - Serial Data
SDA/A4
3V3
Power: 1.7 to 3.6V
3.3V
GND
Ground
GND
Serial Monitor
This example waits until an interrupt is triggered by the magnetic threshold before data is retrieved from the TMAG5273 sensor. The data is then displayed in the Serial Monitor.
The magnetic flux (mT) and temperature (°C) values streamed from the TMAG5273 sensor into the Serial Monitor.
Tip
For this example to work, users will need to move a magnet near the sensor to trigger the interrupt.
Warning
The casing of rare Earth magnets is often conductive. Users should take precautions to avoid shorting out the components or electrical contacts with these types of magnets.