Setting Up Arduino

Arduino

This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-on, please review the following tutorials.

Note

If you've never connected an CH340 device to your computer before, you may need to install drivers for the USB-to-serial converter. Check out our section on "How to Install CH340 Drivers" for help with the installation.

SparkFun has written basic examples for the Qwiic Navigation Switch and is provided in the GitHub Hardware repository.

You will need the SparkFun I2C Expander Arduino Library to work with the Qwiic Navigation Switch's basic examples. You can obtain this library through the Arduino Library Manager by searching for "SparkFun I2C Expander Arduino Library". Find the one written by SparkFun Electronics and install the latest version. Users who prefer to manually install the library can get it from the GitHub Repository or download the .ZIP by clicking the button below: