Software Setup
Installation
The SparkFun Qwiic TMF882X Arduino Library is available within in the Arduino library manager, which is launched via the Sketch > Include Libraries > Manage Libraries … menu option in the Arduino IDE. Just search for SparkFun Qwiic TMF882X Library
Note
This guide assumes you are using the latest version of the Arduino IDE on your desktop. The following resources available at SparkFun provide the details on setting up and configuring Arduino to use this library.
General Use Pattern
After installing this library in your local Arduino environment, begin with a standard Arduino sketch, and include the header file for this library.
The next step is to declare the object for the SparkFun Qwiic TMF882X device used. Like most Arduino sketches, this is done at a global scope (after the include file declaration), not within thesetup() or loop() functions.
For all supported boards, the same object is used: SparkFun_TMF882X.
setup() function of this sketch, like all of the SparkFun qwiic libraries, the device is initialized by calling the begin() method. This method returns a value of true on success, or false on failure.
void setup()
{
Serial.begin(115200);
if(!myTMF882X.begin()){
Serial.println("Device failed to initialize");
while(1); // halt execution
}
Serial.println("Device is initialized");
}
loop() function can call the library to retrieve a single data sample from the connected TMF882X device.
Taken from the libraries Example 1, once a measurement is taken, the relevant data is output to the Serial device.
void loop()
{
delay(2000);
// get a Measurement
if(myTMF882X.startMeasuring(myResults))
{
// print out results
Serial.println("Measurement:");
Serial.print(" Result Number: ");
Serial.print(myResults.result_num);
Serial.print(" Number of Results: ");
Serial.println(myResults.num_results);
for (int i = 0; i < myResults.num_results; ++i)
{
Serial.print(" conf: ");
Serial.print(myResults.results[i].confidence);
Serial.print(" distance mm: ");
Serial.print(myResults.results[i].distance_mm);
Serial.print(" channel: ");
Serial.print(myResults.results[i].channel);
Serial.print(" sub_capture: ");
Serial.println(myResults.results[i].sub_capture);
}
Serial.print(" photon: ");
Serial.print(myResults.photon_count);
Serial.print(" ref photon: ");
Serial.print(myResults.ref_photon_count);
Serial.print(" ALS: ");
Serial.println(myResults.ambient_light);
Serial.println();
}
}
Advanced Data Collection
The TMF882X is unique when compared to our other qwiic libraries. Instead of data being returned directly from a method, measured data is passed back to the user via a callback function. This is how the underlying TMF882X SDK framework is designed and works well for interactive sensors like the TMF882X.
To receive data, a callback function is defined. For this example, we define a callback that prints out the detected data.
void onMeasurementCallback(struct tmf882x_msg_meas_results *myResults)
{
nSample++;
Serial.print("Sample Number: ");
Serial.println(nSample);
// print out results
// Not Shown here - This is similar to the output shown in the
// previous example.
}
setup() function of this example after the device is initialized, the defined callback function is registered with the TMF882 object.
void setup()
{
Serial.begin(115200);
if(!myTMF882X.begin()){
Serial.println("Device failed to initialize");
while(1); // halt execution
}
Serial.println("Device is initialized");
// set our callback function in the library.
myTMF882X.setMeasurementHandler(onMeasurementCallback);
}
For this example, in the loop() function, a measurement session is started, requesting that four samples be taken before returning from the method call. When data is detected by the TMF882X, the onMeasurementCallback() function, is called with the detected results. Once four measurements are taken, the measurement is finished and the TMF882X sensing session is stopped.
void loop()
{
delay(2000);
// get a measurement
// Have the sensor take 4 measurements.
//
// As measurements are taken, the results are sent to the above function,
// "onMeasurementCallback()"
nSample=0; // simple counter
myTMF882X.startMeasuring(4);
}
Library Provided Examples
The SparkFun Qwiic TMF882X Arduino Library, includes a wide variety of examples. These are available from the Examples menu of the Arduino IDE, and in the examplesfolder of this repository.
For a detailed description of the examples, see the Examples section of the documentation.