API Reference for the SFE_QUAD_Menu class
Brief Overview
The SFE_QUAD_Menu class allows the user to create a menu as a linked-list of SFE_QUAD_Menu_Item objects.
The SFE_QUAD_Menu _head points to the head (start) of the linked list.
_next points to the next SFE_QUAD_Menu_Item in the list.
The _next of the final SFE_QUAD_Menu_Item in the list is NULL.
_head is initially NULL. It is set to the address of the first SFE_QUAD_Menu_Item when addMenuItem is called.
There are several different types of menu item, as defined by the SFE_QUAD_Menu_Variable_Type_e enum:
SFE_QUAD_MENU_VARIABLE_TYPE_NONEcontains only the_itemNameas text- The name of the menu and perhaps some underscoring can be defined using this type
- This can be used to include 'empty' lines to separate parts of the menu
SFE_QUAD_MENU_VARIABLE_TYPE_SUB_MENU_STARTis a special type which defines the start of a sub-menu- Only this line is printed when the parent menu is displayed
- The menu items within the sub-menu are only printed when the sub-menu is opened
openMenuis called recursively to enter the sub-menus
SFE_QUAD_MENU_VARIABLE_TYPE_SUB_MENU_ENDmarks the end of a sub-menuSFE_QUAD_MENU_VARIABLE_TYPE_CODEcontains a pointer to a method which is called when this menu item is selectedSFE_QUAD_MENU_VARIABLE_TYPE_TEXTcontains ASCII text- e.g. a WiFi SSID or password
SFE_QUAD_MENU_VARIABLE_TYPE_BOOLis aboolwhich is toggled when the menu item is selectedSFE_QUAD_MENU_VARIABLE_TYPE_FLOATcontains afloat- There is an equivalent type for
double
- There is an equivalent type for
SFE_QUAD_MENU_VARIABLE_TYPE_INTcontains a signed integerint- There are equivalent types for
uint8_t,uint16_t,uint32_t,unsigned longandlong
- There are equivalent types for
Menu items are added with addMenuItem. An overloaded method allows CODE items to be added.
The menu variable can be read with getMenuItemVariable. The value is returned in a SFE_QUAD_Menu_Every_Type_t.
An overloaded method allows TEXT values to be read.
The menu variable can be set with setMenuItemVariable, typically to set its default or initial value.
An overloaded method allows TEXT to be set with a const char *.
Numeric menu items can have minimum and maximum values assigned using setMenuItemVariableMin and setMenuItemVariableMax.
The built-in getValueDouble method will then only allow values between the min and max to be entered.
setMenuPort defines which Stream (Serial port) will be used for the menu.
Debug messages can be displayed if required. setDebugPort sets the Stream (Serial port) for those.
The SFE_QUAD_Menu is not aware of what storage medium is being used by SFE_QUAD_Sensors.
The menu variables can be extracted as CSV text using getMenuVariableAsCSV. Higher methods are then
responsible for writing that text to storage. Likewise, higher methods will read the menu variables from
storage as CSV text. updateMenuVariableFromCSV will update the variable of the appropriate menu item using that text.
Initialization / Configuration
setMenuPort()
This method sets the Stream (Serial port) for the menu.
The supportsBackspace parameter can be set to true if the user is using a terminal emulator, like Tera Term,
which supports backspace. Existing TEXT items can then be edited instead of having to be entered in full each time.
| Parameter | Type | Description |
|---|---|---|
port |
Stream & |
The address of the Stream (Serial port) |
supportsBackspace |
bool |
Default is false. If true, existing TEXT items can be edited |
setDebugPort()
This method sets the Stream (Serial port) for menu debug messages - if desired.
| Parameter | Type | Description |
|---|---|---|
port |
Stream & |
The address of the Stream (Serial port) |
addMenuItem()
This method adds a menu item of the specified type to the linked-list.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item - the text that will be printed when this menu item is shown |
variableType |
SFE_QUAD_Menu_Variable_Type_e |
The variable type associated with this menu item |
| return value | bool |
true if the item is added successfully, otherwise false |
addMenuItem()
This method allows CODE menu items to be added.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item - the text that will be printed when this menu item is shown |
codePointer |
void (*)() |
The address of the method to be called when this menu item is selected |
| return value | bool |
true if the item is added successfully, otherwise false |
getMenuItemVariableType()
This method returns the variable type of this menu item.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
| return value | SFE_QUAD_Menu_Variable_Type_e |
The enum value representing the type |
getMenuItemVariable()
This method returns the value of the menu item variable.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
theValue |
SFE_QUAD_Menu_Every_Type_t * |
A pointer to the struct that will hold the value |
| return value | bool |
true if the item exists and the value is retrieved successfully, otherwise false |
getMenuItemVariable()
This method returns the value of a TEXT menu item variable.
The text is copied into theValue. maxLen should be set to the size of theValue.
The text is only copied if theValue is large enough to hold it.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
theValue |
char * |
A pointer to the char array that will hold the text |
maxLen |
size_t |
Defines how many characters theValue can hold |
| return value | bool |
true if the item exists and the value is retrieved successfully, otherwise false |
setMenuItemVariable()
This method sets the menu item variable in the linked-list with the value passed in theValue.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
theValue |
const SFE_QUAD_Menu_Every_Type_t * |
A pointer to the struct holding the value |
| return value | bool |
true if the item exists and the value is updated successfully, otherwise false |
setMenuItemVariable()
This method sets the menu item variable in the linked-list with the TEXT passed in theValue.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
theValue |
const char * |
A pointer to the text to be copied into the value |
| return value | bool |
true if the item exists and the text is copied successfully, otherwise false |
setMenuItemVariableMin()
This method sets the minimum permissible value for the menu item variable. This is used by the menu to check the value is in range.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
minVal |
const SFE_QUAD_Menu_Every_Type_t * |
A pointer to the struct holding the minimum value |
| return value | bool |
true if the item exists and the minimum value is updated successfully, otherwise false |
setMenuItemVariableMax()
This method sets the maximum permissible value for the menu item variable. This is used by the menu to check the value is in range.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The name of the menu item |
maxVal |
const SFE_QUAD_Menu_Every_Type_t * |
A pointer to the struct holding the maximum value |
| return value | bool |
true if the item exists and the maximum value is updated successfully, otherwise false |
The Menu
openMenu()
This method opens the menu on the chosen Stream (Serial port).
This method calls itself recursively when entering a sub-menu. start points to the address of the SUB_MENU_START menu item.
If start is NULL (the default), the menu starts at _head.
| Parameter | Type | Description |
|---|---|---|
start |
SFE_QUAD_Menu_Item * |
The address of the menu item to be shown first |
| return value | bool |
true if the menu item exists and the menu closes normally, otherwise false |
Menu Item Variable Storage
getNumMenuVariables()
The method returns the number of menu item variables which should be written to storage. The return value dictates how many
time getMenuVariableAsCSV is called.
| Parameter | Type | Description |
|---|---|---|
| return value | uint16_t |
The number of menu item variables requiring storage |
getMenuVariableAsCSV()
This method reads the menu item variable with index num and writes its name, type and value into var as CSV-format text.
Higher methods then write that CSV text to storage.
maxLen defines how many characters var can hold. The text is not written if var is too small.
| Parameter | Type | Description |
|---|---|---|
num |
uint16_t |
The menu item index |
var |
char * |
A pointer to a char array that the CSV text will be written to |
maxLen |
size_t |
The maximum number of characters var can hold |
| return value | bool |
true if the item exists and is copied successfully, otherwise false |
updateMenuVariableFromCSV()
line contains a menu variable in CSV format which has been read from storage.
This method updates the appropriate menu item variable with the value contained in the CSV text.
| Parameter | Type | Description |
|---|---|---|
line |
char * |
A pointer to a char array that contains the CSV |
| return value | bool |
true if the menu item exists and is updated successfully, otherwise false |
Helper Methods
getMenuChoice()
Ask the user to select a menu item.
| Parameter | Type | Description |
|---|---|---|
timeout |
unsigned long |
The timeout in milliseconds |
| return value | uint32_t |
The menu item selected, 0 if none or if a timeout occurred |
getValueDouble()
Ask the user to enter an integer or floating point value. Exponent-format values are also acceptable.
| Parameter | Type | Description |
|---|---|---|
timeout |
unsigned long |
The timeout in milliseconds |
value |
double * |
A pointer to the double which will hold the value |
| return value | uint32_t |
false if nothing is entered or a timeout occurred, otherwise true |
getValueText()
Ask the user to enter a TEXT entry, such as a WiFi password.
getValueText will automatically create a new char array to hold the text and returns a pointer to it.
The old char array is automatically deleted (freed).
| Parameter | Type | Description |
|---|---|---|
timeout |
unsigned long |
The timeout in milliseconds |
value |
char * * |
A pointer to a pointer to the dynamic char array that holds the text |
| return value | uint32_t |
true if text is entered within the timeout, otherwise false |
getMenuItemNameMaxLen()
Returns the maximum length of all of the menu item names. Used to format the menus correctly (space padding).
| Parameter | Type | Description |
|---|---|---|
| return value | size_t |
The maximum name length |
getMenuVariablesMaxLen()
Returns the likely maximum combined length of a full menu item (including min and max values if present). This is used to determine how much memory should be allocated to hold a menu item in CSV format.
| Parameter | Type | Description |
|---|---|---|
| return value | size_t |
The likely maximum length |
menuItemExists()
Returns a pointer to the menu item if it exists, otherwise returns NULL.
| Parameter | Type | Description |
|---|---|---|
itemName |
const char * |
The item name |
| return value | SFE_QUAD_Menu_Item * |
A pointer to the menu item (if it exists), otherwise NULL |
setMenuTimeout()
This method sets the menu timeout.
| Parameter | Type | Description |
|---|---|---|
newTimeout |
unsigned long |
The new menu timeout in milliseconds |
setMaxTextChars()
This method sets the maximum number of characters that can be entered into a TEXT value.
| Parameter | Type | Description |
|---|---|---|
newMax |
uint16_t |
The new maximum length |
setSupportsBackspace()
This method defines if the _menuPort supports backspace for TEXT entry.
| Parameter | Type | Description |
|---|---|---|
support |
bool |
true in the port supports backspace, otherwise false |
Member Variables
| Parameter | Type | Description |
|---|---|---|
_head |
SFE_QUAD_Menu_Item * |
A pointer to the first menu item in the linked-list, initially NULL |
_menuPort |
Stream * |
The address of the Stream (Serial port) to be used by the menu |
_debugPort |
Stream * |
The address of the Stream (Serial port) to be used for debug messages (if desired) |
_menuTimeout |
unsigned long |
The default menu timeout in milliseconds. Default is 10000 |
_maxTextChars |
uint16_t |
The maximum length of TEXT value entries. Default is 32 |
_supportsBackspace |
bool |
true if the port supports backspace, otherwise false. Default is false |