API Reference for the SFE_QUAD_Sensor class
Methods to allow the sensor's underlying Arduino Library be accessed in a homogeneous way:
- Return the sensor's name
- Return which I2C addresses are valid for this sensor
- Detect the sensor
- Begin the sensor (usually by calling the underlying library's
beginmethod) - Initialize the sensor (if required)
- Set a pointer to custom initialization code for this sensor
- Return the number of senses this sensor has
- Return the names of the senses
- Return the maximum length of the sense names (to aid menu formatting)
- Return a sense reading
- Return a count of the number of settings this sensor has (if any)
- Return the names of the settings
- Return the maximum length of the settings names (to aid menu formatting)
- Return the setting type
- Set a setting
- Return a count of the number of things which can be configured on this sensor
- Return the names of the things which can be configured on this sensor
- Return the maximum length of the configuration item names
- Return the configuration item type
- Return the configuration item
- Set the configuration item
Brief Overview
The SFE_QUAD_Sensor class allows that sensor's Arduino Library to be accessed in a homogeneous way.
It provides common methods for all sensor types, to allow SFE_QUAD_Sensors to read and configure the
sensor without needing to know the underlying library's methods.
Think of SFE_QUAD_Sensor as a thin layer which sits on top of the Arduino Library and which provides common access methods for it.
A sensor can have multiple senses. E.g. the BME280 has three : pressure, temperature and humidity.
A sensor may have several things which can be set. These are the settings.
E.g. the NAU7802 scale has two : zero offset (calculateZeroOffset) and calibration factor (calculateCalibrationFactor).
Configuration items are settings which are written to and read from storage (SD, EEPROM, LittleFS). They are used to record the sensor configuration and restore the configuration. Note: the configuration items may or may not be the same as the settings.
Individual SFE_QUAD_Sensor instances are connected in a linked-list. The SFE_QUAD_Sensor object contains a pointer to the
_next object in the list. The _next of the final SFE_QUAD_Sensor in the list is NULL.
The SFE_QUAD_Sensors object is responsible for creating the linked-list.
The possible (known) sensor types are defined in the enum SFEQUADSensorType in the SFE_QUAD_Sensors class.
Sensor detection and initialization will typically be performed as follows:
- For each sensor type in
enum SFEQUADSensorType:- If any Qwiic Muxes are detected, sensor detection is performed on all ports of all muxes.
- The possible I2C addresses for the sensor are requested using
getNumI2cAddressesandgetI2cAddress. - The sensor is detected using
detectSensor. This usually calls the sensor'sbeginmethod, but not always. - If the sensor is detected, it is added to the linked-list of
SFE_QUAD_Sensorobjects. Its I2C address is recorded. If it is connected through a Mux, the Mux address and port are recorded. - Once detection is complete, each sensor is initialized using
initializeSensor. - If a custom initializer has been defined, that is used in place of the standard initializer.
Reading the senses will typically be performed as follows:
- For each sensor in the linked-list:
getSenseCountreturns the number of senses this sensor has_logSense(an array ofbool) records if each individual sense is enabled for logging- All enabled senses are read using
getSenseReading
The sense names can be read using getSenseName. getSenseNameMaxLen aids menu formatting (space padding).
The class destructor ensures that all memory used by the linked-list is deleted (freed) correctly. This has been fully tested - see Example5 for details.
Most SFE_QUAD_Sensor methods are virtual as they need to be redefined by the methods of the individual sensors.
The individual sensor classes (e.g. SFE_QUAD_Sensor_ADS122C04) are derived. They inherit SFE_QUAD_Sensor and then redefine each method with their own.
Initialization / Configuration
getSensorName()
This method returns a pointer to the sensor's name.
| Parameter | Type | Description |
|---|---|---|
| return value | const char * |
A pointer to the sensor's name (ASCII text, null-terminated) |
getNumI2cAddresses()
This method returns the number of I2C addresses this sensor supports.
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The number of addresses |
getI2cAddress()
This method returns the I2C address for the index address.
| Parameter | Type | Description |
|---|---|---|
address |
uint8_t |
The address index |
| return value | uint8_t |
The I2C address |
detectSensor()
This method attempts to detect the sensor at address sensorAddress using Wire port port.
This method usually, but not always, calls the Arduino Library's begin method.
| Parameter | Type | Description |
|---|---|---|
sensorAddress |
uint8_t |
The sensor's I2C address (may be required by begin) |
port |
TwoWire & |
The Wire port the sensor is connected to (may be required by begin) |
| return value | bool |
true if the sensor is detected, false otherwise |
beginSensor()
This method calls the sensor's Arduino Library begin method.
| Parameter | Type | Description |
|---|---|---|
sensorAddress |
uint8_t |
The sensor's I2C address (may be required by begin) |
port |
TwoWire & |
The Wire port the sensor is connected to (may be required by begin) |
| return value | bool |
true if the sensor is begun successfully, false otherwise |
initializeSensor()
Perform any initialization methods this sensor requires. If a custom initializer has been defined, perform that instead.
| Parameter | Type | Description |
|---|---|---|
sensorAddress |
uint8_t |
The sensor's I2C address |
port |
TwoWire & |
The Wire port the sensor is connected to |
| return value | bool |
true if the sensor is initialized successfully, false otherwise |
setCustomInitializePtr()
Set a pointer to the custom initializer for this sensor.
| Parameter | Type | Description |
|---|---|---|
pointer |
void (*)() |
The address of the custom initializer |
The parameters for the custom initializer method are:
| Parameter | Type | Description |
|---|---|---|
sensorAddress |
uint8_t |
The sensor's I2C address (may be required) |
port |
TwoWire & |
The Wire port the sensor is connected to (may be required) |
_classPtr |
void * |
A pointer to the Arduino Library class instance for this sensor (required to access the class methods) |
getSenseCount()
Return the number of senses this sensor has.
| Parameter | Type | Description |
|---|---|---|
count |
uint8_t |
Pointer to the uint8_t which will hold the count |
| return value | bool |
true if the sensor exists, false otherwise |
getSenseName()
This method returns a pointer to the name of the sense with index sense.
| Parameter | Type | Description |
|---|---|---|
sense |
uint8_t |
The sense index |
| return value | const char * |
A pointer to the sense's name (ASCII text, null-terminated) |
getSenseNameMaxLen()
Return the maximum length of all sense names for this sensor. Useful for menu formatting (space padding).
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The maximum name length |
getSenseReading()
Read the sense with index sense. Return the reading as ASCII text in the char array reading.
The calling method is responsible for ensuring reading can hold the entire reading.
| Parameter | Type | Description |
|---|---|---|
sense |
uint8_t |
The sense index |
reading |
char * |
A pointer to a char array to hold the reading (ASCII text, null-terminated) |
| return value | bool |
true is the read is successful, false otherwise |
getSettingCount()
Return the count of the number of settings this sensor has.
| Parameter | Type | Description |
|---|---|---|
count |
uint8_t |
Pointer to the uint8_t which will hold the count |
| return value | bool |
true if the sensor exists, false otherwise |
getSettingName()
This method returns a pointer to the name of the setting with index sense.
| Parameter | Type | Description |
|---|---|---|
sense |
uint8_t |
The setting index |
| return value | const char * |
A pointer to the setting name (ASCII text, null-terminated) |
getSettingNameMaxLen()
Return the maximum length of all settings names for this sensor. Useful for menu formatting (space padding).
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The maximum name length |
getSettingType()
Return the setting type (SFE_QUAD_Sensor_Setting_Type_e) (BOOL, FLOAT, INT, etc.) for this setting.
| Parameter | Type | Description |
|---|---|---|
setting |
uint8_t |
The setting index |
type |
SFE_QUAD_Sensor_Setting_Type_e * |
Pointer to the enum which will hold the setting type |
| return value | bool |
true if the sensor exists, otherwise false |
setSetting()
Apply the value in value to the sensor setting with index setting.
| Parameter | Type | Description |
|---|---|---|
setting |
uint8_t |
The setting index |
value |
SFE_QUAD_Sensor_Setting_Every_Type_t * |
Pointer to the struct containing the setting |
| return value | bool |
true if successful, otherwise false |
getConfigurationItemCount()
Return the count of the number of configuration items this sensor has. Configuration items are settings which need to be written to and read from storage media.
| Parameter | Type | Description |
|---|---|---|
count |
uint8_t |
Pointer to the uint8_t which will hold the count |
| return value | bool |
true if the sensor exists, false otherwise |
getConfigurationItemName()
This method returns a pointer to the name of the configuration item with index configItem.
| Parameter | Type | Description |
|---|---|---|
configItem |
uint8_t |
The configuration item index |
| return value | const char * |
A pointer to the configuration item name (ASCII text, null-terminated) |
getConfigurationItemNameMaxLen()
Return the maximum length of all configuration item names for this sensor. Useful for menu formatting (space padding).
| Parameter | Type | Description |
|---|---|---|
| return value | uint8_t |
The maximum name length |
getConfigurationItemType()
Return the type (SFE_QUAD_Sensor_Setting_Type_e) (BOOL, FLOAT, INT, etc.) for this configuration item.
| Parameter | Type | Description |
|---|---|---|
configItem |
uint8_t |
The configuration item index |
type |
SFE_QUAD_Sensor_Setting_Type_e * |
Pointer to the enum which will hold the configuration type |
| return value | bool |
true if the sensor exists, otherwise false |
getConfigurationItem()
Read the sensor configuration item with index configItem and store it in value.
| Parameter | Type | Description |
|---|---|---|
configItem |
uint8_t |
The configuration item index |
value |
SFE_QUAD_Sensor_Setting_Every_Type_t * |
Pointer to the struct which will hold the value |
| return value | bool |
true if successful, otherwise false |
setConfigurationItem()
Apply the value in value to the sensor configuration item with index configItem.
| Parameter | Type | Description |
|---|---|---|
configItem |
uint8_t |
The configuration item index |
value |
SFE_QUAD_Sensor_Setting_Every_Type_t * |
Pointer to the struct containing the value |
| return value | bool |
true if successful, otherwise false |
Helper Methods
deleteSensorStorage()
This method is responsible for deleting (freeing) all dynamic memory used by the SFE_QUAD_Sensor object. It is called by the destructor.
Member Variables
| Parameter | Type | Description |
|---|---|---|
_sensorAddress |
uint8_t |
The I2C address of this sensor |
_muxAddress |
uint8_t |
The I2C address of the mux this sensor is connected to, 0 is none |
_muxPort |
uint8_t |
The mux port number this sensor is connected to, 0 if none |
_classPtr |
void * |
A pointer to the Arduino Library class instance for this sensor |
_next |
SFE_QUAD_Sensor * |
A pointer to the next sensor in the linked-list |
_logSense |
bool * |
A dynamic array of bool indicating if individual senses are enabled for logging |
_customInitializePtr |
void (*)() |
A pointer to the custom initializer for this sensor, NULL if none |
_sprintf |
SFE_QUAD_Sensors_sprintf |
An instance of SFE_QUAD_Sensors_sprintf to aid printing of double and exponent data |
Data Types
SFE_QUAD_Sensor_Every_Type_t
As the name suggests, this structure contains one of every data type used by the underlying Arduino Libraries.
It allows values to be passed between classes in a homogeneous, non-type-specific way.
The data type is defined by the associated SFE_QUAD_Sensor_Setting_Type_e enum.
typedef struct
{
bool BOOL;
float FLOAT;
double DOUBLE;
int INT;
uint8_t UINT8_T;
uint16_t UINT16_T;
uint32_t UINT32_T;
} SFE_QUAD_Sensor_Every_Type_t;
| Member | Type | Description |
|---|---|---|
BOOL |
bool |
A bool |
FLOAT |
float |
A float |
DOUBLE |
double |
A double |
INT |
int |
An int |
UINT8_T |
uint8_t |
A uint8_t |
UINT16_T |
uint16_t |
A uint16_t |
UINT32_T |
uint32_t |
A uint32_t |