API Reference for the SFE_QUAD_Sensors__EEPROM class
Methods to support writing/reading the sensors and menu configuration to/from EEPROM storage.
Methods
beginStorage()
This method: initializes the EEPROM; if required it also initializes the CRC-protected configuration structure.
| Parameter | Type | Description | 
|---|---|---|
| return value | bool | 
true is successful, otherwise false | 
writeConfigurationToStorage()
This method writes the menu and sensor configuration from the configuration dynamic char array into EEPROM. The CRC is also updated.
If append is false (default) the configuration will be overwritten.
If append is true, the configuration is appended to the end of any existing configuration data.
This can be useful if different sensors are connected for different logging runs. If a sensor configuration is included twice, both will be applied
with the newest configuration superseding the older.
| Parameter | Type | Description | 
|---|---|---|
append | 
bool | 
If false (default) new data overwrites old. If true, new data is apended to old | 
| return value | bool | 
true if the data is written successfully, otherwise false | 
readConfigurationFromStorage()
This method reads the menu and sensor configuration from EEPROM, copying it into the configuration dynamic char array.
| Parameter | Type | Description | 
|---|---|---|
| return value | bool | 
true if the data is read successfully, otherwise false | 
endStorage()
This method would be used to call the storage's end method - if it had one. For EEPROM, it does nothing and simply returns true.
| Parameter | Type | Description | 
|---|---|---|
| return value | bool | 
Always true |