API Reference for the SFE_QUAD_Sensors_sprintf class
Helper methods to support printing of double and exponent-format data.
Helper Methods
_dtostrf()
Convert double to string (included because not all platforms support dtostrf correctly).
It is the calling method's responsibility to ensure buffer is large enough to contain the complete string.
| Parameter | Type | Description |
|---|---|---|
value |
double |
The double to be converted to string |
buffer |
char * |
A pointer to a char array to hold the text |
| return value | char * |
A pointer to the char after the final one printed |
_etoa()
Convert double to ASCII text using exponent format.
It is the calling method's responsibility to ensure buffer is large enough to contain the complete string.
| Parameter | Type | Description |
|---|---|---|
value |
double |
The double to be converted to string |
buffer |
char * |
A pointer to a char array to hold the text |
| return value | char * |
A pointer to the char after the final one printed |
expStrToDouble()
Convert exponent-format string to double.
| Parameter | Type | Description |
|---|---|---|
str |
const char * |
A pointer to the string to be converted |
value |
double * |
A pointer to the double which will hold the result |
| return value | bool |
true if the conversion was successful, false otherwise |
setPrecision()
Set the precision (number of decimal places) to be used by _dtostrf and _etoa.
Set this before calling mySensors.detectSensors();:
mySensors._sprintf.setPrecision(5);
| Parameter | Type | Description |
|---|---|---|
prec |
unsigned char |
The precision |
getPrecision()
Returns the current precision.
| Parameter | Type | Description |
|---|---|---|
| return value | unsigned char |
The precision |
Member Variables
| Parameter | Type | Description |
|---|---|---|
_prec |
unsigned char |
The precision (number of decimal places) to be printed |