Skip to content

Hookup Guide

Introduction

  • SparkFun Qwiic WAV Trigger Pro
    SKU: WIG-25860


    Product Thumbnail

  • The Qwiic WAV Trigger Pro is the latest evolution of the line of high-fidelity polyphonic audio players from robertsonics. The Qwiic WAV Trigger Pro improves on the previous versions with a more powerful processor, enhanced MIDI processing - including velocity switching and multi-timbral support - and MIDI USB Device (Default) and MIDI USB Host support, all in a smaller 1.75" x 1.5" footprint!

    The Qwiic WAV Trigger Pro supports up to 4096 uncompressed 16-bit, 44.1kHz mono and stereo WAV files matching CD audio quality. The WAV Trigger Pro supports polyphony and can play and mix up to 24 tracks simultaneously and independently with exceptionally low latency (7ms typically). Control track playback via either 8 programmable trigger inputs, I2C (Qwiic), or MIDI (USB, Serial UART, or Qwiic). The board can function as both a USB MIDI device and host meaning if the WAV Trigger Pro has power in USB MIDI Host mode it can supply up to 500mA@5V to a connected MIDI device over USB-C allowing for USB MIDI control with no computer required.

    Purchase from SparkFun

Required Materials

The Qwiic WAV Trigger Pro requires a few additional items as well as some through-hole soldering to get up and running properly. If you'd like to follow along with the examples in this tutorial, you'll want at least the following items along with a pair of corded headphones. If you'd like to follow the USB MIDI Host example, make sure you have a USB MIDI device like a MIDI Keyboard or Pad.

Qwiic & Arduino Materials

Users who wish to use the Qwiic WAV Trigger Pro with the Qwiic ecosystem and Arduino library, you may need one or more of the following products:

Soldering Tools & Accessories

The Qwiic WAV Trigger Pro does require some through-hole soldering for the best, permanent installation and uses. Users will need to at least solder to the audio output pins as they are routed to a 0.1"-spaced PTH header. If you need any soldering tools or materials, check out the following products:

Suggested Reading

Before getting started with this guide and the Qwiic WAV Trigger Pro, you may want to read through some of the tutorials linked below if you're not familiar with the concepts covered in them: