Hardware Overview
Design Files
-
Design Files
- Schematic
- KiCad Files
- STEP File
- Board Dimensions:
- 1.75" x 1.25" (44.45mm x 31.75mm)
-
Major changes between the original USB RFID Reader (left) and new USB-C RFID Reader (right). -
- USB Connector
- We have updated the USB mini-B connector to the more prevalent USB-C connector.
-
- USB-to-Serial Converter
- We have transitioned to a most cost-effective the USB-to-serial converter, the CH340C from WCH.
-
- PTH Breakout Pins
- The PTH pins have been relocated and now feature silkscreen labels.
Manipulate 3D Model
Controls Mouse Touchscreen Zoom Scroll Wheel 2-Finger Pinch Rotate Left-Click & Drag 1-Finger Drag Move/Translate Right-Click & Drag 2-Finger Drag
Dimensions of the USB-C RFID Reader. Need more measurements?
For more information about the board's dimensions, users can download the KiCad files for this board. These files can be opened in KiCad and additional measurements can be made with the measuring tool.
KiCad - Free Download!
KiCad is free, open-source CAD program for electronics. Click on the button below to download their software. (*Users can find out more information about KiCad from their website.)
Download Measuring Tool
This video demonstrates how to utilize the dimensions tool in KiCad, to include additional measurements:
-
Board Layout
The USB-C RFID Reader has the following features:
-
- USB-C Connector
- The primary interface for the USB-C RFID Reader. It provides power to the RFID module and reads any serial data output, through a CH340C converter.
-
- PTH Breakout Pins
- Two sets of 0.1" pitch PTH pins that breakout the primary connections to the RFID module.
-
- Female Headers
- Two sets of 2mm pitch, female headers that are compatible with the ID-Innovations Tiny, non-write, RFID modules (excluding the Mifare readers, marked with an MF).
-
- Buzzer
- An audio indicator for card reads.
-
READLED- A green status indication LED for card reads.
-
- CH340C USB-to-Serial Converter
- The CH340C converts the serial output from the RFID module for the USB interface.
Breakout Pins
The primary function of the USB-C RFID Reader is to flip the pin connections between its headers, on the top and bottom of the board.
-
IN_RANGE- This pin is toggled when an RFID tag is in range.
-
PRESENT- This output is only used when the output data format is set to Magnetic Emulation.
-
GND- The common ground or the 0V reference for the voltage supplies.
-
VUSB- The voltage from the USB-C connector, usually 5V.
-
TX- Connected to the
TXpin of the CH340C
-
RST- Connected to the
RES(reset) pin of the RFID module. By default, this is pin is pulled high by theVUSBpin.
-
LED- This pin is activated when a tag is read and triggers the
READLED and buzzer on the board.
-
DATA0/DATA1- The behavior of these pins vary, depending on the output data format that is chosen.
-
ANT2/ANT1- These pins are utilized for an external antennal. This is likely to be necessary for any of the ID-3XX modules. Users should consult with their module's datasheet.
Jumpers
There are five jumpers on the back of the board that can be used to easily modify the hardware connections on the board.
The jumpers on the top of the USB-C RFID Reader.
Never modified a jumper before?
Check out our Jumper Pads and PCB Traces tutorial for a quick introduction!
SHLD- This jumper can be cut to disconnect the shielding of the USB-C connector from the
GNDplane of the board BUZZ- This jumper can be cut to remove power from the buzzer.
READ- This jumper can be cut to remove power from the green
READLED. MD1/MD2-
These jumpers can be modified to control the format of the RFID module's data output between
ASCII,Magnet Emulation, orWiegand26. By default, the jumpers are set for theASCIIdata format.Data Format MD1MD2ASCII Open Open Magnet Emulation Open Closed Wiegand26 Closed Open Info
The CH340C can only interpret data in the
ASCIIformat. An external microcontroller or device should be utilized when another data format is chosen.