Introduction
The SparkFun RTK EVK (Evaluation Kit) is the perfect development platform for your fixed or mobile high-precision positioning and navigation needs. In terms of connectivity, the SparkFun RTK EVK has the lot: WiFi / BT, Ethernet and LTE cellular! We called it the EVK (Evaluation Kit) as it truly covers all the options: L1 + L2 RTK GNSS, with L-Band correction built-in if needed, running on an agile processor with memory to spare!
In this tutorial we'll go over the hardware, assembly, and how get started with the SparkFun RTK.
Kit Contents
The SparkFun RTK EVK comes with everything you need to get up and running. Our kit includes:
- 1x Cased GNSS Receiver
- 1x L1/L2/L5 GNSS Surveying Antenna
- 1x Reinforced RG58 TNC-SMA Cable (10m)
- 1x RPSMA WiFi / Bluetooth Antenna
- 2x SMA LTE Cellular Antennas
- 1x 32GB microSD Card (Class 10)
- 1x USB-C Power Supply (5V, 1A wall charger)
- 1x USB-C Cable (A to C, 2m)
- 1x Ethernet Cable (CAT-6, 1m)
- 1x Hologram eUICC nano-SIM card
GNSS Mounting Accessories
Depending on where you are installing the SparkFun RTK EVK, you also might need some mounting accessories to mount the GNSS antenna. You will want to mount the antenna in a location with the best view to of the sky (i.e. a roof).
The RTK EVK comes with a custom extruded aluminum enclosure. The slotted flanges make it easy to install and secure the enclosure in many locations. If you are going to permanently install it up on a roof, you're going to need a suitable weatherproof box too. We found that the Orbit 57095 - also available from Amazon - was a good one back when we put together our first DIY GNSS Reference Station.
AC Not Required!
The Orbit enclosure comes with a built-in power outlet, but you don't actually need it! The RTK EVK can be powered by Power-over-Ethernet (PoE), meaning all you really need to run up to the roof is a standard 8-core CAT-6 Ethernet cable. Choose a PoE Ethernet Switch that meets your needs. We have had good experiences with the TP-Link TL-SG1005P - available from many retailers including Amazon.
GNSS Interface Cable
The following interface cables are great if say you are mounting the SparkFun RTK EVK in your home on a desk or lab bench and installing the antenna outdoors.
Memory Cards
Finally, if you're going to be logging a lot of data, you might want to stock up on 32GB microSD cards too. The RTK EVK can log 'raw' GNSS data messages (RAWX and SFRBX) at 4Hz if desired. At that rate, you're logging about 10kB per second, close to 40MB per hour or 1GB per day!
Tools
Below are a few tools and accessories that you may need when connecting to the I/O terminal block on the back of the RTK EVK.
Suggested Reading
If you aren’t familiar with the following concepts, we also recommend checking out a few of these tutorials before continuing.
You may also be interested in the following blog posts on GNSS technologies.