Configure from Display
- EVK:
- Facet mosaic:
- Postcard:
- Torch:
- TX2:

Configuration from the Display
On devices that have an external display, pressing buttons can navigate through a limited set of menus and options.
RTK EVK

Front face of the RTK EVK
The RTK EVK has a 1.3" OLED with a MODE button and a recessed RESET button.
- Pressing the button will display the configuration menu.
- Single-tapping the button will advance the menu.
- Double-tapping the button will select the highlighted item.
- If there is no button press for 2 seconds, the menu will exit.
- Pressing the reset button will immediately reset the system.
RTK Facet mosaic

Front face of the RTK Facet mosaic
The RTK Facet mosaic has a 0.96" OLED with a single POWER/SETUP button.
- Pressing the button will display the configuration menu.
- Single-tapping the button will advance the menu.
- Double-tapping the button will select the highlighted item.
- If there is no button press for 2 seconds, the menu will exit.
RTK Postcard

Portability shield shown mounted to the RTK Postcard
The RTK Postcard comes without a display. If a user elects to add the Portability Shield, a 1.3" OLED and 5-way joystick are enabled as shown above. A Navigation Switch Cover is also shown.
- Any press of the joystick will open the menu.
- Pressing down or right will move forward a menu item.
- Pressing up or left will move back a menu item.
- Pressing in the middle of the joystick will select.
- If there is no button press for 2 seconds, the menu will exit.