Configure with Settings File
- EVK:
- Facet mosaic:
- Postcard:
- Torch:
- TX2:

SparkFun RTK Settings File
All device settings are stored both in internal memory and an SD card (if supported and if one is detected). The device will load the latest settings at each power on. If there is a discrepancy between the internal settings and an external settings file then the external settings file will be used. This allows a collection of RTK products to be identically configured using one 'golden' settings file loaded onto an SD card.
All system configuration can be done by editing the SFE_[Platform]_Settings_0.txt file (example shown above) where [Platform] is Facet, Express, Surveyor, etc and 0 is the profile number (0, 1, 2, 3). This file is created when a microSD card is installed.
Danger
The settings are clear text but there are no safety guards against setting illegal states. It is not recommended to use this method unless You Know What You're Doing®.
Keep in mind:
- Not all devices have an SD card slot (ie, RTK Torch) and therefore do not support this configuration method.
- The settings file contains hundreds of settings.
-
The SD card file "SFE_EVK_Settings_0.txt" is used for Profile 1, SD card file "SFE_EVK_Settings_1.txt" is used for Profile 2, etc.
Note
The
Settings_0is for Profile 1,Settings_1is for Profile 2,Settings_2is for Profile 3... -
When switching to a new profile, the settings file on the SD card with all settings will be created or updated. The internal settings will not be updated until you switch to the profile. Additionally, the file for a particular profile will not be created on the SD card until you switch to that profile.
- It is not necessary that the settings file on the SD card have all of the settings.
Example
For example, if you only wanted to set up two wireless networks for Profile 2, you could create a file named SFE_Express_Settings_1.txt that only contained the following settings:
profileName=a name you choose
enableTcpServer=1
wifiNetwork0SSID=your SSID name 1
wifiNetwork0Password=your SSID password 1
wifiNetwork1SSID=your SSID name 2
wifiNetwork1Password=your SSID password 2
wifiConfigOverAP=0
These settings on the SD card will overwrite the settings in the RTK Express internal memory. Once you select this profile on your RTK Express, the SD card file will be overwritten with all of the merged settings.
Forcing a Factory Reset

If the device has been configured into an unknown state the device can be reset to factory defaults. Power down the RTK device and remove the SD card. Using a computer and an SD card reader, open the SFE_[Platform]_Settings_0.txt file where [Platform] is Facet, Express, Surveyor, etc and 0 is the profile number (0, 1, 2, 3). Modify the sizeOfSettings value to -1 and save the file to the SD card. Reinsert the SD card into the RTK unit and power up the device. Upon power up, the device will display 'Factory Reset' while it clears the settings.
Note
A device may have multiple profiles, ie multiple settings files (SFE_EVK_Settings_0.txt, SFE_EVK_Settings_1.txt, etc). All settings files found on the SD card must be modified to guarantee the factory reset.