Configure with u-center
- EVK:
- Facet mosaic:
- Postcard:
- Torch:
- TX2:
On devices that have a u-blox GNSS receiver, the ZED-F9P GNSS module can be configured independently using the u-center software from u-blox by connecting a USB cable to the Config u-blox USB connector. Settings can be saved to the module between power cycles. For more information please see SparkFun’s Getting Started with u-center by u-blox.
However, because the ESP32 does considerable configuration of the ZED-F9P at power on it is not recommended to modify the settings of the ZED-F9P using u-center. Nothing will break but your changes will likely be overwritten at the next power cycle.