Updating u-blox Firmware
- EVK:
- Facet mosaic:
- Postcard:
- Torch:
- TX2:
The u-blox ZED-F9P is the GNSS receiver inside the RTK EVK. The RTK EVK also contains the u-blox NEO-D9S for receiving L-Band corrections. The following describes how to update the firmware on the ZED-F9P and NEO-D9S modules.
The firmware loaded onto the ZED-F9P and NEO-D9S receivers is written by u-blox and can vary depending on the manufacture date. The RTK Firmware (that runs on the ESP32) is designed to flexibly work with any u-blox firmware. Upgrading the ZED-F9x/NEO-D9S is a good thing to consider but is not crucial to the use of RTK products.
Not sure what firmware is loaded onto your RTK product? Open the System Menu to display the module's current firmware version.
The firmware on u-blox devices can be updated using a Windows-based GUI or u-center. A CLI method is also possible using the ubxfwupdate.exe tool provided with u-center. Additionally, u-blox offers the source for the ubxfwupdate tool that is written in C. It is currently released only under an NDA so contact your local u-blox Field Applications Engineer if you need a different method.
Update Using Windows GUI

SparkFun RTK u-blox Firmware Update Tool
The SparkFun RTK u-blox Firmware Update Tool is a simple Windows GUI and python script that runs the ubxfwupdate.exe tool. This allows users to directly update module firmware without the need for u-center. Additionally, this tool queries the module to verify that the firmware type matches the module. Because the RTK EVK contains two u-blox modules that both appear as identical serial ports, it can be difficult and perilous to know which port to load firmware. This tool prevents ZED-F9P firmware from being accidentally loaded onto a NEO-D9S receiver and vice versa.
The SparkFun RTK u-blox Firmware Update Tool will only run on Windows as it relies upon u-blox's ubxfwupdate.exe. The full, integrated executable for Windows is available here.
- Attach the RTK device's USB port to your computer using a USB cable
- Turn the RTK device on
-
Open Device Manager to confirm which COM port the device is operating on
Device Manager showing USB Serial port on COM14 -
Get the latest binary firmware file from the ZED Firmware, NEO Firmware folder, or the u-blox website
- Run RTK_u-blox_Update_GUI.exe (it takes a few seconds to start)
- Click the Firmware File Browse and select the binary file for the update
- Select the COM port previously seen in the Device Manager
- Click Update Firmware
Once complete, the u-blox module will restart.
Update Using u-center
If you're familiar with u-center a tutorial with step-by-step instructions for locating the firmware version as well as changing the firmware can be found in How to Upgrade Firmware of a u-blox Receiver.
ZED-F9P Firmware Changes
This module is used in the RTK EVK. It is capable of both Rover and base modes.
Most of these binaries can be found in the ZED Firmware/ZED-F9P folder.
All field testing and device-specific performance parameters were obtained with ZED-F9P v1.30.
- v1.32 has a few SPARTN protocol-specific improvements. See release notes. This firmware is required for use with the NEO-D9S and the decryption of PMP messages.
- v1.30 has a few RTK and receiver performance improvements, I2C communication improvements, and most importantly support for SPARTN PMP packets. See release notes.
- v1.13 has a few RTK and receiver performance improvements but introduces a bug that causes the RTK Status LED to fail when SBAS is enabled. See release notes.
- v1.12 has the benefit of working with SBAS and an operational RTK status signal (the LED illuminates correctly). See release notes.
NEO-D9S Firmware Changes
This module is used in the EVK to receive encrypted PMP messages over ~1.55GHz broadcast via a geosynchronous Inmarsat.
This binary file can be found in the NEO Firmware folder.
- v1.04 Initial release.
As of writing, no additional releases of the NEO-D9S firmware have been made.