Skip to content

Hardware

  • EVK:
  • Facet mosaic:
  • Postcard:
  • Torch:
  • TX2:

Note

The debug menus are meant for debugging and development, and not for regular configuration. The unit will not be damaged if these settings are modified, but support is limited.

Hardware Debug Menu

Hardware Debug Menu

From the System Menu, pressing 'h' will enter the Hardware Debug Menu. This menu controls various advanced settings, mostly used to enable the printing of verbose debugging messages.

  • 1 - Turn on/off the regular battery status message over serial config.
  • 3 - Turn on/off the display of TP time sync information.
  • 4 - Turn on/off the debug messages associated with log files, including the parsing results of NMEA and other messages.
  • 5 - Turn on/off the regular logging size status message over serial config.
  • 7 - Display the movement of bytes through the GNSS circular buffer to consumers including the SD logging buffer.
  • 9 - Turn on/off verbose GNSS library messages.
  • 10 - Turn on/off the display of interactions with the PointPerfect ZTP interface.
  • 11 - Turn on/off debug messages associated with the set up of the Tilt/IMU sensor.
  • 12 - Turn on/off debug messages when NMEA messages are modified with Tilt information.
  • 13 - Used for upgrading the GNSS receiver.
  • 14 - Enable/disable the use of PSRAM.
  • 15 - Turn on/off debug messages when the ESP-NOW radio is active.
  • 16 - Turn on/off debug messages when the LoRa radio is active.
  • 18 - Display how many bytes are being used by littleFS.
  • 19 - Display verbose messages while the CLI is being used.
  • 20 - Set the amount of time between each LIST message being sent over the UART.
  • 21 - Set the amount of time required between button presses to signify a double-tap.
  • 22 - Turn on/off debug messages during the GNSS is configuration process.
  • 23 - Erase the GNSS configuration to force a re-configuration.
  • e - Format the littleFS file system.
  • t - Display test screen.
  • r - Restart the device.