System Menu
- EVK:
- Facet mosaic:
- Postcard:
- Torch:
- TX2:

System Menu accessed over serial
The System Menu shows a variety of system information including a full system check to verify what is and what is not online. For example, if an SD card is detected it will be shown as online. Not all RTK devices have all hardware options. For example, the RTK Torch does not have an SD slot so its status and configuration will not be shown.
This menu is helpful when reporting technical issues or requesting support as it displays helpful information about the current GNSS firmware version, and which parts of the unit are online.
WiFi Interface
Because of the nature of these controls, the WiFi Config page shows different information than the Serial configuration.

System Config Menu on WiFi Config Page
System Information

System Menu Header Information
The header of the system menu contains various system metrics.
In order of appearance:
- System Date/time
- Device Mode
- GNSS status including receiver type and firmware version
- Unique ID assigned to the GNSS receiver
- GNSS information including SIV, HPA, Lat/Lon/Alt
- Battery information (if supported)
- Bluetooth MAC (ending) and radio status
- WiFi MAC (full)
- System Uptime
- NTRIP Client/Server uptime (if enabled)
- MQTT Client uptime (if enabled)
- Parser statistics
Mode Switch

System Menu Options serial menu
The device can be in Rover, Base, or WiFi Config mode. The selected mode will be entered once the user exits the menu system.
- Base - The device will reconfigure for base mode. It will begin transmitting corrections over Bluetooth, WiFi (NTRIP Server, TCP, etc), or other (ESP-NOW, external radio if compatible, etc).
- BaseCaster - The device will reconfigure for base caster mode. It will broadcast a WiFi access point, allow incoming NTRIP Client connections on port 2101. See BaseCast Mode.
- Rover - This is the default mode. The device transmits its NMEA and other messages (if enabled) over Bluetooth. It can receive corrections over Bluetooth (or other transport methods such as NTRIP Client) to achieve RTK Fix.
- Web Config - The device will shut down GNSS operations and serve a configuration web page over WiFi or ethernet.
- Shut Down - If supported, the device will immediately shut down.
Settings

System Menu Options serial menu
- a - On devices that support it, a beeper is used to indicate various system states (system power on/off, tilt compensation in use, etc). This can be disabled if desired.
- b - Change the Bluetooth protocol. By default, the RTK device begins dual broadcasting over Bluetooth Classic SPP (Serial Port Profile) and Bluetooth Low-Energy (BLE). The following options are available: Dual, Classic, BLE, or Off. Bluetooth v2.0 SPP (Serial Port Profile) is supported by nearly all data collectors and Android tablets. BLE is used for configuration and to be compatible with Apple iOS-based devices. Additionally, the Bluetooth radio can be turned off.
- c - On devices that support it, a device will continue to operate until the battery is exhausted. If desired, a timeout can be entered: If no charging is detected, the device will power off once this amount of time has expired.
- d - Enters the Debug Software menu that is for advanced users.
- e - Controls the printing of local characters (also known as 'echoing').
- f - On devices that support it, show any files on the microSD card (if present).
- h - Enters the Debug Hardware menu that is for advanced users.
- n - Enters the Debug Network menu that is for advanced users.
- o - Enters the Configure RTK operation menu that is for advanced users.
- p - Enters the Configure periodic print menu that is for advanced users.
- r - Reset all settings to default including a factory reset of the GNSS receiver. This can be helpful if the unit has been configured into an unknown or problematic state. See Factory Reset.
- u - Change between metric and Imperial units. This only modifies the units shown on serial status messages and on the display (if available), it does not change NMEA output.
- z - A local timezone in hours, minutes and seconds may be set by pressing 'z'. The timezone values change the RTC clock setting and the file system's timestamps for new files.
- ~ - If desired, the external button(s) can be disabled to prevent accidental mode changes.
Note
Bluetooth SPP cannot operate concurrently with ESP-NOW radio transmissions. Therefore, if you plan to use the ESP-NOW radio system to connect RTK products, the BLE protocol must be used to communicate over Bluetooth to data collectors. Alternatively, ESP-NOW works concurrently with WiFi so connecting to a data collector over WiFi can be used.
Factory Reset
If a device gets into an unknown state it can be returned to default settings using the WiFi or Serial interfaces.
Note
On devices that support an SD card, a factory reset can also be accomplished by editing the settings files. See Force a Factory Reset for more information. During a factory reset, log files and any other files on the SD card are not removed or modified.

Issuing and confirming a Factory Reset
If a device gets into an unknown state it can be returned to default settings. Press 'r' then 'y' to confirm. Factory Default will erase any user settings and reset the internal receiver to stock settings. If SD is supported, any settings file and commonly used coordinate files on the SD card associated with the current profile will be removed.

Enabling and Starting a Factory Reset
Factory Defaults will erase any user settings and reset the internal receiver to stock settings. To prevent accidental reset the checkbox must first be checked before the button is pressed. Any logs on SD are maintained. Any settings file and commonly used coordinate files on the SD card associated with the current profile will be removed.