User Profiles Menu
- EVK:
- Facet mosaic:
- Postcard:
- Torch:
- TX2:

User Profiles Menu in the serial interface

User Profiles Menu in the Web Config interface
Profiles are a very powerful feature. A profile is a complete copy of all the settings on the RTK product. Switching profiles changes all the settings in one step. This is handy for creating a complex setup for surveying, and a different setup for an NTRIP-enabled base station. Rather than changing the variety of parameters, a user can simply switch profiles.
Profiles can be selected, renamed, reset to defaults, and completely erased from the User Profiles menu.
User Profile Selection via Display

Multiple Profiles on Menu
On devices that have a display, if more than one profile is defined, the profiles will be displayed and selectable by using the Power/Setup button. Only the first 7 characters of a profile's name will be shown on the menu. Once a profile has been selected, the device will reboot using that profile.
Print Profile
A profile can be printed to the terminal. This dumps the entire settings file and can be helpful for debugging or getting support.

Printing a Profile