Skip to content

Profiles Menu

Surveyor: Feature Not Supported / Express: Feature Supported / Express Plus: Feature Supported / Facet: Feature Supported / Facet L-Band: Feature Supported

Profiles Menu

User Profiles Menu

Profiles are a very powerful feature. A profile is a complete copy of all the settings on the RTK product. Switching profiles changes all the settings in one step. This is handy for creating a complex setup for surveying, and a different setup for an NTRIP-enabled base station. Rather than changing the variety of parameters, a user can simply switch profiles.

Multiple Profiles on Menu

Multiple Profiles on Menu

If more than one profile is defined, the profiles will be displayed and selectable by using the Power/Setup on the Facet or Setup on the Express and Express Plus. Profiles can be named up to 50 characters; only the first 7 characters will be shown on the menu.

Surveyor Profiles

Because the Surveyor does not have a display, profiles are not available. The Base/Rover switch allows simple pre-set configurations to be toggled.