Profiles Menu
Surveyor:
/ Express:
/ Express Plus:
/ Facet:
/ Facet L-Band:
/ Reference Station: ![]()

Profiles Menu on the WiFi config page

User Profiles Menu
Profiles are a very powerful feature. A profile is a complete copy of all the settings on the RTK product. Switching profiles changes all the settings in one step. This is handy for creating a complex setup for surveying, and a different setup for an NTRIP-enabled base station. Rather than changing the variety of parameters, a user can simply switch profiles.

Multiple Profiles on Menu
If more than one profile is defined, the profiles will be displayed and selectable by using the Power/Setup on the Facet or Setup on the Express and Express Plus. Profiles can be named up to 50 characters; only the first 7 characters will be shown on the menu.
Surveyor Profiles
Because the Surveyor does not have a display, profiles are not available. The Base/Rover switch allows simple pre-set configurations to be toggled.