![]() |
SparkFun Soil Moisture Sensor
v1.0.2-1-g6957953
Library for the SparkFun Soil Moisture Sensor
|
Arduino Library for the SparkFun Qwiic Soil Moisture Sensor
The SparkFun Qwiic Soil Moisture Sensor (SEN-17731) is a simple breakout for measuring the moisture in soil and similar materials. The soil moisture sensor is pretty straightforward to use. The two large, exposed pads function as probes for the sensor, together acting as a variable resistor. The more water that is in the soil means the better the conductivity between the pads will be, resulting in a lower resistance and a higher SIG out.
Looking for the board that matches this library - pick up a SparkFun Qwiic Soil Moisture Sensor (SEN-17731) at www.sparkfun.com.
This library provides a simple interface that enables the following functionality when using the SparkFun Qwiic Soil Moisture Sensor:
The following outlines the general use of the library in an Arduino Sketch.
At the start of your sketch, the library header file is included using the following statement:
Before the arduino setup() function, create a Soil Sensor object in your file with the following declaration:
For I2C bus:
For SPI bus:
In the Arduino setup() function, initialize the sensor by calling the begin method. This method is called after the Arduino Wire (I2C) library is initialized.
The begin method returns true if the sensor is connected and available, and false if it is not. If a value of false is returned in the above example, the sketch execution is halted.
To read the value from the sensor, the readMoistureValue() method is called on the sensor object.
The value returned is from 0 (100% wet) to 1023 (0% web - "dry"). The value is a measurement of resistance between the sensors two probes. The value range is based on the capabilities of the Analog to Digital converter (ADC) on the sensors microcontroller - it's 10 bits with a max value of 2^10 = 1024.
To read the percent moist value, call the readMoisturePercentage() method:
To read the moisture ration value (0 - 1.0), call the readMoistureRation() method:
The Soil Sensor has user controllable LED and the library has two methods to control if the LED is on or off. The following example shows how to wink the LED.
The following examples are provided with the library
The full API and use documentation for this library is provided here. For a quick reference, the main methods available in the library are listed here.
Curious about the hardware this board works with - visit the SparkFun Qwiic Soil Moisture Sensor hardware repository.
The Hookup Guide for the SparkFun Qwiic Soil Moisture Sensor is available here.
This product is open source!
This product is licensed using the MIT Open Source License.